Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=_NoMHDMfZ7Q&utm_medium=VideoTeamDescription - (VID-DM-0029)

Learn how to use a BRX or Do-more to communicate with an AMCI absolute rotary encoder in this brief video tutorial.
**Software Version used in this video: Do-more Designer 1.4.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=_NoMHDMfZ7Q&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Using the Do-more to talk to an EtherNet/IP

encoder like this one is easy. It really only has one class, one object in

that class and the usual services. There is a table of class attributes, but

it only support attribute #1 – the rev number. How do I know all of that? It’s in this manual I found on-line. Looks like Appendix B has the Common Industrial

Protocol Object definitions – which is what EtherNet/IP uses - so we scroll down to that

and here is everything we need. Here are the services that are supported – all

the usual suspects. Here is where it tells me the only Class Attribute

supported is #1. They define all of their units here – that

will be handy in a minute. And here is the one EtherNet/IP position sensor

object and all of its attributes. Looks like we can ask it for the total number

of attributes, a list of which attributes are supported – notice they go from 1 to

2 then to 10, 11, 12 etc. so not all attributes are used here. We can get the current position and the type

of device; specify the counting direction, etc. There are lots of things we can do via EtherNet/IP

with an encoder. And remember – ALL Ethernet/IP encoders

use this same table of attributes, so code you write for this encoder will work on any

vendors EtherNet/IP encoder that supports these same attributes. And that’s one of the main advantages of

using EtherNet/IP – code portability and vendor independence. So let’s do an example or two. We have a Do-more at this IP Address going

into a Stride Ethernet switch, which goes to the EtherNet/IP encoder at this IP address. As always, we start with the configuration. EtherNet/IP doesn’t affect the CPU, the

I/O or the Module configuration. It does create a new device. And while we could use this built in EtherNet/IP

device, it is much better to create a separate new device for each piece of EtherNet/IP hardware. Otherwise one device will have to manage multiple

TCP/IP connections which can slow things down. Fortunately, it’s easy to create a new device. Click on NEW, select the EtherNet/IP Explicit

Client, Give it a name – we’ll call it “AMCI_Encoder.” And we’re done. That’s all there is to creating an EtherNet/IP

device. Now we just drag an EtherNet/IP explicit message

instruction into our code and fill in the blanks. Select our new AMCI_Encoder Device. Enter the encoder’s IP Address. The default port is fine. This device only has one class and Appendix

B tells us its Class 23 hex, so that goes here. There’s only one table so that’s going

ot be instance number one. And now we just pick which parameter – or

‘attribute’ – we want – how about the current position, which is attribute 0A

hex or 10 decimal. And that goes here. We’ll use these for our status bits and

D1 for the result and D2 for the number of bytes received. The value is a DINT which the appendix tells

us is 32 bits or 4-bytes of memory, so we put that here. That’s it. Let’s add a contact so we can activate this

instruction. Accept everything; write it out to the do-more. Add the contact and the result memory locations

to the Data View. Make sure the PLC is running, and toggle the

contact. Sure enough, the instruction was successful,

we got all 4 of the expected bytes and this is the value we got. I’ll rotate the encoder shaft and toggle

another read. And it changes. Perfect. Let’s add the ability to preset the encoder

value so we can set the encoders initial output to whatever we want. It’s very similar to what we just did, so

we’ll copy that and paste it here. Looks like the preset is attribute 19 – that

goes here - and we wat to set the attribute this time. We’ll use these for our status bits and

we’ll retrieve the present value from D0, which is 4 bytes long, so that’s fine. Perfect. Let’s toggle that on C101. Accept all; write it out to the Do-more. Let’s add our preset to the Dataview, along

with its control bit. Make sure we are running, rotate the encoder

a little and read the current value of the encoder. Now let’s set our preset at 100 and toggle

its control bit to write it to the encoder. Now toggle the current value bit and its right

where we expect it to be. And that’s all there is to talking to an

encoder – any EtherNet/IP enabled encoder – from the Do-more. Just pick the attribute you want from the

table in the manual, and the service you want and your in business. If you have any questions, please contact

AutomationDirect’s FREE award winning tech support during regular business hours – they

will be happy to help you with any AutomationDirect parts. The AMCI encoder isn’t an AutomationDirect

part so please don’t and ask them about that, but you can ask folks on the forums

– they love to share their years of experience! Just don’t post any questions directed at

AutomationDirect’s support staff there, they don’t monitor the forums on a regular

basis. Spend Less, Do More. With AutomationDrect.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci