Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=SjVdYa8Hdm4&utm_medium=VideoTeamDescription - (VID-DM-0023)

Learn how to connect any PNP or NPN proximity, photo electric or ultrasonic sensor and mechanical switches to a Do-more PLC for object sensing and detection. A Do-more H2-DM1E is used in this video, but is also applicable to the T1H-DM1x Terminator PLCs.
Software Version used in this video: Do-more Designer 1.3.1

Online Support Page: https://community.automationdirect.com/s/?utm_source=SjVdYa8Hdm4&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Detecting objects with a Do-more PLC is easy. In this video we'll use - and 3 proximity

sensors, an Ultrasonic sensor and 3 different types of Photo sensors diffuse, retro-reflective

and through beam to detect the presence of an object. Here's what it looks like on the test rack. Here are the three Inductive Proximity Sensors,

the Ultrasonic sensor and the Through beam, diffuse and retro reflective photo-optic sensors. First we'll connect the proximity and ultrasonic

sensors, then we'll swap those out with the photo sensors. The Do-more has a 4 slot base with AC Power

Supply, the CPU and an 8 discrete input module. Two of the proximity sensors are intentionally

NPN and the other prox. and the ultrasonic are PNP just so you can see how to connect

the different sensor types to your controller. Since we have both types of sensors, we need

to make sure the PLC input module can handle both NPN and PNP. This Do-more input module has two commons. That's perfect because we can simply connect

one common to the positive voltage rail so the NPN sensors can pull the I/O terminal

low when they activate, and we'll connect the other common to the negative rail so the

PNP sensor can pull the I/O pin on the PLC up when it goes active. And that's all you really need to remember

when you have an NPN sensor which sinks current, you need an input module that can source the

current. When you have a PNP sensor that sources current,

you need an Input module that can sink the current. And since this input module handles both we're

in good shape. AutomationDirect's sensors have a diagram

on the sensor or on the wire showing exactly how to wire the sensor. This little box is the sensors load - which

is the PLC and for this sensor we see that the PLC provides or sources current from the

positive rail to the input of this sensor. So we know without even looking at the part

number, that this must be an NPN sensor to sink that sourced current to ground. So we connect the two NPN sensors to this

block of I/O with the positive common and we connect the two PNP sensors to this block

with a grounded common. Perfect. If we bring up the Do-more Designer software

and connect to the PLC, we can instantly see the results in the dataview when I pass a

metal object in front of the inductive proximity sensors, we see the result and when I wave

my hand in front of the Ultrasonic we also see that result. Easy. Notice that even though the NPN sensors are

pulling the input terminal low, and the PNP's are pulling it high, none of that matters

here. All we see in the dataview is if the sensor

is ACTIVE. Once the sensor is properly wired you don't

worry about whether the signal is high or low. The optical sensors are exactly the same thing. We have a through beam, a diffuse and a retro

reflective sensor, but all we really care about is: are they NPN or PNP? The through beam is NPN and the other two

are PNP, so we connect the NPN sensor to the I/O block with the Positive common and the

PNP sensors to the I/O block with the negative or grounded common. I replaced the other sensors with these so

when we bring up the dataview we get the exact same result. Mechanical switches can be connected as either

sinking or sourcing it doesn't matter. AC Proximity sensors can also be used for

sinking or sourcing, just make sure you have an input card that can handle the AC voltage. If you have any questions, please don't hesitate

to contact AutomationDirect's Free Award Winning Tech Support during regular business hours. They will be happy to help. Also, don't forget the forums. There are lots of folks there that love to

share their years of experience. Just don't post any Tech Support Questions

on the forums AutomationDirect's support staff doesn't monitor the forums on a regular basis.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci