Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=QfZPSvgV95I&utm_medium=VideoTeamDescription - (VID-DM-0026)

Learn how to sense distance using a Micro Detectors UK series ultrasonic and laser sensors with a Do-more PLC industrial automation controller in this brief, hands-on demo.
Software Version used in this video: Do-more Designer 1.3.1

Online Support Page: https://community.automationdirect.com/s/?utm_source=QfZPSvgV95I&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
For this demo we’ll be using an Ultrasonic

distance sensor that outputs 4-20mA and a Laser Distance sensor that is configured to

output 0-10V dc. Watch the Tech Tip videos to see how to setup

and configure those sensors. We just take those outputs and wire them into

the Analog Inputs of the PLC. The DoMore has several modules we could use

for this, but we’re going to use the modules I happen to have handy – a 4 input analog

current module and an 8 input 4 output voltage module. For this video we only need one current input

and one voltage input. The cool thing about the Do-more is it automatically

detects all the installed modules without you having to do anything. Let’s create a new project, and we’ll

be connecting to this style Do-more. When we connect to the PLC, we get this dialog

that allows us to pick a Do-more that was previously found, or add a new one. This is the one we want so we’ll select

that and we see a dialog that says the software is reading the system configuration. We want this blank project, and just like

that we’re connected. And if we click on the System configuration

and this base, then we see all the modules we currently have. This is the 4 input current module and here

is the 8 input and 4 output voltage module. So think about that – we didn’t have to

do anything – the software automatically discovers every module in the base. Very cool. If we click on the I/O mappings we can see

that the 4 input current module starts at WX0, and the 8 input voltage module starts

at WX4. So we’ll wire the Ultrasonics current output

into channel WX0 and the laser sensors voltage output into channel WX4. Both of these modules require 24 volts. Here it is on the hardware: 24 Volts on both

modules, here’s input WX0 and 1 and here’s input WX4 and 5. The datasheet recommend grounding all unused

channels. We didn’t do that for this quick demo, but

in your applications you will definitely want to do that. By the way, do we HAVE to accept this I/O

mapping? No, not at all. If you hit MANUAL here, you can assign these

anything you want. For us and for most of your applications,

Auto is just fine. Great, we are wired up and the hardware is

configured for us so there’s really not much for us to do except write this configuration

to the PLC. Let’s bring up a dataview and watch the

Ultrasonic that’s coming in on WX0 and the Laser that’s coming in on WX4. If I put my hand in front of the Ultrasonic

we see that respond and do the same for the laser sensor, we see that respond. Perfect. These are 12 bit A to D convertors, so the

values range from 0 to 4095. That’s ok, but I really prefer to work in

inches, so let’s bring up a scale function. We just enter the source, and its min and

max. Then what do we want that to represent? Well, this sensor is setup for 3 to 12 inches

so we enter that. Before we setup the Laser, let’s add some

nicknames just to make our lives a little bit easier. I’ll bring up the documentation editor and

add some stuff. Let’s make D0 the Ultrasonic sensor in inches,

D1 the Laser sensor in inches, WX0 is the Ultrasonic sensor raw input to us and WX4

the Lasers raw input to us. Now when we bring up the scale function we

don’t have to remember memory locations, we just use the nicknames. This is the Laser sensor. His raw output range, which represents 2 to

16 inches and the result goes in Laser Inches. Perfect. So now in our ladder code, we can just use

the inches version of the sensor to make our lives easier – if the laser detects something

closer than 10 inches turn on c0. If the Ultrasonic is greater than 8 inches,

the turn on c1, for example. Let’s accept those changes and write that

to the Do-more. And sure enough, if I wave my hand in front

of the sensors, we now see all the results in inches. Exactly what we want. Let’s look at those on the trend view. I’ll create two panes, one for each sensor. On pane 1 we’ll add the Ultrasonic in inches

and on pane 2 we’ll look at the laser in inches. Let’s make the Ultrasonic Green and fatter,

and let’s make the laser red and a little bit fatter. Close that, wave our hands in front of the

sensors and we can see how the sensors respond visually. That’s nice. So between the hardware being automatically

configured, the use of nicknames to keep things easy to read and the scale function to convert

raw data into stuff we can understand, the Do-more makes PLC programming easy. And the best part – it just works the way

you expect it to. If you have any questions, please don’t

hesitate to contact automation directs free award winning tech support during regular

business hours. They will be happy to help you. And don’t forget the forums. There are lots of folks there that love to

share their years of experience. Just don’t post any support questions there. AutomationDirect’s support staff doesn’t

monitor the forums on a regular basis.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci