Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=BtGAaIqC8JE&utm_medium=VideoTeamDescription - (VID-DM-0022)

Learn how easy it is to read temperature with a Do-more Series controller.
Software Version used in this video: Do-more Designer 1.3.1

Online Support Page: https://community.automationdirect.com/s/?utm_source=BtGAaIqC8JE&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Reading temperature with a Do-more PLC is

easy. In fact this is all the code you need right

here. Don't see any? Me neither - there isn't any. You don't have to write a single line of code

to get temperature values with a Do-more PLC! You'll have to write code to USE the temperature,

of course, but once you configure the temperature modules, the temperature values just appear

ready for you to use. Easy. In this example we have a Do-more PLC connected

to 2 thermocouples, 2 RTDs, and 3 different types temperature transmitters, a Sensor Head

Mounted Transmitter, an integral transmitter, and a fixed DIN rail mounted transmitter. Here's what it looks like on the test rack-

Here's the Do-more PLC, 2 thermocouples, 2 RTDs, and 3 different types temperature transmitters. They are wired exactly like the block diagram

shows. The sensor wire shields are grounded only

at the sensor end - if you ground the shield at both ends you just created another current

path which can cause ground loops and actually make things worse than having no ground at

all! So be careful to only ground sensor shields

at one end. The thermocouples use the special thermocouple

DIN rail terminal blocks - these ensure continuity of the special thermocouple wire by clamping

the wires together instead of connecting them through a terminal block which would create

unwanted thermocouple junctions. To configure the thermocouple module, you

just move some jumpers. Select the number of channels you are using

with these first two jumpers. We're using two channels, so we only want

a jumper on terminal 1 - exactly like you see here. The thermocouple module supports all kinds

of sensors and can even be used as a 5V or 156mV analog input! We have Type J Thermocouples, so it looks

like we need all 4 jumpers installed - and we do, so we are good to go. The last two jumpers select the units - degrees

C, degrees F, and you can select whether you want the result to be signed or 2's complement

- which some systems require. We have this one is set for 2's complement,

degrees F. We're only using 2 of the four channels here. Since these channels measure extremely small

voltages, it is easy for them to pick up stray signals from electrical noise when not connected

- so make sure you jumper any un-used channels to keep your system as electrically clean

as possible. That's it for the thermocouple module, let's

look at the RTD module. The RTD module uses the same jumper settings

for the number of channels, no jumpers is one channel, this jumper adds a channel, and

this jumper adds two channels. We're using two channels total, so we need

to add one by putting a jumper in this slot here. The RTD module supports all of these RTDs,

and we are using Pt100's so we need these two jumpers installed, just like you see here. The units selection is just like the thermocouple

module, again we have it set for 2's complement Degrees F.

Finally, we're using an analog input card to read the 4-20mA signals from three temperature

transmitters and it has a similar jumper selection setup. We're using three channels, so we need the

jumper that adds 2 channels. Perfect. Well, the modules are all configured, so let's

look at the software. As we mentioned earlier, you don't have to

write any code to get the temperature values once the modules are configured. The cool thing about the Do-more Designer

Software is when you connect to the Do-more PLC, it automatically identifies all the modules

you have plugged in and assigns memory locations for the results. We see that under system configuration, I/O

Mappings. Here we see the analog card had 8 status bits

we can read and 8 analog values we can read. The Thermocouple and RTD modules are the same

except they have 4 status bits and 4 analog values, one for each channel. All of the details about these modules status

bits and mappings and configuration is in the Do-more Hardware manual, which is free

to download. That's important don't go looking in the individual

module's specs or manuals those are maintained for the older legacy processors, not the Do-more. Everything you need to know about connecting

a module to a Do-more is in the Do-more hardware manual. Here's a Dataview showing us all of the Thermocouple

and RTD values. These values have an implied decimal point. If we put a cup of cold water on one of the

probes and hot water on another, we see the values change. Exactly what we expect. If we add the temperature transmitter values

to the dataview, we can see that the results aren't in degrees F. Remember, the analog

card takes 4-20mA in, and converts that to a number in the range of 0-4095. Wouldn't it be great if we could get the corresponding

number in degrees F? Well, The cool thing about the Do-more is

it has a scale function that does exactly that. We just specify the input range and the range

we want that to correspond to, in this case 0 to 100 degrees F and put that result into

a Real memory type and we are done! Now if we watch these values in the dataview,

we get actual temperature values with decimal point and everything which makes writing your

ladder code much easier. I have a C-more HMI monitoring all of those

values. If we swap the probes, we see the results

graphically. Perfect. And if I disconnect one of the wires, the

indicator that is monitoring that status bit provided by the temperature modules lights

up so I instantly know there is an issue with the wiring of the sensor. Awesome. And again, we didn't have to write one line

of ladder code to get these temperature values though we did add a scale function to makes

things a little easier to work with. If you have any questions or need any help,

please don't hesitate to contact AutomationDirect's free award winning tech support during regular

business hours. They will be happy to help. And don't forget the forums there are lots

of folks there that love to share their years of experience. Just don't post support questions there, AutomationDirect's

support staff doesn't monitor the forums on a regular basis.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci