Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! Communication Options IIoT Edge Device - Your low cost link to Industry 4.0Integrated Motion on Multiple Levels Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy! BRX IIoT in Motion
Free Software
What's New with Do-more Designer Dashboard - Easy Navigation Simulator IIoT WebServer Connectivity Motion on Multiple Levels Simple Data Logging Data Delivered Easy PID Video Help Auto-Discover I/O Powerful Math Trouble free Troubleshooting DirectLOGIC Migration Free Online Training Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Instruction Set
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=dd8qEblkTos&utm_medium=VideoTeamDescription - (VID-DM-0042)

Learn what the difference is between Programs, Tasks, Subroutines and ISR's so you can get the most our of your Do-more PLC.
**Software Version used in this video: Do-more Designer 2.0.0

Online Support Page: https://community.automationdirect.com/s/contactsupport?utm_source=dd8qEblkTos&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
So what is the difference between a task,

a program, a subroutine and an Interrupt Service Routine? In this video we’ll take a quick look at

the differences at a very high level and then in separate videos will focus on each one

with live examples so you can see exactly how to use them. Normally, a PLC program reads its inputs,

executes its logic and then updates the outputs. We call that a scan. Suppose we have a bunch of rungs of ladder

code here and the exact same lines of code here and here. When ever you see redundant blocks of code

like this, think about pulling that code out and putting it into a subroutine. Now the ladder code just has a single call

to the subroutine and all three call the exact same code. Now if you have to modify it in the future

you only have to modify it in one place. That saves you time and effort and just makes

your ladder code much easier to read and maintain. You can even pass the subroutine parameters

so if each section needs to use different values you can do that too. The key thing to remember is the Subroutine

runs as if it is part of the main scan loop. The main loop jumps to the subroutine, executes

it and then picks up right where it left off. So you are still running the same long scan

loop, it’s just packaged a more modular easier to maintain fashion. And it also takes less memory. So if you have redundant code that may just

need to use different values but does the exact same operation – Think Subroutines. Programs are not subroutines. The Main Program is a Program that is guaranteed

to run every scan while the PLC is in RUN mode. The cool thing about the Do-more is you can

create your own programs. Suppose for example that you have several

machines in a process line. Maybe one preps material, one drills holes,

one rivets, and one does some kind of finishing work. You could do all of those in one long monolithic

block of code, or you could pull each one out and create a separate Program for each. Then in the Main program you just RUN each

routine to enable it and they all go off and run their own machine – I like to think

of it as independent background process. Programs are also good for processing asynchronous

things like handling of incoming messages. You start the message handler program with

a RUN command and then it just patiently waits for messages in the background while the main

scan loop runs its normal processes. When it gets one it processes it and then

goes back to waiting. Again, an asynchronous or background process. So any time you have a large bock of code

that’s running multiple processes that each needs to run continuously or even for just

several scans at a time, think about breaking the code out into separate programs. You can do all the same stuff in a Program

that you can do in main program loop, but it will make your code much easier to read

and maintain. In this example main launches each of the

processes and then sits back and does nothing. We’ll do some live examples of this in the

video dedicated to programs and tasks. A Task is basically a stripped down Program. The main difference is it executes to completion

and exits. One pass and it’s done. It won’t execute again until it’s re-enabled. Of course, since a task only runs one pass,

it doesn’t do stage programming. That wouldn’t make any sense because stage

always runs over multiple scans – right? Tasks are ideal for doing things that just

need a single pass like checking an alarm value periodically because you can just call

that code block when you need it OR you can tell the Task to do periodic updates for you. That’s cool. Tasks are also great for doing episodic stuff

- maybe you need to calculate the production rates and values at the end of a shift. And calculating all of that stuff is going

to take a long time relative to your scan. Well, look at this. You can tell a Task to only run for a limited

amount of time – we call that a time slice. So now it might take several scans to finish

the calculations, but since it only does a little bit at a time, it doesn’t affect

your regular scan interval very much. That’s a great way to make sure your episodic

task doesn’t overly burden you main scan loop and slow down your machine processes. Time slicing can also be used with Programs

so you can dedicate the bulk of the scan to one machine or process and the rest of the

scan time to the others if you want to. That’s one of the things that makes the

Do-more so powerful. You have complete control over exactly how

your system runs. You also have complete control over WHEN things

run. You can tell the Do-more PLC what order you

want the various tasks and programs to run in. We’ll do several live demos of time slicing

and execution order in the video on Programs and Tasks. For now just know that it’s an amazing feature

of the Do-more PLC. Interrupt subroutines are great for handling

events that need to be serviced right now. You have a scan loop, and maybe some programs

and tasks and they are doing their thing. But when a triggering event occurs you want

to run a specific block of code as soon as that event happens. Maybe you want to react to the rising edge

of a signal when it occurs and not wait until the next scan to see something changed for

example. That’s a good example of when you would

want to use an interrupt service routine – or ISR. It doesn’t mater where the program is in

the scan loop, the program immediately jumps away, executes that ISR and then comes back

to where the scan loop left off and continues on its way. It’s kinda like a subroutine that can run

when ever a triggering event happens. That triggering event could be an external

input coming in, a timer timing out, all kinds of things. Of course, since it is interrupting the flow

of the scan, you always want to make sure the ISR is just as short as it can possibly

be. For example, in an ISR, all you would do is

make note that a signal changed. Just take note that a signal changed and let

some other routine take care of the details later. Don’t try to do any more than that in an

ISR, otherwise it might impact your scan time. So we have Subroutines which are great for

cleaning up redundant code. We have Programs which are really great for

running independent processes. We have Tasks which are particularly good

for periodic and episodic processes that only require one pass. And we have Interrupt Service routines which

are great for reacting immediately to an event of some kind. All of which make maintaining and debugging

your code a whole lot easier. This was just a very quick introduction there’s

a whole lot more to this. Check out the dedicated videos to learn exactly

how to use each of these powerful tools. And if you have any questions, please contact

AutomationDirect’s free award winning support team during regular business hours. They will be happy to help. And don’t forget the forums. There’s lots of experienced automation professions

there that love to share their years of experience. Just don’t post any questions directed at

AutomationDirect’s support staff there, they don’t monitor the forums on a regular

basis. Spend Less. Do-more. With AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci