AutomationDirect will be closed for Christmas holiday on Wednesday, Dec 24th and Thursday, Dec 25th
We will close at 3PM ET on Tuesday, December 23rd. Please note our shipping changes for Tuesday.
Freight shipments, FedEx ground and customer pickup deadline is 11:00AM ET. FedEx Priority (and free 2-day delivery) cutoff will be 1:00 PM ET. No UPS shipping will be available on Tuesday.
Drop ship vendors, Saginaw, Husky and Weigmann will also be closed Friday, Dec 26th.

Merry Christmas to each of you and your families from the employees of AutomationDirect
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
Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=LdvNtZEA4Hs&utm_medium=VideoTeamDescription - (VID-DM-0031)

Learn how to use an EtherNet/IP Explicit Do-more client with Datalogic Matrix 210 Bar Code Imager in this brief video tutorial.
Software Version used in this video: Do-more Designer 1.4.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=?utm_source=LdvNtZEA4Hs&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
The Datalogic Matrix210 is an awesome little

bar code imager that can handle both 1D and 2D bar codes. Instead of the traditional red laser beam

scanning the bar code, it actually grabs an image of the bar code with a camera and analyzes

the captured image to decode it. And the best news is it is EtherNet/IP compatible,

so you can monitor and control it from an AutomationDirect Do-more PLC. I have a Do-more PLC connected to a Stride

Ethernet switch which is connected to the Matrix Imager. I am also using the Datalogic CBX500 breakout

box as a simple way to connect power to the imager. Once you have the unit setup and calibrated,

Get the Datalogic utility called VisiSet, connect to the Matrix210, and under Device,

get the devices current configuration. Make sure EtherNet/IP is enabled here. Make sure the operating modes are setup as

shown here. And make sure you enable the codes you plan

to use. We’ll be using this Code128 in our examples. Send that to the unit and you are ready to

use EtherNet/IP. If you have any questions about setting up

the Matrix210, call the folks at Datalogic – I found them very friendly and helpful. Now that we have a configured imager, we just

setup the Do-more like we always do. I have a new project open and I’m connected

to the Do-more. We always start with the system configuration

and work our way down this list. Under CPU we can make sure that the Do-more’s

IP address is on the same subnet as the imager – if not we can change it here. And the Do-more is a Client controlling the

Imager which is a server, so we don’t need to enable the Do-more as a server. We’re not adding any I/O to the Do-more

so there is nothing to do here. We’re only using the built-in Ethernet port

and not adding any new modules to the PLC so there is nothing to do here. Under Device configuration we could use the

built-in EtherNet/IP device to talk to the Matrix210, but it it’s always better to

create a new Do-more Device for each piece of hardware you want to talk to via EtherNet/IP. That way no Do-more Device has to manage multiple

TCP/IP connections which would slow down your code. Let’s create a new device, we want an EtherNet/IP

device, and we’ll call it Matrix210. Great we now have a Do-more Device that will

handle all the low level details of dealing with the imager. Which means we don’t have to worry about

buffer management, or handshaking, or memory allocation, or any of that stuff. The Do-more does all of that for us. We don’t have any new I/O and the EtherNet/IP

device we created doesn’t create any heap structures for us to talk to so we’re done

configuring the Do-more and we’re ready to talk to the Matrix210 imager. To do that, we just grab an EtherNet/IP instruction,

drop it on the rung and fill in the blanks. We want to use our new Martix210 Device and

he is at this IP address. This is where we put the codes we use to talk

to the EtherNet/IP device. Where do you get the codes? Over on the Datalogic website search for the

Matrix EtherNet/IP User Guide. I got this list here. They are all the same, just pick one. This user guide lists all the things you can

do with the imager via EtherNet/IP. Let’s do something simple for our first

example – let’s get the vendor ID which is always in the Identity object. And here it is. Looks like we need Class 1, Instance 1 and

Attribute 1 to get the Vendor ID. We want to Get this information and we’ll

do it on the leading edge of the ladder contact. We’ll use these status bits and we’ll

put the Vendor ID in D1 and the number of bytes actually returned in D2. The Vendor ID is an Integer, so we expect

a maximum of 2 bytes. Great. Accept that and add a contact to enable the

instruction. Remember – we told the instruction to start

on the rising edge of this contact – which is indicated by this triangle - so we don’t

need a rising edge contact here. Looks good to me, so let’s accept all changes

and write it out to the Do-more. Let’s bring up a dataview so we can control

this and add the contact and the result. Make sure we’re running, enable status and

enable editing for the dataview. If we toggle this contact we get this 850

which according to the manual is the Vendor ID. Perfect. Here’s the sequence of events we need to

get the barcode: First we need to trigger the Image. Then we need to wait a little while for the

imager to do its thing. Then we read this item sequence number and

fragment sequence number and then we write those back to the imager to acknowledge that

we actually got the barcode. I went ahead and created this little Get Bar

Code program so you wouldn’t have to wait while I typed all this stuff in. Let’s take a look at that. In stage 0 we activate the message trigger. It’s just the one EtherNet/IP instruction

talking to our Matrix210 Device at this IP Address, using these codes and issuing a write

with bit 7 set in this variable. Bit 7 of this byte is what’s going to trigger

the imager. If that’s successful we jump to stage 10,

if not, we jump to stage 99 and increment an error counter. Stage 10 releases the trigger so it’s the

exact same instruction except it sends this register which has a zero in it to clear the

trigger bit and it jumps to stage 20 when done. In stage 20 we give the imager a little time

to process the image. We start a timer and jump to stage 1 when

the timer is done. Which also shows that Stages don’t have

to be in numerical order. In Stage 1 we Get the data into this string

using these EtherNet/IP attributes from the user guide and jump to stage 2 when we are

successful. In stage 2 we get the Item Sequence number

into this memory location and jump to stage 3 where we get the Fragment Sequence number

into this memory location and jump to stage 4. In stage 4 we write the Item Sequence number

back to the imager using a Set command and in stage 5 we write the Fragment Sequence

number back to the imager. Again ,writing the Sequence numbers back to

the Imager is what acknowledges the receipt of the data so the imager can process the

next bar code. When done we exit the program. Stage programming makes sequencing things

like this so easy because it takes care of all of the interlocking and transitions automatically. So all of these EtherNet/IP instructions we

used are the pretty much the same aren’t they? We just look up the codes in the user guide

for what we want to do and fill in the blanks. Back in the main program, we run that Get

Bar Code program on a rising edge of a contact. Accept all of that and write it out to the

Do-more. Let’s add the new contact that triggers

that program and the Bar Code result to our dataview. Toggle the contact and we get our bar code. Change the bar code, trigger another read. And we get the new result. Perfect. This is by no means a complete example. There’s a lot more of information you can

pull from the imager and use to your advantage all of which is in that EtherNet/IP manual. But for now, this ought to be enough to get

you up and running. If you have any questions about using EtherNet/IP

on the Do-more, contact AutomationDirect’s free award winning tech support during regular

business hours. Don’t call them about Datalogic Imagers

or any other device AutomationDirect doesn’t currently have – they will just send you

to that vendors support. So save yourself a phone call. And check out the forums. That’s another great place to get information

from experienced - and very helpful – Do-more users. Spend Less. Do more. With Automation Direct.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci