Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! IIoT Edge Device: Your low cost link to Industry 4.0..and beyond! Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy!
Free Software
What's New with Do-more Designer Dashboard- Easy Navigation Simulator Easy PID Auto-Discover I/O Powerful Math Troublefree Troubleshooting DirectLOGIC Migration Instruction Set Free Online Training Video Help Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Videos


BRX Series PLCs (Stackable Micro Brick) Videos

View Do-more Designer Video


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=Fope7_yqwek&utm_medium=VideoTeamDescription - (VID-DM-0038)

Do-more Designer has a lot of utilities to help debug projects. This video quickly walks through those and points you to dedicated video tutorials for each.
**Software Version used in this video: Do-more Designer 2.0

Online Support Page: https://community.automationdirect.com/s/?utm_source=Fope7_yqwek&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
Do-more designer has a lot of tools you can

use to debug and troubleshoot your programs. We’ll take a quick spin through them in

this video, and point you towards other videos where you can learn more. The dashboard is a great place to look for

issues because it shows you pretty much the entire system at a glance. For example, I see it’s reminding me that

the firmware is not the latest version. How would I fix that? Just click on it and it takes you right to

the dialog you need to see what your options are. This example says there is something wrong

with the I/O system. How do you fix it? Just click on it and again it takes you to

right where you need to go to figure it out. And that’s the key with the dashboard – if

you see anything that looks out of place, all you have to do is click on it and Do-more

Designer will walk you right down the path needed to solve the issue. Here’s a little test program for us to play

with. The quickest way to see what’s going on

is to click on all status. If I change the inputs on the PLC, then we

see the results right on the screen which makes it super easy to visualize how power

flows through the contacts and instructions. Keep in mind these are updated at the bottom

of the scan – not during the scan. Dataviews are another quick way to quickly

see what’s going on. You just put whatever you want to monitor

here and with status on, you see the current values. You can monitor anything here, strings, structures,

done bits, and any memory location in the entire system. You can also change values - press the edit

button, enter a value and if you watch the current value while I hit the write button,

sure enough it changes. Keep in mind that if you write to an input

in the dataview, that’s going to get overwritten on the next scan making whatever you wrote

go away. Same thing applies to any outputs the program

is writing to. That’s easy to forget so keep that in mind. While you can’t change an input using the

data view you CAN force it to do what you want. Suppose you need to ignore a certain input. That’s where forces come in handy. You can override any I/O point or memory value

using this table, right clicking on an element or right clicking on a data view entry. By the way, did you know that if you are NOT

I edit mode and you double click on a contact you can change its value right there? Or any value you want. That’s really great for those times when

you just want to mess with one value and don’t want to brig up a whole dataview to do it. Just click on the value and hit the write

button. Trend views monitor data so you can see how

things change over time. You can change the scale and even pause the

trending with this history button so you can scroll back in time and see the history of

the data. To create a trend view you could push the

trend view button and add items to it manually, but look at this. If you right click on an instruction you can

just select trend and it automagically fills in the trend view for you. You can then add or remove items till your

hearts content. Speaking of Trend Views, some instructions

even have little mini trend views built in. Just turn on status to see it. If you have a program with lots of programs,

or tasks and subroutines, expand those over here and if status is enabled, you will see

which of them are currently in use. You can even see which stages of your stage

program are active. I love this because at a glance I can see

if I’m stuck in one stage or one routine or if a task is even being executed and how

often. Do-more Designer has a built-in debugger. You just click on debug and you can now pause

the program, issue just a single scan, multiple scans, manage suspended tasks, monitor the

current scan time of the PLC, etc. There’s even PID overviews and viewing tools

so you can monitor and adjust your PID loops. And don’t forget the simulator for debugging–

it’s a great way to verify code independent of the hardware and it has a built in PID

simulator too! To learn more about any of these debugging

and troubleshooting tools, go to the start page, and click on the Video Browser tool. You can type any topic you want here, or select

a category here and even expand the search to include all related videos. You can then watch the video right now or

download it so you can watch it later in places where you don’t have internet access. Having all of these video tutorials instantly

available is one of my favorite features of Do-more Designer. That’s a pretty good summary of the troubleshooting

tools you have at your finger tips with Do-more Designer. If you need any help with any of these remember

that pressing the F1 key from pretty much any place in Do-more designer will bring up

context sensitive help. If you are in the dataview and hit F1 – you

get data view help. If you are over an instruction and press F1

you get the instruction help. If you in the trend view and press F1 – what

do you get? Trend view help. You get the idea. If you need even more help with your Do-more

program, please contact AutomationDirect’s free award winning support team during regular

business hours. They will be happy to help. And don’t forget the forums – there are

lots of experienced automation professionals there that love to share their years of experience. Just don’t post any questions directed at

AutomationDirect’s support team there, they don’t monitor the forums on a regular basis. Spend Less. Do More. With AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROqT5KTqjfyhR7t0fD16Nya8

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci