Filter Results Clear All
You've selected:
> Programmable Controllers > BRX PLCs (Stackable Micro Brick)
  •   Shop  
  •   Overview  
  •   In Depth  
BRX Home BRX - Your Automation Foundation Configure a BRX
 
Features
10 ways it's better with BRX PLCs! Communication Options IIoT Edge Device - Your low cost link to Industry 4.0Integrated Motion on Multiple Levels Not Your Everyday Analog Security Simple Data Logging/Advanced Data Control Fortified with American Pride Easy Migration Motion Control/Positioning made easy! BRX IIoT in Motion
Free Software
What's New with Do-more Designer Dashboard - Easy Navigation Simulator IIoT WebServer Connectivity Motion on Multiple Levels Simple Data Logging Data Delivered Easy PID Video Help Auto-Discover I/O Powerful Math Trouble free Troubleshooting DirectLOGIC Migration Free Online Training Download the Free Software
Hardware
Hardware Overview M Series CPUs (no I/O) 10-point Series CPUs 18-point Series CPUs 36-point Series CPUs Ethernet Remote I/O Expansion Modules Pluggable Option Modules Connection Options Spare Parts Go to ZIPLink Selector Tool
Instruction Set
Videos


BRX Series PLCs (Stackable Micro Brick): Do-more Designer Videos

Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=K6j4825YZlo&utm_medium=VideoTeamDescription - (VID-DD-0038)

This video gives basic information on Using the LABEL "Program Label" instruction in the Do-more Designer software. It presents information that is commonly missed by users.
** Software Version used in this video: Do-more Designer 2.0.3

Online Support Page: https://community.automationdirect.com/s/?utm_source=K6j4825YZlo&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
When a Goto instruction is executed it can

jump directly to the location of a label in the code block. Now, this label must be inside of the same

code block as the GOTO that is pointing to it. The label instruction, itself, is a 'power-rail'

instruction. This just means that even though it is displayed

on the left hand side of the logic, it is actually entered in on the right-hand side

of the logic and then collapses directly down to to the Power rail as it cannot have contacts

or logic in front of the instruction.


BRX Do-more PLCs Do-more Designer Software & Programming
  • Video
    BRX Do-more Designer Using the CALL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENDC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the ENTASK Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the EXIT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the GOTO Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the HALT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the LABEL Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the REBOOT Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RESTART Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RET Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RETC Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTCONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTDECONFIG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTRESUME Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the INTSUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the JMPI Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the RUN Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the STOP Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SUSPEND Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the WATCHDOG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the YIELD Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SG Stage Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGCONVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGDIVRG Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRST Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGRSTR Instruction from AutomationDirect
  • Video
    BRX Do-more Designer Using the SGSET Instruction from AutomationDirect

Playlist Not Found Could not find playlist PLPdypWXY_ROovolXmvgjO63qk2RdsoIGx

Playlist Not Found Could not find playlist PLPdypWXY_ROoIDZ7MO4OLz8AMJ_lExObe

Playlist Not Found Could not find playlist PLPdypWXY_ROoiFQetOa9Kc_9NF3dLgQon