AutomationDirect
Login | Register
Accounts & Orders
Cart
1
$337.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $337.00
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
CLICK PLUS Home Looking for the lowest-cost? Check out the original CLICK Configure a CLICK PLUS
Features
Hardware
CLICK PLUS CPU modules CLICK PLUS Option Slot modules DC I/O modules AC I/O and Relay modules Analog modules Specialty modules Power Supplies Programming Cables ZIPLink Wiring Solutions Go to ZIPLink Selector Tool
Free Software
What's New with CLICK Software Programming Environment Easy PID Instruction List Toolbars Address Picker Subroutines Interrupt Routines System Configurator Software Help
Getting Started
Programming a CLICK/CLICK PLUS Power Considerations What you Need Installation & Wiring Choosing I/O Configure a CLICK PLUS
 
Software Download
Intelligent Modules

Programming the CLICK/CLICK PLUS

  • Download and install the CLICK Software
  • Connect your programming cable between the CLICK PLC and your PC
  • Please refer to the Manual, the online help, and these online training videos for more information.

A Simple PLC Application:

Example Application

A Simple PLC Program:

Here is a sample CLICK PLC program, that might be used to control a stack light. Suppose we connected a switch to the first input on the CLICK CPU module, and a stack light to the first output. This simple PLC program could be used to associate the switch with the light, and to provide on/off control of the light via the switch. And yes, you might ask why not simply wire the switch to the light - and you might be able to do that in some situations, but let's assume the the switch must use low voltage DC, and the stack light requires 110VAC. Now we have an application where a relay might be used, and since a PLC is basically a collection of relays - we can use a PLC!

A Simple PLC Program:

Example Program

Ladder Logic:

Example Program

Ladder Logic:

PLCs use a programming scheme known as ladder logic. Ladder logic is a visual representation modeled after the relay wiring schematics that the PLCs often replace. The vertical line on the left of the schematic is known as a "power rail" and the horizontal lines are called rungs. When a contact is placed on a rung and that contact is "closed", then you can imagine that power will flow across the rung to the right and power any other instructions (or coils) that may be present on that rung. In this example we have one rung of ladder logic, with a single normally-open contact controlling an output coil. When this program is compiled and transferred to a CLICK PLC and the PLC is placed in the "Run" mode - the PLC will scan this ladder logic several hundred times per second. It will evaluate the state of the first input (X001) on every scan, and if that input is active (ie. if our switch is turned "on") then the PLC will energize the first output (Y001) thereby turning on the light. If the input is inactive, the output will be de-energized

Inserting Instructions:

It's easy to insert and configure instructions with CLICK. Simply drag the desired instruction from the right-hand pane in the software, and drop it onto one of the rungs in the ladder window. The configuration dialog box will appear and you can fill-in-the-blanks with your desired memory addresses and any other parameters that may be optional or required. There is a help button on every instruction dialog box that will take you directly to the help file entry for that instruction.

Memory Addresses:

PLCs use Memory Addresses to refer to the various bits, words, and strings of data that are used for programming. The naming convention for CLICK PLC memory addresses uses X to indicate "real-world" inputs, and Y for real-world outputs. In our example we wired the switch to the X1 input, and we then refer to that input in the program using the memory address X001. Likewise we wired the light to Y1 and we use Y001 to refer to this output. There are also naming conventions for other types of PLC memory addresses including internal addresses that are used for programming and internal functions but which may not have a "real-world" counterpart. See the help files for an in depth explanation of PLC memory addresses. With the CLICK PLC you can also assign "nicknames" to your memory addresses to help maintain your sanity.

This is the END:

The END instruction is required, and signals the PLC that the end of the ladder logic has been reached. Any instructions placed below the rung with the END instruction will not be executed.

The Scan:

One important thing to understand is that on each scan the PLC evaluates all the rungs of logic, and THEN updates the physical I/O - before scanning the ladder logic again. The "real-world" I/O is not updated on a rung-by-rung basis.

More Examples:

We've got more example programs here.

Online Training:

InterConnecting Automation Inc. is an independent company dedicated to PLC based training with an emphasis on real world experience. They also offer online training as well as on-site training for PLCs. They offer both generic PLC training (applying to any brand) and they also have training for specific PLCs including the CLICK PLC. AutomationDirect has found the CLICK training to be so useful that we use it to train our own employees. The online training is absolutely free of charge for anyone.

Click here to access the CLICK PLC specific training site at InterConnecting Automation Inc.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info