AutomationDirect
Search
Login | Register
Accounts & Orders
Cart
1
$40.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...Loading...

Your Account

Account Home

Checkout   $40.50
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
> Programmable Controllers > Do-more H2 & T1H PLCs (Micro Modular & Stackable)
  •   Shop  
  •   Overview  
  •   In Depth  
Do-more Home Download Free Software
 
Features
Top 11 Ways You Can Do More with this PLC Serial Communications Ethernet Communications High Speed Modules Hign Speed Inputs Motion Control Remote I/O Free Online Training
Free Software
Simulator Auto-Discover I/O Communications Powerful Math Monitoring & Troubleshooting Memory Management Program Management Project Management Security Download the FREE software
Hardware
H2 CPUs T1H CPUs Bases AC I/O Modules DC I/O Modules AC & DC I/O Modules Analog I/O Modules Specialty Modules Go to ZIPLink Selector Tool
Videos


Do-more H2 (Micro Modular PLC) Videos

View Do-more Designer Videos


Detailed Product
Overview



To learn more: https://www.automationdirect.com/do-more?utm_source=_d4MfGSAyvM&utm_medium=VideoTeamDescription - (VID-DH-0006)

This video covers how to use CTRIO2 and Do-more processor to implement a Trapezoid profile.

Online Support Page: https://community.automationdirect.com/s/?utm_source=_d4MfGSAyvM&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript
The Trapezoid command simply ramps up to speed,

runs for a while, and then ramps back down to the position specified. Make sure the Module is configured correctly

– so hit the configure button, module configuration, our module, Configure the IO. These are my inputs – I’m not using any. And I have assigned two outputs to be pulse

step and direction. Step 2: Set up the profile. We’re going to use the same one we had in

a previous video – the JOG video – but just as a reminder, this is our CTRIO module,

we’re going to start at 100 pulses per second and we’re going to ramp up to 200,000 pulses

per second. Since this stepper motor is a 20,000 pulses

per revolution and that is 10 times that, that would be 10 shaft revolutions per second. And we are going to get there in half a second

because we are going to ramp at 400,000 pulses per second. And it’s going to decelerate at the same

rate. We are not using an encoder. We are also going to initialize our starting

position at zero. So we initialized the hardware, we setup a

profile. All that is left to do now is to setup our

trapezoid function. The CTRIO2 has a CT AXis Trapezoid function. This one is easy – we select the module

we are going to use, what kind of move it is going to be. Are we going to move to an absolute position

or are we going to move relative to where we are? Let’s start with an absolute move. Our target position will be placed in register

D0. You can put any register you want there or

you can even put a constant if you want to. That’s all there is to setting up the Trapezoid

function. Let’s put some controls in here. We’ll use our X0 switch to enable the Trapezoid,

and let’s use X1 to suspend it. We need one more thing here – we need a

Dataview so we can put some values in that D0 register that specifies our position. Let’s turn on EDIT and let’s make our

first position we want to go to 100,000 pulses. Which would be 5 shaft revolutions. Let’s accept that, save it, write it to

the PLC, and we are ready to go. If we go back and look at our configuration,

and I reset the PLC, sure enough the configuration zeroed out our position and now if we enable

the trapezoid function by flipping on switch X0, and we watch our position right here,

we can see our carriage ramp up and ramp back down very quickly and stop at the 100,000

we specified. If I turn off this switch, and turn it back

on, the carriage doesn’t move. Remember, this is an Absolute move. Since we told it to go to 100,000, and we

are there already, the carriage didn’t move. I’m going to turn off X0. Let’s go out to 200,000. D0 is now 200,000 – we can see that here. If I turn on X0 – sure enough the carriage

moves out to 200,000 and ramps back down and stops. If I want to go back home, well, I just put

a zero here – write that to D0. D0 is now a zero so if I re-enable X0, the

carriage moves all the way back to zero and stops. Now let’s see how the Relative command works. We simply go into the Trapezoid function,

flip it over to relative, say ok, accept it, save it, write it out to the PLC. D0 is at 100,000. And I am currently at position 0. If I enable X0 with this relative command,

sure enough, the carriage moves out 100,000 pulses. Remember, with the Absolute positioning, if

I flipped X0 again, nothing happened because we were already at the 100,000 we specified. But because this is a relative move - if I

flip X0 – the carriage moves another 100,000 pulses. And yet a third 100,000 pulses. So now we are out at 300,000 using the relative

move. With the absolute move, to get home, I would

put a zero in D0. With relative, I want to go minus 300,000

pulses. Enable X0 and the carriage goes all the way

home. PLEASE make sure your CTRIO2 firmware is up

to date. Use the live update under Help – Check for

Updates. Of course mine is up to date so there is nothing

showing here. But if you did, you would download the files

using this button here. Once you have those files, go to PLC, Monitor

CTRIO Module and look right here. If this has an asterisk next to it, it means

it is out of date and you hit the Update OS Button. It will then take that file you just downloaded

and burn it into the CTRIO module. That’s all there is to implementing motion

using the Trapezoid instruction with the Do-more and the CTRIO2. Be sure to check out the other videos in this

series for more on using motion. And as always, please send us any comments

you may have, we appreciate the feedback. Spend Less. Do-more. From AutomationDirect.


Playlist Not Found Could not find playlist PLPdypWXY_ROoEcDCcD10Qdb3S9tOmfEn5

Playlist Not Found Could not find playlist PLPdypWXY_ROoJx-HnK9gj2Z5a-i7th-UK

Playlist Not Found Could not find playlist PLPdypWXY_ROqvbaYVBWc3kH-pP01fI4-E

Playlist Not Found Could not find playlist PLPdypWXY_ROr5OPw3e0o8rLC0JQijmCNY

Playlist Not Found Could not find playlist PLPdypWXY_ROrtSkGYNq8Xc52QWTCWf2Ci

Playlist Not Found Could not find playlist PLPdypWXY_ROrRJ5YuFYxs3mSXr9250AN7

Playlist Not Found Could not find playlist PLPdypWXY_ROqJO86ikigKmjnSkbguBKBw

Playlist Not Found Could not find playlist PLPdypWXY_ROqWWy8OnWGt3YD4Dald6uf-

Playlist Not Found Could not find playlist PLPdypWXY_ROrmjIdXLaeovoTLZP65hdac

Playlist Not Found Could not find playlist PLPdypWXY_ROoqTZihvX8c8UUj5GzVCuKH

Playlist Not Found Could not find playlist PLPdypWXY_ROr0ZfCV-fAgau5yDemA19CV

BRX Do-more PLCs - Motion Control & High Speed Inputs
  • Video
    BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Config & JOG from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Dynamic Motion from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Limits from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Trapezoid Moves from AutomationDirect
  • Video
    BRX Do-more CTRIO2 Motion Using Encoders from AutomationDirect
BRX Do-more PLCs - Hardware
  • Video
    How To Sense Temperature with a Do-more PLC from AutomationDirect
  • Video
    How To Detect Objects with an AutomationDirect Do-more PLC
  • Video
    AC Motor On/Off with Do-more PLC Part 1 from AutomationDirect
  • Video
    AC Motor On/Off with Do-more PLC Part 2 from AutomationDirect
  • Video
    How to Sense Distance with an AutomationDirect Do-more PLC