AutomationDirect
Search
Login | Register
Accounts & Orders
Cart
2
$142.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...Loading...

Your Account

Account Home

Checkout   $142.50
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
> Pneumatic Components
  •   Shop  
  •   Overview  
  •   In Depth  
NITRA Pneumatics Home
 
Air Prep
Air Prep Basics Filters Regulators Lubricators
Valves
Valve Sizing Valve Selection Ports and Ways 2 vs. 3 Position Valves Pneumatic Automation Link (PAL) Frequently Asked Questions About Valves
Cylinders
Cylinder Overview Cylinder Types Cylinder Size & Force Cylinder Speed Cylinder Mounting Cylinder FAQ Cross reference another brand to NITRA All About Cylinder Switches
Fittings, Tubing & More
Types of Fittings Thread Sizes Explained Special Purpose Fittings Tubing/Hoses
Tools and Tips
Air Consumption Calculator Understanding Circuit Symbols Improving Energy Efficiency PAL Controller Configurator

Valve Selection

There are many factors that contribute to the performance of a pneumatic system. Some of these factors are: quantity and type of fittings leading to the cylinder, tube length and capacity, cylinder operating load, and air pressure. The following chart allows a look-up of the resulting cylinder speed in seconds for a given valve Cv and cylinder diameter. The sizing table below relates various AutomationDirect air valves to cylinder bore sizes between 7⁄16" and 4". The cylinder operating speed resulting from the use of each valve/cylinder combination are shown in the chart:

Enter Stroke Distance (in)

Select Pressure Drop Across Valve¹:




Select Inlet Pressure:

Select Air Temperature (F°):
Select Atmospheric Pressure (PSI):
Theoretical time (in seconds) required to make a    inch stroke
Valve Series Cv Cylinder Bore Sizes (in inches)
7/16 9/16 3/4 7/8 1 1/16 1 1/4 1 1/2 2 2.5 3 3 1/4 4
BVS series  0.02
0.05*
AVP series 0.051
AVS series 0.67
0.78
0.89
1.0
1.39-1.40
1.67-1.68
CMV series  0.1
0.2
0.5
0.65
1.0
1.2
CVR series  0.89
5.29

NA = Not Available. BVS valves with Cv of 0.05 can only operate at or below 30PSI; some other BVS valves are only rated for 90PSI  (please double-check the actual ratings if using high inlet pressures)

NS = Not Suitable. Valve/cylinder combinations that result in low theoretical speeds will likely result in jerky or lurching motion.

VF = Very Fast. Predicting theoretical speeds is not practical beyond certain limits (see note below). Other "fast" speeds that ARE shown should be taken with a grain of salt (see note below).

¹ The pressure drop shown is the DROP ACROSS THE VALVE ONLY, see note below. In practice, you can not choose ΔP (pressure drop) - the pressure drop of a given system is dependent on many things.

NOTE: This chart does not take into account tubing diameter or length, number or size of fittings and orifices, size or weight of the load, etc. You may need to factor in these (and other) values to determine the actual duration of a stroke. There are also practical limits to how fast a cylinder can physically operate.


General Rules of thumb for Fast Cylinder Action

The first general rule of thumb is choose a cylinder which will allow for at least 25% more force than what is required. For extremely fast operations, choose a cylinder which will allow for 50% more force than what is required. This will leave 25% or 50% of inlet pressure to satisfy system losses.

The second rule of thumb is to select a directional control valve which has the same port size as the cylinder which it will be operating. For large valves, internal flow capacity is typically the same or greater than the capacity of the intended connection fittings. On smaller valves, the internal flow capacity is typically much less than that of the connection fittings. But always be sure to check the valves flow rate, and do not rely solely on the port size.

Lastly: use large diameter tubing (relative to cylinder bore), keep the tubing length as short as possible and use as few fittings as possible.

Achieving a Specific Speed

If a specific cylinder speed is desired, it's advisable to size the valve, tubing, fittings, and cylinder for a faster stroke. And then use flow control valves to slow the cylinder down to the desired speed. If extremely fast action is desired, some trial and error testing will probably be required. Consider the use of cushioned cylinders to prolong the life of the components in high speed systems.

More about CV calculations here.

More about cylinder speed here.

 

Here are links to the various pneumatic valves currently sold by AutomationDirect:

Solenoid Valves
Solenoid Valves
Manifolds & Bases
Manifolds & Bases
Control Interfaces
Control Interfaces
I/O Modules
I/O Modules
Solenoid Valve Accessories
Solenoid Valve Accessories