AutomationDirect
Login | Register
Accounts & Orders
Cart
3
$76.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $76.00
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
Filter Results Clear All
You've selected:
> Pneumatic Components
  •   Shop  
  •   Overview  
  •   In Depth  
Home
 
Air Prep
Air Prep Basics Filters Regulators Lubricators
Valves
Valve Selection Ports and Ways 2 vs. 3 Position Valves Pneumatic Automation Link (PAL) Frequently Asked Questions About Valves
Actuators
Actuator Overview Actuator Types Cylinder Size & Force Cylinder Speed Cylinder Mounting Actuator FAQ All About Cylinder Switches
Fittings, Tubing & More
Types of Fittings Thread Sizes Explained Special Purpose Fittings Tubing/Hoses
Tools and Tips
Air Consumption Calculator Understanding Circuit Symbols Improving Energy Efficiency PAL Controller Configurator

Thread Sizes

Threaded fittings are used extensively to facilitate the connection of components, tubing and hose that make up all pneumatic systems. The different thread types and sizes can be confusing.

Thread Standards

Pipe thread and tubing OD are two completely different things. A 1/4” tube fitting doesn't necessarily have a 1/4” threaded connection at the opposite end, you will need to specify both. There are several standard pipe threads including:

  • NPT (National Pipe Taper)
  • BSPT (British Std Pipe Taper)
  • BSPP (British Std Pipe Parallel)
Diagram showing cross section of tapered thread vs straight thread

Tapered vs Straight Thread Types
(cross-section)

NPT

NPT is the most commonly used in the U.S. and has a tapered thread. Thread standards should never be mixed on a machine, as a BSPT male thread fitting won’t mate correctly with a NPT female thread fitting (or vise versa). Although they may screw together, the thread angle and shape are different and won’t create a proper seal.

NPT can be referenced multiple ways. MNPT, MPT and NPT(M) all mean the fitting has male threads and uses the NPT standard. Female thread is labeled in a similar fashion, but with an F instead of an M. NPT fittings require thread sealant when installed, such as Teflon tape, but many fittings are provided with sealant already applied from the factory.

NTP threads all have an angle of 60 degrees and the same shape (flat peaks and valleys)

BSP

BSPT is sometimes called R-thread or Rc and is most commonly used in Europe, but is also sometimes used in the U.S. and Canada. BSPT fittings require thread sealant when installed, such as Teflon tape, or pre-applied sealant may be supplied on the fitting.

BSPP, also called G-thread or Rp, is less common, and a straight thread, but sometimes needed to connect certain standardized components. BSPP threads don’t require thread sealant since they have an o-ring for sealing.

Both type of BSP threads (BSPT and BSPP) have the same 55 degree thread angle,
with rounded peaks and valleys.

Thread Dimensions
Pipe size NPT
(Tapered)
BSPT (R-thread)
(Tapered)
BSPP (G-thread)
(Parallel)
OD (in) TPI OD (in) TPI OD (in) TPI
1/8" 0.405 27 0.383 28 0.383 28
1/4" 0.540 18 0.518 19 0.518 19
3/8" 0.675 18 0.656 19 0.656 19
1/2" 0.840 14 0.825 14 0.825 14
3/4" 1.050 14 1.041 14 1.041 14
1" 1.315 11.5 1.309 11 1.309 11
1-1/4" 1.660 11.5 1.650 11 1.650 11
1-1/2" 1.900 11.5 1.882 11 1.882 11
2" 2.375 11.5 2.347 11 2.347 11

Verify fitting sizes using the OD of the pipe and the Threads per Inch (TPI).
(if working with female threads, the ID of the hole will be slightly smaller that the OD values shown)


Shop for Fittings

Fittings
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info