AutomationDirect
Login | Register
Accounts & Orders
Cart
2
$327.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $327.00
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
Filter Results Clear All
You've selected:
> Pneumatic Components
  •   Shop  
  •   Overview  
  •   In Depth  
Home
 
Air Prep
Air Prep Basics Filters Regulators Lubricators
Valves
Valve Selection Ports and Ways 2 vs. 3 Position Valves Pneumatic Automation Link (PAL) Frequently Asked Questions About Valves
Actuators
Actuator Overview Actuator Types Cylinder Size & Force Cylinder Speed Cylinder Mounting Actuator FAQ All About Cylinder Switches
Fittings, Tubing & More
Types of Fittings Thread Sizes Explained Special Purpose Fittings Tubing/Hoses
Tools and Tips
Air Consumption Calculator Understanding Circuit Symbols Improving Energy Efficiency PAL Controller Configurator

Cylinder Sizing & Force

Bore Dia. & Cylinder Area
Bore Dia: Cylinder
Area
(Sq. in.)
7/16" 0.150
9/16" 0.249
3/4" 0.442
7/8" 0.601
1-1/16" 0.887
1-1/4" 1.23
1-1/2" 1.77
2" 3.14
2-1/2" 4.91
3" 7.07
3-1/4" 8.30
4" 12.57
5" 19.64
6" 28.27
8" 50.27
10" 78.54
12" 113.10

Cylinder Sizing

The equations below & chart at right show the relationship between the force required to move a load, the pressure available and the required cylinder bore size. Always factor in 25% more force than actually required to overcome friction, pressure drop, and other factors.

Given:
Pressure (PSI) = Force(lbs) รท Area(sq-in)
Piston Area = π × r²
Cylinder Bore (in) = 2 × r
Therefore:
P = F ÷ (π × (B ÷ 2)²)

And solving for B:

Where:

F = Force Required, the estimated force needed to move the load (lbs)
P = Air Pressure, the nominal air pressure of the pneumatic system (PSI)

Interactive Cylinder Bore Calculator:

Minimum Bore Required (inches) = 
  Bore
 = 
4 ×   Enter Force Required (lbs) (include 25% cushion)

π ×   Select System Pressure
Next largest cylinder available:
Next largest metric cylinder:

Example:

Given an estimated force required of 900lbs (including the 25% overage for friction, pressure drop, etc.) and that the system will operate at 80PSI:

  • The Required Piston Area = 900 lbs ÷ 80 lbs/in2 = 11.25 in2.
  • Divide 11.25 by π, take the square root to get r, and note that the bore (dia) must be at least 3.78 inches.
  • From the chart, the next largest cylinder diameter is 4". Use a 4" cylinder.


Cylinder Force

The force a cylinder can apply during extension is a simple calculation (the inverse of the above formula): the effective surface area of the cylinder's piston × the differential pressure. For example: a 4" cylinder has a surface area of 12.57 square in. (πr²). If that cylinder is extended with 100 PSI of air pressure, it can supply a force of 1257 pounds.

Factoring in the Rod

When retracting a double acting cylinder, the cylinder rod blocks a portion of the effective surface area. If that same 4" cylinder has a 1" rod, the effective surface area is reduced to 11.78 sq. in. and it can only supply 1178 pounds of force while retracting (given the same 100 PSI differential pressure).The following chart shows the available force (in pounds) for both extension and retraction. White rows show extension force, which takes advantage of the full piston area. Grey rows show retraction forces with the rod diameter taken into account.

Spring Return

If you choose a cylinder with spring return, be sure to factor in the additional force needed to overcome the spring during extension.

Differential Pressure

Pressure in the above equations represents differential pressure across the two cylinder ports and assumes that the back pressure of the cylinder is negligible. In practice, the air supply line must supply another 5% of pressure to make up for cylinder loss, and must supply 25-50% additional pressure to make up for flow losses in lines and valving so the cylinder will have sufficient travel speed.

Systems should always be designed with calculated forces at least 25% above the actual requirements.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info