AutomationDirect
Login | Register
Accounts & Orders
Cart
1
$9.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $9.50
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
Filter Results Clear All
You've selected:
> Pneumatic Components
  •   Shop  
  •   Overview  
  •   In Depth  
Home
 
Air Prep
Air Prep Basics Filters Regulators Lubricators
Valves
Valve Selection Ports and Ways 2 vs. 3 Position Valves Pneumatic Automation Link (PAL) Frequently Asked Questions About Valves
Actuators
Actuator Overview Actuator Types Cylinder Size & Force Cylinder Speed Cylinder Mounting Actuator FAQ All About Cylinder Switches
Fittings, Tubing & More
Types of Fittings Thread Sizes Explained Special Purpose Fittings Tubing/Hoses
Tools and Tips
Air Consumption Calculator Understanding Circuit Symbols Improving Energy Efficiency PAL Controller Configurator

Understanding Circuit Symbols

Directional air control valves are the building blocks of pneumatic control. Symbols representing these valves provide a wealth of information about the valve they represent. Symbols show the methods of actuation, the number of positions, the flow paths and the number of ports. Here is a brief breakdown of how to read a symbol:

Every valve symbol has multiple parts (see figure below). The Actuators are the mechanisms which cause the valve to shift from one position to another. The Position and Flow Boxes indicate how the valve functions. Every valve has at least two positions (learn more) and each position has one or more flow paths, thus every valve symbol has at least two Flow Boxes to describe those paths.

Position and Flow Boxes

The number of position and flow boxes that make up a valve symbol indicate the number of positions the valve has. Flow is indicated by the arrows in each box. These arrows represent the flow paths the valve has when it is in that position.

Valve Symbol - 2 position - 5 port
2 Position, Lever Actuated, Spring Return Valve
Valve diagram - Interactive 2 pos 5 port
Interactive Demo (Push button to actuate lever)

Actuators

The box next to the 'active' actuator always shows the current flow path(s) of the valve. In the example above, when the lever is not activated, the spring actuator (right side) is controlling the valve, and the box adjacent to the spring shows the flow path. When the lever is actuated, the box next to the lever shows the flow path of the valve. A valve can only be in one "Position" at a given time.

In the example below (a three position valve), the "spring return" actuators on both sides return the valve to the center position but only IF neither of the solenoids is active:

Interactive Valve Demo - 3 position - 5 port
3 Position, Double Solenoid Actuated, Spring Return Valve

With this three position valve, the center position shows the flow path when neither actuator is active, and the springs are holding the valve in the center position). In this fairly common example, the center box indicates that there will be no air flow (i.e. the cylinder will 'hold position') unless one of the two actuators is active. This can be used to "bump" or "inch" a cylinder incrementally along its extension or retraction stroke for various purposes.

Ports

The number of ports is shown by the number of end points in a given box. Count only the ports in one flow box per symbol (the other boxes just show different states of the same valve). In the example at right, there are a total of 5 ports. Learn more about the number of ports here. NOTE: Sometimes a port (usually an exhaust port) goes directly to atmosphere and there is no mechanical means for attachment of silencers, flow control valves, or any other accessories. To indicate this (in some flow diagrams), ports with attachment capability will have a short line extending beyond the box (as shown on ports 1, 2, & 4), while the ports you cannot attach to will not have the external line segment (ports 3 & 5 in this example).

Ports vs "Ways"

Valves are also refered to by the number of "ways" that air can enter or exit the valve. In most situations the number of ports and ways are the same for a given valve, but take a look at the 3 position example above. It has five ports, but it is considered a 4 way valve because two of the ports share the same exhaust function. This is a holdover from hydraulics - where the two exhaust paths are joined (internally to the valve), so that only one exhaust port is required, and only one return line is required to get the hydraulic oil back to the storage tank for re-use. The single return port (exhaust) is only counted as a single "way". In the case of our pneumatic valve (above) with similar functionality, the separate exhaust ports are created for mechanical simplicity (and as a cost saving measure), but they are not considered distinct "ways". The symbols above detail many of the ports, ways, and positions of common pneumatic valves. The specification for "ways" can be somewhat tricky; analyzing the circuit symbols is a better method for verifying that a given valve offers the required functionality.




Common Symbols, Descriptions, and CAD Downloads

Valve Symbols, Flow Paths and Ports   Actuator Symbols
2 position, 2 way, 2 ported 2 position, 2 way, 2 ported Download a DXF version of this symbol   Manual Manual Download a DXF version of this symbol
2 position, 3 way, 3 ported 2 position, 3 way, 3 ported Download a DXF version of this symbol   Push Button Push Button Download a DXF version of this symbol
2 position, 4 way, 4 ported 2 position, 4 way, 4 ported Download a DXF version of this symbol   Lever Lever Download a DXF version of this symbol
3 position, 4 way, 4 ported, Center Closed 3 position, 4 way, 4 ported, Center Closed Download a DXF version of this symbol   Foot Operated Foot Operated Download a DXF version of this symbol
2 position, 4 way, 5 ported 2 position, 4 way, 5 ported Download a DXF version of this symbol   Mechanical Mechanical Download a DXF version of this symbol
3 position, 4 way, 5 ported 3 position, 4 way, 5 ported Download a DXF version of this symbol   Detent Detent Download a DXF version of this symbol
Simple Pneumatic Valves   Spring Spring Download a DXF version of this symbol
Check Valve Check Valve Download a DXF version of this symbol   Solenoid Solenoid Download a DXF version of this symbol
Flow Control, 1 direction Flow Control, 1 direction Download a DXF version of this symbol   Internal Pilot Internal Pilot Download a DXF version of this symbol
Relief Valve Relief Valve Download a DXF version of this symbol   External Pilot External Pilot Download a DXF version of this symbol
Lines   Piloted Solenoid with Manual Override Piloted Solenoid with Manual Override Download a DXF version of this symbol
Main Line Main Line   Piloted Solenoid and Manual Override Piloted Solenoid and Manual Override Download a DXF version of this symbol
Pilot Line Pilot Line   Lever with Spring Lever with Spring Download a DXF version of this symbol
Exhaust Line or Control Line Exhaust Line or Control Line   Solenoid with Spring Return Solenoid with Spring Return Download a DXF version of this symbol
Lines Crossing Lines Crossing
Lines Connecting Lines Connecting
Miscellaneous
Accumulator Accumulator Download a DXF version of this symbol Differential Pressure Differential Pressure Download a DXF version of this symbol
Air Dryer Air Dryer Download a DXF version of this symbol Direction of Flow Direction of Flow Download a DXF version of this symbol
Air Motor (One Direction Flow) Air Motor (One Direction Flow) Download a DXF version of this symbol Lubricator Lubricator Download a DXF version of this symbol
Air Motor (Two Direction Flow) Air Motor (Two Direction Flow) Download a DXF version of this symbol Filter Filter and Regulators Download a DXF version of this symbol
Check Valve (Spring Loaded) Check Valve (Spring Loaded) Download a DXF version of this symbol Filter (Automatic Drain) Filter (Automatic Drain) Download a DXF version of this symbol
Compressor Compressor Download a DXF version of this symbol Filter (Manual Drain) Filter (Manual Drain) Download a DXF version of this symbol
Cylinder (Spring Return) Cylinder (Spring Return) Download a DXF version of this symbol Fixed Restriction Fixed Restriction Download a DXF version of this symbol
Cylinder Double Acting Cylinder Double Acting (Double Rod) Download a DXF version of this symbol Flow Meter Flow Meter Download a DXF version of this symbol
Cylinder Double Acting
(Double Rod)
Cylinder Double Acting (Double Rod) Download a DXF version of this symbol
Cylinder Double Acting (Single Fixed Cushion) Cylinder Double Acting (Single fixed cushion) Download a DXF version of this symbol
Cylinder Double Acting (Two Adjustable Cushions) Cylinder Double Acting (Two Adjustable Cushions) Download a DXF version of this symbol
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info