https://www.automationdirect.com/do-more?utm_source=HX1th57oYeU&utm_medium=VideoTeamDescription (VID-DD-0020) - This video gives basic information on Using the TMR "Timer" instruction in the Do-more Designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0
**Please check our website for our most up-to-date product pricing and availability.
Hide Transcript
View Transcript
This is a multi-scan instruction, because
it takes multiple scans to complete, it cannot be used in either Subroutines or Interrupt
Service Routines. It can used in Programs and under special
circumstances can it be used in Stages inside of a Program or in Tasks. See the help topic “Instruction Set Chart”
for more information. This instruction has only one power rail that
doubles for both Enable and Reset. If the rung is true the timer will be enabled. If it is false the timer will be reset. When the timer accumulator is greater or equal
to the preset the timer done bit will turn on.
Do-more & BRX PLCs - Do-more Designer Software & Programming