=
 Cookies are not enabled on your browser.
    Cookies are not enabled on your browser.




In a typical motion control system, there are three basic components: the controller, the drive (sometimes referred to as an amplifier), and the motor. The path planning or trajectory calculations are performed in the controller, which sends command signals to the drive, which in turn applies the necessary voltage and current to the motor, resulting in the desired motion. The most common command signal type when using PLC-based control is the pulse train also referred to as "pulse and direction". Pulse and direction signals provide an inexpensive, noise-free (digital) method for precision motion control. While typically limited to a few axes of control and where coordination between axes is not necessary, PLC controllers with pulse and direction capability are an excellent fit for many motion applications.
Pulse and direction signals are typically square waves that alternate between a high and low voltage at a determined frequency. With this square wave, the PLC can ultimately control:
By controlling the frequency and polarity of the pulses, the PLC (through a drive) can precisely control the motor/actuator's position and speed.
Pulse and direction control is used throughout industrial automation for numerous types of movement, including those involving:
 
    
         Safe &
                Secure
   Safe &
                Secure
             
                
        Voted #1 mid-sized employer in Atlanta
        Check out our 
        
            job openings
        
    
 Updating...
 Updating...