Install the iOS or Android mobile app from the appropriate app store.
Open the mobile app and create your account.
Create a device profile from the Web app. The device profile defines the Modbus device and variables, and local I/O, to be monitored
and logged. You can create a device profile from your account at www.pocketportal.com, or you can use the default profile for now and
create a profile after the new Pocket Portal is connected to your account. Profile creation is a one-time activity and the same profile
can be applied to multiple devices.
3. Install and connect the Pocket Portal to your account
Install and properly wire the Pocket Portal IIoT bridge, making sure the device is powered ON and the PWR LED on the device is SOLID
GREEN.
In the mobile app, select "Add device" to start registration and provisioning of the Pocket Portal device to your account.
You need to have physical access to the Pocket Portal for registration.
Follow the steps provided in the mobile app to complete the process.
4. Choose your subscription
SE-PP500K for 200,000 data samples per month with email alerts and notification
SE-PP5M for 1 million data samples per month with email alerts and notification