DURApulse GS4 VFD Built-in PLC Control Part 1 from AutomationDirect


Related Products

GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-47P5
GS4-47P5 Thumbnail
GS4-4010
GS4-4010 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=ypqK1s7y3IA&utm_medium=VideoTeamDescription

(VID-DR-0035)

In this video, we demonstrate the GS4 drive's built-in PLC to control the drives Run, Stop and Frequency.

Online Support Page: https://community.automationdirect.com/s/?utm_source=ypqK1s7y3IA&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Let’s walk through this example in the examples folder which set’s the drive’s frequency, acceleration and deceleration times, Enables the drive, issues the run/stop, and forward and reverse commands. It also does a drive fault reset. I moved my menu buttons to make more room on the screen so don’t be surprised if my screen looks different than yours. If you don’t see the comments, then make sure the show comments button is on. Rung 0 says when we set the internal general purpose M1 bit, set the frequency and ramp times. I can never remember which register is which, so let’s right click and edit the register comments. D50 is the frequency with two implied decimal places. D52 is the acceleration with two decimal places and D53 is the Deceleration also with two implied decimal places. Ahh, that’s much better. Of course, these D registers will need to be pre-loaded with these values before running this command. In this example, we’ll do that with the register monitor when we go on line with the drive. That rung used 8 of our 10,000 steps, so the next rung starts at step 8 where we use input X0 to enable the drive. That’s not the RUN STOP Command – it just enables the drive’s outputs. The comment says “power On” – think of that as applying power to the output stage of the drive. The row comment reminds us that X0 is what the drive refers to as the Forward input and use that input as the drive enable by enabling this special function register output coil. The next row uses the drives Reverse input as the RUN/STOP control by enabling this special function register. The next rung uses this input X2 to control forward and reverse via this special function register and this rung uses X3 to reset a fault. Lets select the com port that our USB to RS485 adapter is plugged into … these are the correct comm parameters and we do want RTU. Perfect. Let’s write this program to the drive, go online, and open the monitor window. Let’s add the M1 Control Register and the Frequency, Acceleration and deceleration registers. Let’s set the drive’s frequency at 60 hertz – remember the two implied decimal places – and the ramp times to be 5 hz. Again, with two implied decimal places. Let’s toggle M1 to set the frequency and ramp times. I have some switches connected to the drives inputs, so I’ll enable X0 to power up the drives output, Set the forward switch and set the run switch. And sure enough, the drive ramps up to speed over 5 seconds. Perfect. Well ... That’s really all there is to it … BUT … there are a number of things you need to know to get the most out of your GS4 drive when controlling it from the built in PLC. We’ll cover all of that in Part 2. Click here to learn more about the GS4 drives. Click here to learn about AutomationDirect’s free support options. And click here to subscribe to AutomationDirect’s YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > DURApulse GS4 VFD Built-in PLC Control Part 1 from AutomationDirect