https://www.automationdirect.com/motor-controls (VID-MS-0004)
How to build a Combination Manual Motor Starter, Starter Assembly
building a combination manual motor started using Fuji components offered by automationDirect I'm carry Scheiber and this is part 3 assembling the combination motor starter the only tools that are required for assembly are a few screwdrivers step 1 start by mounting the manual motor starter to the baseplate while holding the baseplate in one hand slip the din rail clip of the manual motor starter onto the mounting rail then press it onto the rail until it snaps into position if preferred screws can be installed for a tighter mount to remove the manual motor starter simply insert a screwdriver into the din rail clip release tab and pry the tab away from the manual motor starter the manual motor starter will pop away from the base plate mount step to the link module links l1 l2 and l3 between the manual motor starter and the contactor verify that the contacts are in the open position laying the base plate on a table with the manual motor starter to the right position the link module with the label facing towards you simply slide the poles of the link module into the contacts then tighten the contact screws step 3 as you can see the coil is located on the top of the contactor this could be a problem when trying to connect the contactor to the link module the solution is to remove and rotate the front of the body so the coil is positioned at the bottom of the contactor using a Philips screwdriver remove the two screws that secure the front to the back of the body separate the front from the back of the body turn the front of the body 180 degrees and attach it back to the body then remount with the screws making sure that no foreign matter enters the interior of the magnetic contactor during the removal and remounting procedure this procedure is for the 55 mm sighs contactors SCE 1 through SC - III for the smaller 45 millimeter SC d 0 2 through SC d 0 5 contactors simply remove the arc chamber cover by inserting a flat blade screwdriver between the cover and the terminal screw lift the arc chamber to remove it and rotate 180 degrees align the cover with the top and bottom terminals and press firmly to attach to attach a contactor to the link module verify that the contacts are open then slide the contactor onto the link module poles next tighten the two mounting screws located at opposite corners of the contactor then tighten the three contact screws step 4 mount the assembled unit into the panel for wiring we are now ready to connect the wiring
Voted #1 mid-sized employer in Atlanta
Check out our
job openings