DURApulse GS4 VFD Sleep Mode Hardware Setup & Configuration from AutomationDirect


Related Products

GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-47P5
GS4-47P5 Thumbnail
GS4-4010
GS4-4010 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=wdciqTJctKw&utm_medium=VideoTeamDescription

(VID-DR-0063)

Learn how to setup and use all the various sleep modes the GS4 provides with this series of videos:
GS4 VFD Sleep Mode Video List
1. Intro and Overview
2. Hardware Setup and Configuration
3. Sleep Mode 1: Sensor Feedback
4. Sleep Mode 2: PID using PID Cmd Freq to control Sleep
5. Sleep Mode 3: PID Forward Acting uses PV to control sleep
6. Sleep Mode 3: PID Reverse Acting

uses PV to control sleep.

Online Support Page: https://community.automationdirect.com/s/?utm_source=wdciqTJctKw&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

This video walks through the hardware and basic drive configuration used in all of the sleep mode video tutorials. We have a reservoir feeding this centrifugal pump. The pump is driven by a 2-pole jet pump motor and a GS4 Drive. The pump fills the tank. You can ignore all of this stuff – it is used in other video tutorials. Up here we have an ultrasonic distance sensor that provides a 4-20mA signal back to the GS4 drive. The sensor can be setup to provide either 20mA down here or, 4mA down here.. That signal will be used differently by the various sleep modes. We can adjust the demand on the tank via this valve. This is my high-tech reservoir. We spare no expense for you guys. Notice the check valve here which prevents water from flowing backwards. The ultrasonic sensor is wired into analog input 1 and I wired some potentiometers into analog ports 2 and 3 – you don’t need these to do sleep mode. You’ll see why I did it in just a minute. Before doing anything in each video, I reset the drive to factory default so you can follow along from a known configuration. These are the motor parameters required for this test setup. Of course, yours will probably be different. Since I’m using a 3600 rpm Jet Pump Motor, I had to set the poles parameter to two BEFORE the drive would let me increase the rpm parameter. I love that the GS4 Drive won’t let me mess that up. I also set the ramps to some small values to help smooth out transitions and prevent overload faults when the motor is woken up and shut down. The remote frequency source is controlled by the analog input, and the local frequency source is controlled by the keypad in case we need to do some manual testing. Parameter 4.02 tells remote mode to use the ultrasonic sensor on analog input 1. The ultrasonic sensor is sending us 4-20mAmps, so we set analog input 1 for current mode and make sure the switch on the terminal board is also set to current. Analog input 2 is a potentiometer so we need to set it for voltage and make sure it’s switch is set for voltage. Analog input 3 is also a potentiometer, but since it defaults to voltage there is nothing to do for that one. The cool thing about connecting potentiometers to analog inputs is we can see them in GSFOT2’s Scope function to mark things like the sleep and wake levels. I also added a Styrofoam float in the water tank with some LEDs on it to make it easier for you to see the water level rise and fall. The sleep mode parameters will be set differently in each video, so we won’t go over those here. That’s it for the hardware setup. Check out the other videos in this series to see all the different ways the GS4 drive can implement sleep mode. Click here to learn more about the GS4 Drive. Click here to learn about AutomationDirect’s free award-winning support options and click here to subscribe to AutomationDirect’s YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > DURApulse GS4 VFD Sleep Mode Hardware Setup & Configuration from AutomationDirect