DURApulse GS4 VFD Built-in PLC Quick Start Part 1 from AutomationDirect


Related Products

GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-47P5
GS4-47P5 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail
GS4-4010
GS4-4010 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=w4jMRp_vVZg&utm_medium=VideoTeamDescription

(VID-DR-0033)

Learn how to use the PLC to access the GS4 Variable Frequency Drive parameters in this video tutorial from AutomationDirect.

Online Support Page: https://community.automationdirect.com/s/?utm_source=w4jMRp_vVZg&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Every GS4 Variable Frequency Drive has a built in PLC that's perfect for those times when you need just a little extra logic. For example, suppose you have an irrigation system and you just want to run the pump a couple times each day. All you need to do that is a timer and a little bit of logic. The PLC that’s built into the GS4 drive is perfect for that. Or, suppose you have a conveyor that you need to stop automatically so you can swap out containers? All you need for that is a couple inputs and a little bit of logic. Again, the built in PLC is perfect for these kinds of applications. Since you no longer need an external controller, power supply, wiring or enclosure, you get your system up and running quicker, have lower maintenance costs, save on control system foot print, save on reduced spares inventory, and will have an all-around less expensive and more reliable system. BUT, because you have both a PLC and a Drive in the same box, you need to be very aware of a couple things. While the drive comes with a PLC built in, it comes from the factory with the PLC disabled. And for all practical purposes, it’s not there until you enable it. That means you can’t even talk to it or set it up until you enable it. How do you enable it? Easy – just go to the keypad, hit the MENU key, scroll down to PLC and select either RUN or STOP. Either of those “enables” the PLC part of the drive. Once the PLC is not disabled you now have something new to keep in mind. The GS4 Drive has built in analog and digital I/O and more I/O available via expansion modules. When the PLC is enabled you now have two different devices trying to access the same I/O. Which one gets control of the I/O? The answer is: The PLC AWLAYS wins IF the PLC is not disabled AND the PLC uses the I/O in its ladder code. So, for example, if the PLC has Ouput3 in the ladder code – then the drive’s corresponding digital output won’t function – even if you set it up in the drive to do something. If you disable the PLC, then the drive will regain control of that digital output, until you re-enable the PLC again. Keep an eye on the various mask parameters – they will show you graphically which I/O are owned by the PLC. For example, here is the digital output mask and we see that that output three we used in the ladder code is shown as being owned by the PLC. And finally, when trying to remotely communicate with the two devices, remember that the Drive and the PLC have different addresses which you can change. So be careful not to set them to the same address. They come from the factory as address 1 and 2. Why do they have different addresses? Because they both use the SAME RS485 serial port for communications! There are two modular jacks, but they are connected in parallel so you can Daisey chain drives. Of course, you can only have one master device connected and since GSoft2 and GSLogic are both masters – that means you can only have one running at any time. That is, you can only program the PLC OR Configure the drive – you can’t do both at the same time because they will try to talk over each other and mess up everybody’s communications. OK, That’s enough background stuff. Join us in Part II of this Quick Start we’ll do a live demo to show you how to get up and running quickly. Click here to learn more about the GS4 Drive. Click here to learn more about AutomationDirect’s free support options and click here to subscribe to AutomationDirect’s YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > DURApulse GS4 VFD Built-in PLC Quick Start Part 1 from AutomationDirect