https://www.automationdirect.com/sensors
(VID-SEN-0007)
Wenglor Contrast sensors from Automationdirect are ideal print mark detection sensors. Contrast sensors determine contrast by sensing reflected white light to detect the difference in the wavelength of the reflected light between the mark and background. With detection ranges up to 40mm, these Wenglor sensors have IP67 rated plastic housings and quick-disconnect termination, offer teach-in sensitivity adjustment, and a choice of PNP or NPN output.
Industrial applications include packaging lines, beverage and bottling lines, paper and printing machinery, and ceramics printing.
Welcome to Kickstart where you get to see new products here at AutomationDirect. We are excited to show you the new wenglor brand Contrast sensors that AutomationDirect is now offering. There are 6 new contrast sensors in this launch as well as new mounting brackets. So, if you want to learn more, keep watching! Contrast sensors determine contrast by sensing reflected white light to detect the difference in the wavelength of the reflected light between the mark and background. Contrast sensors also known as print mark detection sensors are used in applications like packaging lines, beverage and bottling applications, as well as paper and printing applications. These new Wenglor contrast sensors all operate on 10 to 30 volts DC and come in sensing ranges of 12 to 40mm distances depending on the sensor models. You can select from NPN or PNP models and they all have Teach In sensitivity adjustments. The OPT2024 and 25 models are normally open and require an M12, 4 pin quick disconnect cable. The OPT2026, 27, 28 and 29 models are normally open or normally closed and require an M12, 8 pin quick disconnect cable and the cable base connector can be rotated 270 degrees for mounting in confined spaces. You can find the specs for these new Wenglor contrast sensors on our website at: www.automationdirect.com And don't forget: we sell hundreds of models of sensors from proximity, photo, laser, ultrasonic and more. Don't for get to pick up a quick disconnect cable for your sensor, we sell hundreds of these as well. Check back with us often on AutomationDirects websites or on Youtube.com/Automationdirect for more Kickstart videos. If you are watching us on YouTube, please let us know what you think about these new Wenglor sensors or how you plan to use them in your application by dropping us a comment down below. Don't forget to hit the like button! Thanks for watching and we hope to see you again soon. If you have any questions about using AutomationDirect's sensing products, please contact AutomationDirect's free award-winning support team during regular business hours. They will be happy to help. Click on this short video to learn more about AutomationDirect's support options and click here to learn more or see more videos on our sensors. And be sure to click here to subscribe to our YouTube channel to be notified of new Videos.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings