WEG CFW300/320 VFD Display RPM from AutomationDirect


Related Products

CFW300A01P6S1NB20
CFW300A01P6S1NB20 Thumbnail
CFW300A06P0S1NB20
CFW300A06P0S1NB20 Thumbnail
CFW300A01P6S2NB20
CFW300A01P6S2NB20 Thumbnail
CFW300A02P6S2NB20
CFW300A02P6S2NB20 Thumbnail
CFW300A04P2S2NB20
CFW300A04P2S2NB20 Thumbnail
CFW300A06P0S2NB20
CFW300A06P0S2NB20 Thumbnail
CFW300A07P3S2NB20
CFW300A07P3S2NB20 Thumbnail
CFW300A01P6T2NB20
CFW300A01P6T2NB20 Thumbnail
CFW300A02P6T2NB20
CFW300A02P6T2NB20 Thumbnail
CFW300A04P2T2NB20
CFW300A04P2T2NB20 Thumbnail
CFW300A06P0T2NB20
CFW300A06P0T2NB20 Thumbnail
CFW300A07P3T2NB20
CFW300A07P3T2NB20 Thumbnail
CFW300B10P0B2DB20
CFW300B10P0B2DB20 Thumbnail
CFW300B15P2T2DB20
CFW300B15P2T2DB20 Thumbnail
CFW300-CRS232
CFW300-CRS232 Thumbnail
CFW300-CRS485
CFW300-CRS485 Thumbnail
CFW300-CUSB
CFW300-CUSB Thumbnail
CFW300-KHMIR
CFW300-KHMIR Thumbnail
CFW300-IODR
CFW300-IODR Thumbnail
CFW300-IOAR
CFW300-IOAR Thumbnail
CFW300-IOADR
CFW300-IOADR Thumbnail
CFW300-IOAENC
CFW300-IOAENC Thumbnail
CFW300-KFA-S1-S2
CFW300-KFA-S1-S2 Thumbnail
CFW300-KFB-S2
CFW300-KFB-S2 Thumbnail
CFW-WPS
CFW-WPS Thumbnail
CFW300-FAN-A
CFW300-FAN-A Thumbnail
CFW300-FAN-B
CFW300-FAN-B Thumbnail
CFW100A01P6S120G2
CFW100A01P6S120G2 Thumbnail
CFW100B02P6S120G2
CFW100B02P6S120G2 Thumbnail
CFW100A01P6S220G2
CFW100A01P6S220G2 Thumbnail
CFW100B02P6S220G2
CFW100B02P6S220G2 Thumbnail
CFW100C04P2S220G2
CFW100C04P2S220G2 Thumbnail
CFW320A01P6S1NB20
CFW320A01P6S1NB20 Thumbnail
CFW320A02P6S1NB20
CFW320A02P6S1NB20 Thumbnail
CFW320A04P2S1NB20
CFW320A04P2S1NB20 Thumbnail
CFW320A06P0S1NB20
CFW320A06P0S1NB20 Thumbnail
CFW320A01P6S2NB20
CFW320A01P6S2NB20 Thumbnail
CFW320A02P6S2NB20
CFW320A02P6S2NB20 Thumbnail
CFW320A04P2S2NB20
CFW320A04P2S2NB20 Thumbnail
CFW320A06P0S2NB20
CFW320A06P0S2NB20 Thumbnail
CFW320A07P3S2NB20
CFW320A07P3S2NB20 Thumbnail
CFW320A01P6T2NB20
CFW320A01P6T2NB20 Thumbnail
CFW320A02P6T2NB20
CFW320A02P6T2NB20 Thumbnail
CFW320A04P2T2NB20
CFW320A04P2T2NB20 Thumbnail
CFW320A06P0T2NB20
CFW320A06P0T2NB20 Thumbnail
CFW320A07P3T2NB20
CFW320A07P3T2NB20 Thumbnail
CFW320B10P0B2DB20
CFW320B10P0B2DB20 Thumbnail
CFW320B15P2T2DB20
CFW320B15P2T2DB20 Thumbnail
CFW320A01P1T4NB20
CFW320A01P1T4NB20 Thumbnail
CFW320A02P6T4NB20
CFW320A02P6T4NB20 Thumbnail
CFW320A03P5T4NB20
CFW320A03P5T4NB20 Thumbnail
CFW320A04P8T4NB20
CFW320A04P8T4NB20 Thumbnail
CFW320B07P6T4NB20
CFW320B07P6T4NB20 Thumbnail
CFW320C11P0T4NB20
CFW320C11P0T4NB20 Thumbnail
CFW320C14P0T4NB20
CFW320C14P0T4NB20 Thumbnail
CFW320B01P1T4DB20
CFW320B01P1T4DB20 Thumbnail
CFW320B02P6T4DB20
CFW320B02P6T4DB20 Thumbnail
CFW320B03P5T4DB20
CFW320B03P5T4DB20 Thumbnail
CFW320B04P8T4DB20
CFW320B04P8T4DB20 Thumbnail
CFW320B07P6T4DB20
CFW320B07P6T4DB20 Thumbnail
CFW320C11P0T4DB20
CFW320C11P0T4DB20 Thumbnail
CFW320C14P0T4DB20
CFW320C14P0T4DB20 Thumbnail


To learn more: https://www.AutomationDirect.com/drives?utm_source=mo840qswlQc&utm_medium=VideoTeamDescription

(VID-DR-0083)

Learn how to change the LCD display (aka HMI) to show RPM instead of Hertz on the WEG CFW300 or 320 Variable Frequency Drive in this brief tutorial. This is the best VFD, with a super low cost, but with high-end features like Dynamic Braking, Fire Mode, PID, 65,000A SCCR, Zero Stack footprint, Multi-Speed, etc and is even cULus listed!

Online Support Page: https://community.automationdirect.com/s/?utm_source=mo840qswlQc&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

By default, the WEG CFW300 drive displays the output frequency. Can we change it to display rpm? Sure! I’m going to use this free WEG programming software as a parameter lookup tool. It isn’t actually connected to the drive in this video. If we look at the 400 parameters, my motor is set up for a rated speed for 1720rpm at 60 Hz. So, to convert the displayed rpm we just scale the display to 1720 instead of 60. Parameter 208 is the display scaling factor. We see it defaults to 600, but parameter 210 moves the decimal point over one digit, so we end up with 60-point zero hertz on the display. And parameter 209 selects the units to be displayed. So, all we need to do is change parameter 208 to scale the display to 1720, change parameter 209 to show rpm and change parameter 210 to zero decimal places. It’s important to remember this only affects the motor frequency DISPLAYS. Everything else in the drive still uses hertz. For example, if we go to parameter 121 to enter a motor speed – it is still in Hz. So, let’s tell the drive to run at half speed which would be 30 Hz. And scroll back down to view the motor output speed in parameter 2. Now if we hit run, the drive ramps up to half speed which is 860rpm. Perfect. Notice that the speed reference in parameter 1 is also in rpm. Again, this scaling only affects those two parameters. Because it only affects the display, you can scale the display to whatever you want. Feet of conveyor per minute, the shaft rotation after a gear box, etc. You can change the units from hertz, rpm, volts, percent or just turn them off. These three parameters give you a lot of flexibility over what you can display on the LCD, so use it to your advantage to present a display that is in units that make sense for your application. Click here to learn more about the WEG CFW300 variable frequency drive. Click here to learn about AutomationDirect’s free award-winning support options and click here to subscribe to our YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > WEG CFW300/320 VFD Display RPM from AutomationDirect