To learn more: https://www.automationdirect.com/io-link?utm_source=mcQf3SBUOao&utm_medium=VideoTeamDescription
(VID-FD-0005)
IO-Link is a standardized protocol that enables easy connection of field devices such as sensors and actuators to a controller like a PLC. In this video series, AutomationDirect will demonstrate the use of an IO-Link network to connect a Productivity 2000 PLC to two representative field devices, using methods and resources that can be adapted to users' needs for implementation in their projects.
***Note: The Productivity Suite Task Library Integration File mentioned in this video NO LONGER contains the example Productivity project file shown in this video. The project file is not used or needed for integration as demonstrated here.
Online Support Page: https://community.automationdirect.com/s/contactsupport?utm_source=mcQf3SBUOao&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
This is the first in a 3-video series from AutomationDirect.com, “Using Productivity Line PLCs with IO-Link.” IO-Link is a standardized protocol that enables connection of field devices such as sensors and actuators to a controller, like a PLC. Two-way communication between the controller and a number of field devices is facilitated by an IO-Link Master. The controller is connected via an Ethernet network to the IO-Link Master, which then connects point to point to one or more intelligent field devices. In this example, we’ll set up communications through a Stride Basic IO-Link Master between an AutomationDirect Productivity 2000 PLC and two field devices: a Werma eSign stacklight and a Wenglor photo eye sensor. A quick overview of these components: The eSign stacklight is an advanced multi-tiered signal tower from Werma. With 15 independently configurable signal tiers and 10 selectable audio siren tones, the eSign provides maximum signaling flexibility. The Wenglor photoelectric sensor is a retroreflective model. If the beam is blocked and does not return to the emitter, the sensor’s output will change states. The Stride Basic IO-Link Master allows a PLC to connect with up to 8 IO-Link capable field devices with no complicated field wiring – simply plug the devices into the master’s 5-pin M12 ports. If not connecting to an IO-Link device, each of the M12 ports can handle 2 simple discrete IO points. On the other side, the Master is in dialogue with the PLC over an Ethernet IP connection, relaying device status, PLC commands, error reports, and system data back and forth between the PLC and each connected field device. The Productivity 2000 PLC (P2-550) needs no introduction. The powerful and versatile controller from AutomationDirect makes setting all of this up astonishingly easy with a freely downloadable configuration program available on our webstore at www.automationdirect.com: In the Shopping Categories field on the left of the screen, click Field I/O. Select IO-Link. Click IO-Link Masters. Select the Stride Basic IO-Link Master. Click Downloads. Click the download link for the Productivity Suite Task Library Integration File. Once the Productivity Suite Integration folder is downloaded, unzip and find inside these 5 items: • The Stride IO-Link Integration project is an example program for the Productivity demonstrating the use of various IO-Link components. • 2 EDS files – one for the Stride Basic IO-Link Master, the other for the Murrelektronik Premium IO-Link Master. • The AutomationDirect IO-Link.adtkl is the library containing the IO-Link program tasks we’ll use in this project. • The PDF “Using Productivity with IO-Link” covers some of the same setup information we’ll be discussing in these videos. In the next video, we’ll begin to look at the setup needed in the Productivity software to make this all work. Click here to see Video 2. Click here to check out AutomationDirect’s range of IO-Link capable products.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings