To learn more: https://www.automationdirect.com/productivity?utm_source=kdBvuCPzVTU&utm_medium=VideoTeamDescription
(VID-P3-0047)
This demo will show how easy it is to set up Implicit (connected) EtherNet/IP messaging between a Productivity series controller and an Advantech 6160EI Remote Relay module.
**Requires Productivity Suite Software 1.10.0.10 or later.
Online Support Page: https://community.automationdirect.com/s/?utm_source=kdBvuCPzVTU&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
in this video will skip all the introductory stuff and get ready to connecting the Adam 61-60 relay module to the productivity 3,000 using Ethernet IP protocol if you need more details on using it and I P on the productivity 3,000 check out these videos they provide a lot more background an introductory information we want to control the six relay outputs by simply putting bits and a 16-bit tag on the productivity 3,000 and then what the evening I P I O messaging copy that down to the Adam 61-60 in the background so we don't have to worry about it setting it up is just like setting up any other eating IP scanner on a productivity 3,000 he just double click on Harbor configuration and wreckage in her client over into this window you notice that the digital and analogue models didn't previous videos are already set up here and now we're gonna have this relay module went ahead and filled in all the usual tags: anything IP address and then down here always liked it I O messaging we need to create an input data rate the input array here just a dummy placeholder cuz the relay module a strictly in output only device go ahead with the one word expect to see right here or any output tab that's the important one we're gonna send that data four times a second the connection point on the oven tech devices 101 then when you create an output array with one 16-bit unsigned word and just a single car racing element in that array and of course we're gonna send that one element down to three lei device don't forget that on the about tech devices we need to include a status header and configuration data same thing as before let's create an array couldn't specify as a 60 min Thein Sein one element mr Katter said any data down with the configuration header give-and-take doesn't need it was click OK or text look good again I like to extend all my strengths they can handle any message that might come down the pike and there's a 61-60 relay output module let's go back in there click on that monitor button so we can create a data view that contains all these new tags we just created great we are said ready to go let's transfer that down to the controller and I was being the data views we see what's going on let's go find that new data view we created there to 61-60 here's our techs in the last example is doing some graphing on me get rid of that year ago SLA see this is our Relay output module let's go in the neighborhood click on that write this we were successful connection we are connected we did for the crackdown outta the device perfect all we're gonna do now is modify this output word to control the relays on the module for we do that let's go ahead convert this view over to binary I make it will be easier to see I currently have a light connected to the second bit which is the third digit here in the six-team that word such a turn on that relay we just that bit and sure enough the light turns on clear that that in the light turns off well that's all there is a setting up and using the Monte Kadam 61-60 relay module with the productivity 3,000 and Ethernet IP check out the other videos in the series for more tips on using get an IP with the productivity 3,000 and don't forget automation direct tech support is always free and you always talk to a live person here in the US within minutes please keep in mind that will support will be happy to help you with any productivity 3,000 even the IP questions you may have if you have any questions about the Avante tech devices you need to contact Yvonne tech support automation direct cell or support about tech devices performance post value thats productivity from automation direct
Voted #1 mid-sized employer in Atlanta
Check out our
job openings