• Purchase History Reports
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
DURApulse GS4 VFD Factory Reset from AutomationDirect


Related Products

GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-47P5
GS4-47P5 Thumbnail
GS4-4010
GS4-4010 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=h7WkA8Bn_8c&utm_medium=VideoTeamDescription

(VID-DR-0050)

Learn how to reset to factory default the drive parameters, the built-in PLC, the kWh display and the optional communication cards.

Online Support Page: https://community.automationdirect.com/s/?utm_source=h7WkA8Bn_8c&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

There are four things you can reset in a GS4 Drive. The Drive Parameters, the Drive’s built in PLC, the kWh display and the optional communications cards. Before resetting the Drive or the PLC, make sure the PLC is DISABLED. You don’t want it trying to control the drive while resetting the drive and you can’t reset the PLC while it is active. You will see the PLC status here on the main screen if it is enabled. If it is, go to the main menu, item 4 and select disable and press enter. The PLC can’t be in either RUN or STOP mode to be reset. It has to be disabled entirely. To reset the drive, go to parameter 9.08 and enter a 9 to reset to 50 hertz or 10 to reset to 60 hertz. Before I hit ENTER, a word of caution: If you created a password in parameter 8.07, then you will have to enter it in parameter 8.06 to be able to reset the Drive’s Parameters. If I press ENTER, I see an END which tells me all of the drives parameters were reset to factory default. If the reset didn’t work, you will get an error message on the screen. For most parameter entry operations it’s easy to miss that because they are both three letters and they both begin with the letter E. So, watch that closely when you are entering parameters. Fortunately, for the Reset operation, it’s hard to miss because the display also frantically flashes at you until you press the STOP button to clear the error. To reset the PLC, again make sure the PLC is NOT enabled. Then go to parameter 9.08 and select item 6. Again, if you see the END then the PLC is now reset. Setting Parameter 8.0 to a 41, will show the Kilowatt hours used by the drive in the user portion of the display. I can reset that by going to parameter 9.08 and entering a 5. To reset the communications cards, go to parameter 9.63 and enter a 1. This will reset the IP Addressing that was copied to the card from the Drive’s P9 parameters. The Drive’s P9 commands will still be in the drive, so you can simply copy them back to the Communications card after you reset itusing parameter 9.64 and entering a 2. All of this is super easy to do using the GSOFT2 app which you can download for free from the AutomationDirect website. Click here to learn more about the GS4 drive. Click here to learn about AutomationDirect’s free support options and click here to subscribe to AutomationDirect’s YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > DURApulse GS4 VFD Factory Reset from AutomationDirect