https://www.automationdirect.com/laser-sensors (VID-PH-0009)
Live demo and walk-through of this laser distance measuring sensor from AutomationDirect's family of laser distance sensors:
Sensor Range Laser
----------------------------
OPT2001: 30-80mm Class II
OPT2002: 30-80mm Class I
OPT2003: 40-160mm Class II
OPT2004: 40-160mm Class I
OPT2005: 50-350mm Class II
OPT2006: 50-350mm Class I
OPT2007: 60-660mm Class I
OPT2010: 200-3000mm Class I
OPT2011: 50-3050mm Class I
OPT2012: 0.2-6.2m Class I
OPT2013: 0.1-10.1m Class II More I/O Pins
OPT2014: 0.1-10.1m Class II Less I/O Pins
OPT2015: 0.2-100m Class I
The OPT2011 is an awesome mid-ranged full featured Laser Distance Sensor from AutomationDirect.com. The display has a bar graph giving you some idea where the target is in the range that you setup, an actual measured distance in mm and a bubble for each of the I O pins. These bubbles show you at a glance how the pins are configured. An A1 or an A2 tells you both output pins are switching outputs. AN means the pin is setup as an analog output – only pin A2 can do that on this sensor. An F is an error or Fault output which tells you if the sensor is receiving enough of the laser energy back to make a measurement. V is a contamination output. LA means the pin is configured as an external Laser enable input and T1 or T2 means the pin is configured as a Teach input – that means the pin can be used to update or re-calibrate the sensor while it is running. That’s cool. This sensor has a ton of options you can configure which are shown in this menu map from the user manual. Hit any button to get into the menus, then use the arrows to navigate this chart and enter key to select the option you want. To configure an I/O pin, you drop into this Pin Function menu first and tell the pin what you want it to do. Then you drop into that pin’s configuration menu – A1 or A2 to configure it. If you set A1 to be a switching output back in this menu, then you will be presented with the switching output options in the A1 configuration menu. If you set it to be an error output back here, then you’ll get these options. If you set it to be one of these inputs, then you will get these input options and if you set A2 to be an analog output then you’ll get a menu to set the analog parameters. In this video we will quickly walk through the options shown in Bold in this chart - these guys. These are the ones that are active out of the box. The rest of the options can be accessed by simply enabling expert mode in this menu item here – we’ll cover those in Part II of this video. We’ll use pin A2 for this walkthrough because it can do everything A1 can do, BUT it also can be set as an analog output. Let’s start at the top of this chart and work our way down – again – just the non-expert mode menus will be covered in this video. Here we go … To set A2 to be a switching output. Press any button, scroll down to the pin function menu, select pin A2 and select switching. To exit to the top level menu, scroll down to BACK and hit enter, then do it again. Now we scroll down to the configuration menu for pin A2. Note that it is telling me pin A2 is setup to be a switching output. Perfect. Hit enter to get into the switching output sub-menu. Let’s start with the Teach Foreground mode. In this mode we put the object we want to detect in front of the sensor and hit T for Teach. The sensor calibrates on that object, so now whenever an object passes by the sensor that is at that range or closer to the sensor, pin A2 will go active. Sure enough, A2 lights up when I bring an object close enough to the sensor. This is great for detecting all objects at this range or closer to the sensor. Teach Background is the exact same thing, except this time you calibrate with no object present. In this mode the sensor detects any object that is closer than the background, so it doesn’t discriminate like the Teach Foreground mode – it detects ALL objects that pass by that are a little closer than the background. This is great for looking down on a conveyor, for example.To set it up, you just drop into that menu, make sure no objects are in front of the laser and hit T for Teach. Teach Window is used for detecting all objects within a certain range or window. Objects outside of that range won’t be detected. You set it up just like the other two, except for one thing. You want to teach on the midpoint, so make sure your object is at the center of the detection range when you calibrate it. You then work your way down to this menu to set the width of the window. That’s the total width, so half of that is on either side of the detection range we just calibrated. That window can be up to 1 meter wide. This Potentiometer menu lets you tweak the detection threshold. That way if you teach on an object and it sets this level, you can move that level around without having to re-teach. You could also use this to create a larger gap from the background when in teach background mode, and you can use it to move the center of the window in Teach Window mode. The Hysteresis menu option allows you to set the width of the hysteresis. When an object is detected, the signal won’t go away until the object has moved beyond the original detection level PLUS an added amount. This is called the Hysteresis and it prevents the sensor from giving you false detections on small changes. You can set it to anything you want, but the minimum hysteresis depends on the filtering you have setup in this menu down here. I have filtering setup to average just 1 sample – which is no filtering - so the min hysteresis I can set is 20mm. The more filtering you use – or the more samples you average – the smaller you can set the hysteresis to. For example, here I’ve set the filtering to 500 samples. Now I can set the hysteresis as low as 3mm if I want to. So again, the more averaging you have, the smaller you can set the hysteresis. Let’s see, we already did Window Size, so we’ll skip down to this menu which allows you to switch the output between three options: PNP, NPN and Push/Pull. Note that pin A2 doesn’t have to be the same as Pin A1. This menu allows you to change the output behavior between Normally Open and Normally Closed. The last switching mode option - of the non-expert mode - is Teach External. This is a cool option that allows you to trigger a teach using an external signal. You could use it to simply re-calibrate the sensor manually – maybe you run different product sizes along the conveyor on different days and just want to walk up and hit a button to re-teach the sensor instead of navigating all of these menus. This is perfect for that. Or if you want to get fancy, you could have a sensor detect the temperature of the environment and when it has changed enough, re-calibrate this sensor to account for expansion of the metal frame that this sensor is mounted to. Lots of uses for this one. To use it, you have to tell one pin – we’ll use pin A2 – that it is going to be an external teach input for the other pin – A1 in this case. Of course pin A1 has to be setup as a switching output. Then down in A2’a menu – which look it reminds you it is the teach input for A1 now - you tell it that you want it to trigger the A1 teach on a high or low voltage input. Under A1’s menu you tell it you want it to be taught from an external signal and what kind of teach you want. That’s it. A1 will now recalibrate – or be re-teached, if that’s a word - every time A2 is activated. The Analog menu is only visible if you set pin A2 to be an analog output back here in the Pin Function Menu. Remember A1 can’t be an analog output. Once you set A2 to be an analog output, drop into Pin A2’s menu and scroll down to analog. Here you can set the output type: Current or Voltage. We’ll use Voltage – that’s 0 to 10 Volts. You can set the start and end of the range. Suppose you are only using the middle meter of the 3 meter range of this sensor. You COULD use the sensor as is, but your voltage swing will only be this. Using this menu item you can set this range to zero volts, or 4ma if you are using current, and this range to 10 volts or 20ma if you are using current. Now your PLC will get the full dynamic range of the sensor over just this limited disatnce. That makes your PLC programming a lot easier because now your min range is at min voltage or current and your max range is at max voltage or current. To do that you just put an object at the min range and teach that and then move the object to the max range you want and teach that. Now you will get the full voltage swing between those two settings and the even bar graph on the display will also give you full range over that limited distance. This at 0V and at 10V allows you to tweak the start and end of the analog output range. You simply increment or decrement them to what ever you want. Of course this would say 4ma and 20ma if we had chosen the Current mode … Finally, the last option in the non-expert mode is the display. We’ve been using the Switching mode display, but there is also an analog display. In this mode you see the actual voltage or current being output by the sensor, instead of the I/O pin bubbles. That’s especially handy when you are trying to program your PLC and do system test. You can also rotate the display which is helpful if you have to mount the sensors upside down in your application and you can change the intensity of the display and set a couple different screen saver modes. Power Save turns the display off after a minute. Screen saver inverts the display periodically to get equal wear on the pixels. In the next video we’ll enable this EXPERT mode and walk through those options. And don’t forget – Automation Directs tech support is FREE and you’ll talk to a real live person here in the US within minutes. Got a question? You can call, e-mail, or even do on-line chat during regular business hours. AutomationDirect.com offers Wenglor distance measuring sensors from 80 micro meters all the way out to 100 meters to cover all of your distance measuring needs.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings