https://www.automationdirect.com/do-more?utm_source=fs0TlrVnnG8&utm_medium=VideoTeamDescription (VID-DD-0051)
- This video gives basic information on Using the SUSPEND "Suspend Program or Task" instruction in the Do-more Designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0.3
Online Support Page: https://community.automationdirect.com/s/?utm_source=fs0TlrVnnG8&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
This instruction is used to stop the designated Program or Task from running. When this instruction has power flow the designated Program or Task will not run. The current state of all of the ladder logic in the Program or Task will be maintained. When this instruction loses power flow the designated Program or Task will resume from the point it was suspended. If a Program or Task is suspended, the Program or Task will be shown with a yellow background in the Project Browser.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings