DURApulse GS4 VFD EtherNet/IP Part 1: How to Setup EtherNet/IP from AutomationDirect


Related Products

GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-47P5
GS4-47P5 Thumbnail
GS4-4010
GS4-4010 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=fhHZeYb0Oz0&utm_medium=VideoTeamDescription

(VID-DR-0012)

Learn how easy it is to setup this EtherNet/IP VFD. on the GS4 Variable Frequency Drive (VFD).

Online Support Page: https://community.automationdirect.com/s/?utm_source=fhHZeYb0Oz0&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Before configuring a GS4 drive for EtherNet/IP, you will need to install the optional EtherNet/IP com card. This video shows you how to do that. There’s only three things we need to tell the drive to configure it for EtherNet/IP: Use the comm card for remote run stop control, Use the com card for remote frequency control, and assign an IP Address to the drive. Here we go … Use parameter 3.0 to tell the drive to use the comm card for remote run stop control. Second use parameter 4.0 to tell the drive we want to control the frequency remotely. Finally, we just setup the IP address of the Comm Card to be compatible with the network the drive will be on. I’m using this USB to Ethernet adapter to create an extra Ethernet port on my PC because the PC’s built in Ethernet port is being used for something else. You will usually use your PC’s built in Ethernet port. This Ethernet Port I am using has these settings, so to make my GS4 Drive compatible with that, I’ll enter these values into these parameters for the IP Address configuration. Remember – this IP address is compatible with MY network. Your IP Address will probably be different - something that is compatible with your network. Make sure the mask is correct. And I’ll set the gateway to zero since I am directly connecting from the PC to the drive. If you are uncomfortable with all of this IP Addressing stuff, just go find your local IT guy, he will know what to do. Could we have set the drive for DHCP and let the system automatically assign the IP Addresses? Sure – but that allows the system to dynamically change the IP Address whenever it wants to, which can make things really difficult for you, so we strongly encourage you to use static IP Addresses on your GS4 Drives so you always know the IP Address of your drive. This is important. We just entered these parameters into the drive. The Com card has its own set of registers that need these values. To push these values to the com cards, simply set P9.64 to a 2. When it turns back to a zero, the values were all correctly written to the EtherNet/IP card. One side note, you could have done all of this via GSoft2. And, the good news is GSoft2 automatically pushes the parameters to the com card for you, so you don’t need to fool with P9.64 when you’re using the GSoft2 application. And look at this, instead of entering the IP address stuff here, use this convenient IP Config dialog. You instantly see the drive firmware version, the com card type, firmware version and IP address. Switch to this tab to change the com card’s IP configuration. This dialog makes it so easy to see exactly what you have and to change the IP Configuration. The drive is now ready to talk to your system via EtherNet/IP. And all we did was install an EtherNet/IP com card, tell the drive to take run stop commands from the comm card, take the frequency commands from the comm card, and setup the IP Address. Watch this video to see how to test your EtherNet/IP communications using a third party EtherNet/IP explorer application. That’s a great way to verify the drive’s EtherNet/IP communications independent of your system and it’s also a great way peek under the hood and see how EtherNet/IP works. Click here to learn more about the GS4 Drive. Click here to learn more about AutomationDirect’s free support options and click here to be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > DURApulse GS4 VFD EtherNet/IP Part 1: How to Setup EtherNet/IP from AutomationDirect