To learn more: https://www.automationdirect.com/click-plcs?utm_source=fTSAqboNQcA&utm_medium=VideoTeamDescription
(VID-CL-0011)
Video Tutorial
CLICK PLCs
Getting Started
Part 6, Establish PC to PLC Communications
Online Support Page: https://community.automationdirect.com/s/?utm_source=fTSAqboNQcA&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
if you have been following along in this series of videos then you now have a project and you have also a five powers to the clip CPU next we need to get the pc talking to the click port1 on the click CPU module is designed as the primary programming port this port has fixed communication parameters so you can always connect the programming software to the clique CPU module through this port without any configuration changes there are a couple of choices for connecting the PC to port 1 on the click CPU module if a 9-pin rs-232 serial communications port is available on your PC then use an automation direct PC serial programming cable shown here to connect between the PC and the CPUs port 1 the trend on newer pcs has been not to include a serial port in that situation use an automation direct USB to rs-232 PC to panel programming cable assembly shown here and connect between the PC and the CPUs port 1 once the communication cable is connected we need to establish communications between the two if using the PC serial port then we need to know what comm port number it is assigned typically this will be com1 or calm 2 if using USB communications then we will need to know what comm port number has been assigned when the coil USB driver recognizes the click CPU the software has a built in utility that will allow us to easily identify the comport number from the PLC pulldown menu in the programming software select connect as shown here or you can click on the connect icon located on the PLC toolbar the connect to PLC dialog box will be displayed under the PC comm port number drop down list select the communications port that is connected to the CPUs port 1 if you are connecting the programming cable to port 1 on the click CPU module you do not need to change any of the rameters just click the ok' button the software should start to immediately connect to the click CPU module if you cannot connect the software to the click CPU module try the above procedure one more time and keep watching the tx1 and our x1 indicators on the click CPU module if the our x1 is not blinking it means the click CPU module is not receiving any data from the programming software check to make sure you selected the correct PC comport and also check the cable connections the following connect dialog box will appear once communications has been established with the click CPU it is typical that the project that is opened in the programming software will not match the project that resides in the CPU the dialog box gives you a choice to either read the PLC's project for viewing purposes but at the same time allowing the project open in the software to still be saved or not read the project in the PLC we now have communications part 7 and this video series will show you how to write your project into the memory of the click CPU until next time thank you for watching have a great day
Voted #1 mid-sized employer in Atlanta
Check out our
job openings