To learn more: https://www.automationdirect.com/click-plc?utm_source=c_qScHu8s3A&utm_medium=VideoTeamDescription
(VID-CL-0015)
Video Tutorial
CLICK PLCs
Getting Started
Part 10, Y001 Output On? Follow this CLICK PLC series as we walk through setting up and using the CLICK PLC hardware and software.
https://community.automationdirect.com/s/?utm_source=c_qScHu8s3A&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
[Music] this is it we've taken the click CPU installed the programming software written a simple project powered it transferred the project to The Click cpu's memory and tested the project now we get to see the results [Music] [Music] hopefully you still are connected to the CPU with your project up and running and you still have the data view dialogue box showing the C1 bit entered if not please do this next okay if you are there and the C1 bit is still in the on state from Step nine we need to turn it off by double clicking on the off button in the new value column on our c C1 entry as shown here in other words we can toggle the C1 bit on and off by double clicking on the opposite state of the new value button here we go while watching The Click CPU y001 output double click the on button in the new value column of the C1 entry showing here after 5 Seconds you will see the red LED come on if you missed viewing the transition of the y0 01 status LED from off to on write an off state to the C1 bid and then an on State and data view to do it again let's try one more thing you may have noticed we also have an x001 input in our ladder logic that is programmed in parallel to our C1 bit in our demo unit we have a push button wired into x001 and also an indicator pilot light wired to Output y001 if we press the push button and wait 5 Seconds we will see the indicator turn on our ladder logic program is working as we intended we are done we hope you have gained some insight into the simple use of the click PLC system and are now more comfortable in finding a use for it in your next control or automation project until next time thank you for watching and have a great day [Music]
Voted #1 mid-sized employer in Atlanta
Check out our
job openings