WEG CFW300/320 VFD Over Current Debug Part 2 from AutomationDirect


Related Products

CFW320A02P6T4NB20
CFW320A02P6T4NB20 Thumbnail
CFW300A01P6S1NB20
CFW300A01P6S1NB20 Thumbnail
CFW300A01P6S2NB20
CFW300A01P6S2NB20 Thumbnail
CFW300A04P2S2NB20
CFW300A04P2S2NB20 Thumbnail
CFW300A06P0S2NB20
CFW300A06P0S2NB20 Thumbnail
CFW300A07P3S2NB20
CFW300A07P3S2NB20 Thumbnail
CFW300A01P6T2NB20
CFW300A01P6T2NB20 Thumbnail
CFW300A04P2T2NB20
CFW300A04P2T2NB20 Thumbnail
CFW300A06P0T2NB20
CFW300A06P0T2NB20 Thumbnail
CFW300A07P3T2NB20
CFW300A07P3T2NB20 Thumbnail
CFW300B10P0B2DB20
CFW300B10P0B2DB20 Thumbnail
CFW300B15P2T2DB20
CFW300B15P2T2DB20 Thumbnail
CFW300-CRS232
CFW300-CRS232 Thumbnail
CFW300-CRS485
CFW300-CRS485 Thumbnail
CFW300-CUSB
CFW300-CUSB Thumbnail
CFW300-KHMIR
CFW300-KHMIR Thumbnail
CFW300-IODR
CFW300-IODR Thumbnail
CFW300-IOAR
CFW300-IOAR Thumbnail
CFW300-IOADR
CFW300-IOADR Thumbnail
CFW300-IOAENC
CFW300-IOAENC Thumbnail
CFW300-KFA-S1-S2
CFW300-KFA-S1-S2 Thumbnail
CFW300-KFB-S2
CFW300-KFB-S2 Thumbnail
CFW-WPS
CFW-WPS Thumbnail
CFW300-FAN-A
CFW300-FAN-A Thumbnail
CFW300-FAN-B
CFW300-FAN-B Thumbnail
CFW100A01P6S120G2
CFW100A01P6S120G2 Thumbnail
CFW100B02P6S120G2
CFW100B02P6S120G2 Thumbnail
CFW100A01P6S220G2
CFW100A01P6S220G2 Thumbnail
CFW100B02P6S220G2
CFW100B02P6S220G2 Thumbnail
CFW100C04P2S220G2
CFW100C04P2S220G2 Thumbnail
CFW320A01P6S1NB20
CFW320A01P6S1NB20 Thumbnail
CFW320A02P6S1NB20
CFW320A02P6S1NB20 Thumbnail
CFW320A04P2S1NB20
CFW320A04P2S1NB20 Thumbnail
CFW320A06P0S1NB20
CFW320A06P0S1NB20 Thumbnail
CFW320A01P6S2NB20
CFW320A01P6S2NB20 Thumbnail
CFW320A02P6S2NB20
CFW320A02P6S2NB20 Thumbnail
CFW320A04P2S2NB20
CFW320A04P2S2NB20 Thumbnail
CFW320A06P0S2NB20
CFW320A06P0S2NB20 Thumbnail
CFW320A07P3S2NB20
CFW320A07P3S2NB20 Thumbnail
CFW320A01P6T2NB20
CFW320A01P6T2NB20 Thumbnail
CFW320A02P6T2NB20
CFW320A02P6T2NB20 Thumbnail
CFW320A04P2T2NB20
CFW320A04P2T2NB20 Thumbnail
CFW320A06P0T2NB20
CFW320A06P0T2NB20 Thumbnail
CFW320A07P3T2NB20
CFW320A07P3T2NB20 Thumbnail
CFW320B10P0B2DB20
CFW320B10P0B2DB20 Thumbnail
CFW320B15P2T2DB20
CFW320B15P2T2DB20 Thumbnail
CFW320A01P1T4NB20
CFW320A01P1T4NB20 Thumbnail
CFW320A03P5T4NB20
CFW320A03P5T4NB20 Thumbnail
CFW320A04P8T4NB20
CFW320A04P8T4NB20 Thumbnail
CFW320B07P6T4NB20
CFW320B07P6T4NB20 Thumbnail
CFW320C11P0T4NB20
CFW320C11P0T4NB20 Thumbnail
CFW320C14P0T4NB20
CFW320C14P0T4NB20 Thumbnail
CFW320B01P1T4DB20
CFW320B01P1T4DB20 Thumbnail
CFW320B02P6T4DB20
CFW320B02P6T4DB20 Thumbnail
CFW320B03P5T4DB20
CFW320B03P5T4DB20 Thumbnail
CFW320B04P8T4DB20
CFW320B04P8T4DB20 Thumbnail
CFW320B07P6T4DB20
CFW320B07P6T4DB20 Thumbnail
CFW320C11P0T4DB20
CFW320C11P0T4DB20 Thumbnail
CFW320C14P0T4DB20
CFW320C14P0T4DB20 Thumbnail


To learn more: https://www.automationdirect.com/cfw300?utm_source=8mWTTDERfUg&utm_medium=VideoTeamDescription

(VID-DR-0091)

Learn how Current regulation is handled and how to use it to your advantage in this video tutorial using the WEG CFW300. This is the best VFD, with a super low cost, but with high end features like Dynamic Braking, Fire Mode, PID, 65,000A SCCR, Zero Stack footprint, Multi-Speed, etc. and is even cULus listed!

Online Support Page: https://community.automationdirect.com/s/?utm_source=8mWTTDERfUg&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

To show you how current limiting works on this drive, I put a large 12-pound steel sprocket on this motor to give us some inertia to overcome. I reset the drive to factory default and setup the motor parameters to match this motor and set the reference frequency to 60 Hz to tell the drive to ramp up the motor to full speed over the acceleration time we specified. The acceleration ramp is currently at the default 5 seconds which is a good place for us to start, and I’ll reduce the deceleration ramp time to 4 seconds so we’re not spending a lot of time waiting on the motor to decelerate. I’m using the free WPS software and this USB com module to talk to my drive from my PC. I’ve already created a configuration and a resource and am online with the drive. We’re just going to use WPS to visualize things, I’ll enter the parameters from the Drive’s built-in HMI as a reminder that we don’t need the free WPS software and an optional com module to do this. Speaking of visualizing things, look at this. Down here under protections, Inverter – these graphs show us exactly how limiting works. This side is voltage limiting. We cover that in a different video – and this is the current limiting we’re doing in this video. The current limiting threshold is in parameter 135. That threshold can be used for three things. First it can be used to disable current limiting. If we set the threshold really high, the manual says to set it to 1.9 times the drives max rated current - then there won’t be any current limiting. Let’s try it. This drive is rated for 4.2A, so I’ll go to parameter 135 and enter 8 amps. I’m also going to go to parameter 100 to set the acceleration ramp at a ridiculously small number to really stress the drive. Hit run, and of course we get an overcurrent fault. The second current limiting option is to set the threshold at a reasonable value and employ one of two current limiting techniques. The default current limiting threshold for this drive is 6.3 amps – about 50% above the drive's max rated current of 4.2 amps. Remember – the drive’s max rated current is how much current the drive can handle continuously. This threshold is looking for spikes in current. If we go to the data sheet we see this drive can handle a 150% overload for 60 seconds and 200% overload for 3 seconds. So, a 6.3 amp threshold makes sense. Ok, given that threshold we have two choices. One is if the current hits the threshold, have the acceleration ramp hold to give the motor a chance to catch up. Remember, it’s the acceleration of the motor that creates the demand for the current. The greater the acceleration, the more current it needs. So, if the drive holds the ramp constant until the motor catches up then the current demand falls. The other current limit option is when the motor current hits the threshold. Instead of holding the acceleration ramp rate, it actually allows it to decelerate until the motor catches up. In both cases, once the motor catches up, the original ramp continues on. So, what these are really doing is automatically extending the ramp time to prevent an overcurrent fault. You could accomplish the same thing yourself by just using a longer ramp time, but then you would have to figure out how long that needs to be. By using the current limiting options, you’re letting the drive give you the best possible ramp time automatically. Let’s do an example so we can see how this works. I would love to show you this in the WPS Trend View, but trend view isn’t really fast enough to show us what we need to see. It’s fastest sample rate is only 50 ms, so instead I’m using this optional I/O module that has two analog outputs. And we’ll send the motor current and the output frequency to those two outputs, so we can view them on a scope. If I look in the programming manual’s analog output functions table, we see output current is a 5, and the output speed, which they call the “real speed”, is a 2. So, I’ll go to parameter 251 for analog output 1’s function and enter a 2 for real speed and then go to parameter 254 for analog output 2’s function and enter a 5 for the output current. I’m monitoring those on an inexpensive USB oscilloscope I bought on the internet. Ok, before we change anything let’s get a baseline. Let’s get the acceleration ramp back to a reasonable 5 seconds and put the over current threshold back at the default value for this drive which is 6.3 amps. I’ll get the scope running … and hit run on the drive. Wait the 5 seconds for it to ramp up, give it a couple more seconds to settle out, and hit stop. Cool. We can see the red frequency ramp is pretty much what we expected – and the drive was able to get the motor up to speed in the 5 seconds we wanted. And most important, the current looks good. The analog current output is 0-10 volts where 10 volts is twice the drives rated current of 4.2 amps. How did I know that? It’s in this analog output table in the programming manual where parameter 295 is the drives rated current. Which means the current got up around to around 3.2 amps. And we know from parameter 135 that the current overload threshold is set at 6.3 amps. So, since the current never got anywhere near that level, it says the 5 second ramp was easy for the drive to do. So, let’s challenge the drive by going to parameter 100 and reducing the acceleration ramp to a ridiculously small time to really stress the drive. Start the scope, hit run ... stop. Let’s zoom in so we can see this better. Now the motor current IS crossing the threshold and the ramp is getting extended but it’s kind of hard to see, so I’ll speed up the scope AND let’s go to parameter 135 and lower the current limit threshold to exaggerate the effect. On our base line we saw the current never got above 3.2 amps, so I’ll lower the threshold to something just above that – how about 3.6 amps. Again, you wouldn’t normally do this, I’m just doing it to get current limiting to kick in sooner, so we can see the effect a little better. Start the scope, hit run ... Stop. Our new current limit threshold is here at 3.6 amps. The bad news is, it looks like the drive is only updating the analog output every 25 ms. So, we get this stair step effect instead of a smooth curve. Which means we have to use our imaginations a little bit and just know there are some fast transitions here that we can’t see on this plot. But, we can see the end result. The frequency output is definitely going into that ramp deceleration mode in several places to extend the ramp time and prevent an overcurrent fault. Looks like the 0.1 second ramp time we asked for was extended to a little over 1.5 seconds. Let’s go to parameter 150 and switch from ramp decel to ramp hold mode by putting a 2 here. Start the scope, hit run, stop. And we got pretty much the same ramp time … but this time instead of decelerating the ramp to limit the current draw, it was simply held level. Exactly what we wanted. And again, while the analog output is too coarse to see the actual threshold crossings, we can definitely see the ramp hold periods and that the current was held at a reasonable level. Ok, well, while we are at it, let’s see what an over current fault looks like. I’ll go back to parameter 135 and put it at 8 amps again to turn off current limiting. Start the scope, hit run, stop. Well, that was pretty quick. We put the over current threshold way up here, and sure enough, the Motor current was allowed to spike and in a little over 100 milli-seconds the drive shut the output down. Cool. The bottom line is, if you are getting an overcurrent fault like this, you probably have the current limiting threshold set too high and the fault is kicking in before the limiting can take effect. Setting that overcurrent limiting threshold to a value that works best for your application is usually the key to fixing overcurrent fault issues. And a good starting point is about 150% of the drive’s max rated current, which is the default value for these drives. Click here to learn more about the WEG CFW300 Variable Frequency Drive. Click here to learn about AutomationDirect’s free award-winning support options and click here to subscribe to our YouTube channel so you will be notified when we publish more videos.



No data returned!
An error has occurred! Please contact support
Videos Home > WEG CFW300/320 VFD Over Current Debug Part 2 from AutomationDirect