Cookies are not enabled on your browser.
To learn more: https://www.AutomationDirect.com/drives?utm_source=ZpS28fqGl_o&utm_medium=VideoTeamDescription
(VID-DR-0111)
This video shows you a simple way to organize the parameters associated with PID to make it easy to get up and running with PID quickly. If you are familiar with PID, then this will be all you need to get up and running. If you are new to PID or just need a refresher there are focused topic videos that do a deep dive into all of the aspects of PID. Things like: Process Variable, Setpoint, PID Tuning, Control Output, Alarms, Auto/Manual control, Bumpless mode, etc.
Download resources used in these videos here: https://library.automationdirect.com/weg-vfd-pid-resource-page/
Online Support Page: https://community.automationdirect.com/s/?utm_source=ZpS28fqGl_o&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
In this video we’ll use this excel spreadsheet configuration utility to do a quick walk through of how to setup PID in a WEG CFW100 or 300 drive with very little explanation of why we chose the particular values we used. If you are already familiar with PID it’ll be all you need to get up and running. If you aren’t that familiar with PID or just need a refresher, there are focused topic videos for each part of this. I’ll pop those up as we go along to remind you they are available if you want to learn more about that particular topic. Our task is to get rid of all the yellow cells by filling them in with appropriate values. Gray cells are read only cells and I’ve marked the cells with default values that we don’t need to change with blue, so you know to just verify they are still at that default value. Before starting, go to parameter 900. A four says an application is currently running, so I’ll go to parameter 901 and set it to a zero to disable the softPLC. Go back to parameter 900 and we see a three which tells us the application is not running. Now we can go to parameter 204 and set it to an 11 to reset all of the soft PLC parameters. The default SoftPLC app is the PID function the drive uses – PID isn’t actually in the drive, it’s in the Soft PLC. We’ll talk more about that in the SoftPLC PID video. My drive parameters are still setup from the previous video, so I’ll just re-enter those here to clear the yellow boxes. EXCEPT for these two – we are going to change those in a minute so we’ll leave those yellow to remind us. OK, Let’s start with the set point parameters. We want the setpoint to come from the Drives HMI Keypad so we put a 0 here. I’ve added comments like this to most of the blocks to help guide you, but I’m not guaranteeing I typed everything exactly right so please double check with the user manual if in doubt. We want our setpoint to be 6 psi, so I’ll put that here. We can filter the setpoint if you are driving it from an analog input. We aren’t so we’ll set it to zero. The Setpoint video covers all of the various setpoint options. The RED box reminds us that this is entered in engineering units. Which means we need to configure the display for engineering units. Parameter 510 sets the units indicator in the HMI Display. There is no indicator for psi, so we’ll set that to a zero to display nothing. Parameter 511 sets the decimal point for all SoftPLC parameters that use engineering units so let’s make sure that’s 2 decimal places. Finally, we will want to disable bumpless mode while we are getting things setup so we’ll put a 0 in here. Let’s configure the Process variable. Parameter 921 is where we tell the PID app that the process variable is coming in on analog input 1 and you can view the current process variable value at any time in parameter 916. We have a direct or forward acting system so we put a 1 here. Of course we need to setup analog input 1 so we tell Analog input 1 it will be used as the process variable, and we’ll use the default gain, 0 to 10 volt signal, offset, and we’ll add a little filtering. We have a whole video set aside for techniques you can use to reduce process variable noise, filtering is just one of those ways. Since the PID app expects the process variable in engineering units, we have to tell it how to convert the analog input to engineering units using PV min and PV max along with the min and max motor frequency. We derive those straight from the curves we created in the previous video. This is critical to your success and frankly, this is the single most common thing I see folks screw up. So if you aren’t real sure how to do that, then be sure to watch the process variable video where you will see how simple it is to get right once you understand what these four parameters represent and how they work together to give you the best possible PID performance. Our initial PID values are easy – we just use the default values. The PID Tuning video will give you a better feel for what each really does and how to optimize them! We are going to control the Manual/Auto modes from Digital input 2 and this is where we put the value we want for the drives output. Down here I listed the parameters we didn’t need for this demo just so you have them if you want to use alarms, add torque boost, use a different type of setpoint and if you want to use sleep mode. Well, we’ve gotten rid of all the yellow cells, so we are ready to give this a try. Over here is a list of all of the PID related parameters in numerical order which makes entering them into the drive super easy. We’re not covering alarms in this video, so I just entered some values that will prevent alarms and faults. There’s a whole separate video about how to use alarms and faults if you want to use those. Since all the blue parameters are default’s, we don’t need to change those and the gray parameters are ones we aren’t using, and most of these we setup in the previous video, all we really have to do is enter the new min and max drive frequencies and verify the rest are where we think they should be, and enter just 3 PID parameters and modify these four alarm parameters so they don’t interfere with this demo. I’ll go ahead and enter all of the new parameters into the drive, and verify all of the rest. Ok, let’s go to parameter 901 and set it to a 1 to tell the softPLC PID app to run. I’ll go to parameter 900 and sure enough it’s a four which tells us the PID app is running. We are in manual mode, so I’ll go ahead and switch to run and I’ll go to parameter 918 and scroll through some values. Remember, we set the min and max motor speed to 25 to 50 hertz, so while we can set the manual setpoint where ever we want, it won’t actually do anything until it is between those two frequencies. If I go to 35 hertz, then sure enough, the pressure is near 7 psi – exactly what we expect to see from the plot we created in the previous video. So, could we have setup PID first and then generated our curves using this manual mode where we manually control the output of the drive? Yep, just widen up the min and max drive frequencies before you start and change them to the values you need before running PID. Great Manual Mode works, let’s flip over to having PID control the output to automatically maintain 6 psi. And sure enough, with one valve open, the system settles out right at 6 psi. Cool. And remember, you can also see the process variable in parameter 916. How about 2 valves? Wait a few seconds. Yep it settles out at 6 psi too. How about 3 valves? Again, give it a few seconds … and sure enough it settles out right at 6 psi. 4 valves? Sure enough it ramps up and settles out right at 6 psi. How about no open valves? Sure enough, given enough time it settles out right at 6 psi. Very cool. But, there’s a problem. It’s taking around 10 to 15 seconds for the system to settle out. Can we make it respond faster? Yeah, we can. For example, with the PID parameters optimized, now when I open and close valves look how fast the system responds! It settles out at 6 psi within a second or two. Even for the no valves open case. And it only took me a minute to optimize the PID coefficients, so if you want to learn how I did that, be sure to check out the PID Tuning video where we’ll do that and run some examples to help you get a better feel for how PID works. So again, all really all we did, was enter the usual motor and drive parameters, entered the setpoint and PV min and PV max – which we got from the plot we created in the previous video – and we told the PID app to run and everything just worked. How about that? This little configuration utility makes it super easy to visualize how to setup PID and helps make sure we don’t miss anything. If you are using the free WPS software for your drive configuration, then guess what … it has a built in PID wizard that does the exact same thing except it actually enters the values for you and you can see the results on a trace in real time. Watch the PID wizard video to learn more about that. Click here to see all the PID video tutorials for the WEG CFW series of drives. Click here to subscribe to our YouTube channel so you will be notified when we publish new videos and click here to learn about AutomationDirect’s free award-winning support options.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings