To learn more: https://www.AutomationDirect.com/click-plus-plc?utm_source=YRZXqin9bCU&utm_medium=VideoTeamDescription
(VID-CL-0077)
The CLICK PLC line from AutomationDirect may have started out as a simple entry-level PLC, but it has evolved into a full-featured controls platform. With the addition of the CLICK PLUS models, we added even more power and versatility. Explore some of the amazing option modules available for the CLICK PLUS. Add Node-RED interactions with the C2-NRED module. Open the world of OPC UA communications with the C2-OPCUA module.
Online Support Page: https://community.automationdirect.com/s/contactsupport?utm_source=YRZXqin9bCU&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
In 2008, AutomationDirect introduced the affordable and accessible Click PLC to the world of automation. With a compact form factor and an intentionally simplified instruction set, the Click found its niche as a fantastic entry-level controller. Well, over the years, the Click line has grown into something else altogether. We’ve added the Click Plus and continued to refine its capabilities. With Wi-Fi, high-speed IO, MQTT support, data logging, remote Mobile App connectivity and dozens of advanced capabilities, the Click Plus is one of the most versatile and capable PLCs out there, with features most PLCs only dream of, even those at multiple times the Click’s astonishingly low price point. Let’s look at a couple of these features, some intelligent option modules: The C2-NRED module provides an industrial interface to the most popular open-source software tool for developing IIoT applications – Node-RED®. With low-code Node-RED programming, you can easily facilitate interactions between the CLICK PLUS CPU and upper-level IT or business systems. This intelligent module utilizes its own processor, ensuring the main CPU remains unburdened but has direct access to the memory of the PLC and all the data needed. The C2-NRED also supports custom JavaScript programming, extending the CLICK PLUS platform's functionality even further. OPC UA is a long-standing communication protocol used throughout industry and provides a standardized way for industrial systems, regardless of manufacturer, to communicate and share data. The C2-OPCUA module, when added to a CLICK PLUS CPU, allows the simplicity and reliability of CLICK PLCs to be deployed in many more applications that support this protocol. Click and Click Plus PLCs are as remarkable for their reliability and sheer versatility as they are for their affordability and user-friendliness. Check them out today at AutomationDirect.com. Click here to learn more about AutomationDirect and our products. Click here to see more videos about the Click line of PLCs. Click here to subscribe to our YouTube channel and stay informed on all new products and developments from AutomationDirect.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings