To learn more: https://www.AutomationDirect.com/label-maker?utm_source=VU4lc2-CXO8&utm_medium=VideoTeamDescription
(VID-WD-0057)
Epson LabelWorks PX series label printers allow users to easily create professional labels, self-laminating wire wraps, wire and cable markers, and more! Design your labels directly using the multifunction keyboard, the Epson Label Editor software, or print straight from your mobile device. Print on a wide variety of colors and sizes using adhesive or magnetic tape, and even directly on heat-shrink tubing. Watch this video to learn more about our line of Epson LabelWorks printers and buy yours today.
Online Support Page: https://community.automationdirect.com/s/?utm_source=?utm_source=VU4lc2-CXO8&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
Industrial wiring can be a hassle when wires aren’t labeled correctly. That’s why we carry the Epson LabelWorks PX series label printers. These printers allow users to easily create professional labels, self-laminating wire wraps, wire and cable markers, and more! Design your labels directly using the multifunction keyboard, the Epson Label Editor software, or print straight from your mobile device. Print on a wide variety of colors and sizes using adhesive or magnetic tape, and even directly on heat-shrink tubing. When it comes to label printing for your next management or organizational project—at any budget—AutomationDirect and Epson LabelWorks have you covered. Let’s take a look at the LW-PX900, the top choice for industrial automation engineers. The LW-PX900 was designed with the modern engineer in mind. It’s ruggedly built and requires no software to use, making it perfect for labeling on the job site. It can print on tapes up to 1.5 inches wide and shrink tubing up to 7/8 inch for clear, easy-to-read labels. Magnetic tape and die-cut labels are also available! You can even print barcodes and images. With both half-cut and full-cut options, labeling is a breeze. Print a single label or sequence them to speed up your wiring projects. This printer is packed with features, so let’s explore a few! You can customize this printer to create nearly any label you need in the field—general labels, punch block labels, flag labels, wrap-around labels, block-66 labels, and faceplate labels are all at your fingertips. Save frequently used labels directly to the device for quick reprinting whenever needed. If you require labels of varying lengths, the printer can handle that too! The half-cut feature ensures labels are separated at the adhesive backing rather than being fully cut, making them easy to peel as needed. The half-cut feature also makes labeling and tubing insertion more efficient. For example, if you need five labels for VFDs in your panel and want to ensure each wire connects to the correct output in your PLC, sequencing is simple. 1. Turn on the printer and enter "VFD." 2. Press the sequencing button on the bottom left of the printer, enter "01" for the first VFD, and press return. 3. Specify how many times you want it repeated, then press return. 4. Your screen should now display "01" with dots over it. 5. Press shift and print to access the special print menu, then find "Print Copies." 6. Press return, enter the number of copies needed, and press return to start printing. Once the shrink tubing begins to print, you’ll notice that the cuts don’t go all the way through. Simply insert the wire into the first label, break it off, and repeat until all your wires are labeled. It’s that easy! To make wrap-around labels, it's just as easy. 1. Start by pressing the wrap button. 2. Once the menu opens, select diameter or length and press return. 3. Enter the label length and press return. 4. Select whether to have the text repeat and press return. 5. Select your margins and press return. The tape/3 is a third of your tape width, and tape is the entire width of the tape. 6. Enter the text. 7. Hit print, and your labels are ready to go! You can never be too prepared on the job site! Check out the LW-PX900 and the rest of our Epson printers available now at AutomationDirect.com! Click here to learn more about these Epson Printers. Click here for more videos.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings