AutomationDirect
Login | Register
Accounts & Orders
Cart
0
$0.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $0.00
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
Videos Home > CLICK PLC Connect to a DURApul...

CLICK PLC Connect to a DURApulse GS4 VFD via Modbus TCP from AutomationDirect


Related Products

GS4-47P5
GS4-47P5 Thumbnail
GS4-2100
GS4-2100 Thumbnail
GS4-41P0
GS4-41P0 Thumbnail
GS4-42P0
GS4-42P0 Thumbnail
GS4-43P0
GS4-43P0 Thumbnail
GS4-45P0
GS4-45P0 Thumbnail
GS4-21P0
GS4-21P0 Thumbnail
GS4-22P0
GS4-22P0 Thumbnail
GS4-23P0
GS4-23P0 Thumbnail
GS4-25P0
GS4-25P0 Thumbnail
GS4-27P5
GS4-27P5 Thumbnail
GS4-2010
GS4-2010 Thumbnail
GS4-2015
GS4-2015 Thumbnail
GS4-2020
GS4-2020 Thumbnail
GS4-2025
GS4-2025 Thumbnail
GS4-2030
GS4-2030 Thumbnail
GS4-2040
GS4-2040 Thumbnail
GS4-2050
GS4-2050 Thumbnail
GS4-2060
GS4-2060 Thumbnail
GS4-2075
GS4-2075 Thumbnail
GS4-4010
GS4-4010 Thumbnail
GS4-4015
GS4-4015 Thumbnail
GS4-4020
GS4-4020 Thumbnail
GS4-4025
GS4-4025 Thumbnail
GS4-4030
GS4-4030 Thumbnail
GS4-4040
GS4-4040 Thumbnail
GS4-4050
GS4-4050 Thumbnail
GS4-4060
GS4-4060 Thumbnail
GS4-4075
GS4-4075 Thumbnail
GS4-4100
GS4-4100 Thumbnail
GS4-4125
GS4-4125 Thumbnail
GS4-4150
GS4-4150 Thumbnail
GS4-4175
GS4-4175 Thumbnail
GS4-4200
GS4-4200 Thumbnail
GS4-4250
GS4-4250 Thumbnail
GS4-4300
GS4-4300 Thumbnail


To learn more: https://www.automationdirect.com/VFD?utm_source=TMwTr7k2lc0&utm_medium=VideoTeamDescription

(VID-DR-0049)

Learn how to connect a CLICK PLC to a GS4 Variable Frequency Drive (VFD) via Modbus TCP in this video tutorial from AutomationDirect.

Online Support Page: https://community.automationdirect.com/s/?utm_source=TMwTr7k2lc0&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

We want a CLICK PLC to talk to a GS4 Drive over Modbus TCP. To do that, you need to have a CLICK PLC with an Ethernet Port, of course, and connect it and your GS4 Drive to your Ethernet Network. You will need the GS4 Drive’s optional com card to communicate via Modbus TCP. I’m using a little test network in my office with these IP addresses, yours will probably have different IP Addresses. In the CLICK software, let’s have the rising edge of contact C1 .. Send … a Frequency command. We want Port 1, which is the Ethernet port on this CLICK, and the Modbus protocol. Let’s set up the CLICK’s ethernet port. We want to set the IP Address to be compatible with our network, so I’ll give it this address, mask and gateway that we had on the previous diagram. The rest of this is fine so hit OK. Enter the IP Address of the GS4 Drive that we saw on the network diagram just a minute ago, here. The GS4 Drives ID is a 1. We want to write to a singer REGISTER. Using Modbus. And if we look in the GS4 manual we see these are the addresses we need to control the Drive. Frequency is this address so we put that here. Notice that the CLICK uses the 40 here instead of the 4 shown in the GS4 user manual. That’s important, don’t miss that. And we’ll put the frequency value to send in this register. I’ll fill out the status data just in case we get an error. Perfect. Well, that set up the frequency command. I’m just going to copy that rung, and paste it and let’s have C2 send a RUN command. The GS4 user manual tells me that is at address and we have to add a 40 for the CLICK. And we will use DS2 to hold the RUN command which we will set to a 2 in a Dataview in just a minute. Copy that rung and paste it and we’ll have C3 be the stop command. It’s identical except it sends a 1 which we will store in DS3. Copy that rung, paste it and let’s have C4 send a Forward Command. That’s at the same Modbus address and we’ll put the forward command in DS4. Copy that, paste it, and let’s have C5 send a reverse command, which uses the same address, but will send the contents of DS5 which will be a 32. And don’t forget the END instruction. Great. Let’s write that to the PLC. I’ve already created a data view with all of the control bits, created Nicknames for all of those, and I put the values we need for the various commands in the DS registers. Let’s put a frequency of 33 Hz in here. I already setup the GS4 to accept RTU commands using this video … so let’s try it. Make sure the click is in RUN mode. If I toggle C1 to change the frequency, sure enough the drive responds. If I toggle C5 to change to reverse, yep, the drive got it. Toggle the run bit, the drive starts spinning. Toggle the forward bit and it starts to change direction … and toggle stop and the drive ramps to a stop. Well, that ought to be enough to get you started. Click here to learn more about GS4 Drive. Click here to learn about AutomationDirect’s free support options. Click here to subscribe to AutomationDirect’s YouTube channel so you will be notified when we publish new videos.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info