To learn more: https://www.automationdirect.com/do-more?utm_source=PltcOthe_5U&utm_medium=VideoTeamDescription
(VID-DD-0073)
This video gives basic information on Using the Delta Contact in the Do-more Designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0.3
Online Support Page: https://community.automationdirect.com/s/?utm_source=PltcOthe_5U&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
This contact is used to evaluate if there is a change in value of the assigned register from one PLC scan to the next. If the value has changed it will enable Power flow through the contact. Since this action happens in one PLC scan it is unlikely you will ever see status indication of this change, in the programming software. Use an increment or counter instruction to verify the contact’s operation. This contact supports integers Reals, or even bits.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings