Linear Slide Value Series Rebuild from AutomationDirect


Related Products

LARSD2-08T24BP2C
LARSD2-08T24BP2C Thumbnail
LAVL-60T12LP2
LAVL-60T12LP2 Thumbnail
LAVL-60T12LP5
LAVL-60T12LP5 Thumbnail
LAVL-60T18LP2
LAVL-60T18LP2 Thumbnail
LAVL-60T24LP2
LAVL-60T24LP2 Thumbnail
LAVL-60T24LP5
LAVL-60T24LP5 Thumbnail
LAVLACC-001
LAVLACC-001 Thumbnail
LAVLACC-002
LAVLACC-002 Thumbnail
LAVLACC-003
LAVLACC-003 Thumbnail
LAVLACC-004
LAVLACC-004 Thumbnail
LAVLACC-005
LAVLACC-005 Thumbnail
LACP-16T06L1
LACP-16T06L1 Thumbnail
LACP-16T06LP5
LACP-16T06LP5 Thumbnail
LACP-16T12L1
LACP-16T12L1 Thumbnail
LACP-16T12LP5
LACP-16T12LP5 Thumbnail
LACP-16T24L1
LACP-16T24L1 Thumbnail
LACP-16T36L1
LACP-16T36L1 Thumbnail
LACP-16T36LP5
LACP-16T36LP5 Thumbnail
LACPACC-001
LACPACC-001 Thumbnail
LACPACC-002
LACPACC-002 Thumbnail
LACPACC-003
LACPACC-003 Thumbnail
LACPACC-004
LACPACC-004 Thumbnail
LACPACC-005
LACPACC-005 Thumbnail
LARSA1-08L12C
LARSA1-08L12C Thumbnail
LARSA1-08L24C
LARSA1-08L24C Thumbnail
LARSA1-08L36C
LARSA1-08L36C Thumbnail
LARSA1-12L12C
LARSA1-12L12C Thumbnail
LARSA1-12L24C
LARSA1-12L24C Thumbnail
LARSA1-12L36C
LARSA1-12L36C Thumbnail
LARSA1-16L12C
LARSA1-16L12C Thumbnail
LARSA1-16L24C
LARSA1-16L24C Thumbnail
LARSA1-16L36C
LARSA1-16L36C Thumbnail
LARSACC-001
LARSACC-001 Thumbnail
LARSACC-002
LARSACC-002 Thumbnail
LARSACC-003
LARSACC-003 Thumbnail
LARSACC-004
LARSACC-004 Thumbnail
LARSACC-005
LARSACC-005 Thumbnail
LARSACC-006
LARSACC-006 Thumbnail
LARSACC-007
LARSACC-007 Thumbnail
LARSACC-008
LARSACC-008 Thumbnail
LARSACC-009
LARSACC-009 Thumbnail
LARSACC-010
LARSACC-010 Thumbnail
LARSACC-011
LARSACC-011 Thumbnail
LARSACC-012
LARSACC-012 Thumbnail
LARSACC-013
LARSACC-013 Thumbnail
LARSACC-014
LARSACC-014 Thumbnail
LARSACC-015
LARSACC-015 Thumbnail
LARSACC-016
LARSACC-016 Thumbnail
LARSB1-08L12C
LARSB1-08L12C Thumbnail
LARSB1-08L24C
LARSB1-08L24C Thumbnail
LARSB1-08L36C
LARSB1-08L36C Thumbnail
LARSB1-12L12C
LARSB1-12L12C Thumbnail
LARSB1-12L24C
LARSB1-12L24C Thumbnail
LARSB1-12L36C
LARSB1-12L36C Thumbnail
LARSB1-16L12C
LARSB1-16L12C Thumbnail
LARSB1-16L24C
LARSB1-16L24C Thumbnail
LARSB1-16L36C
LARSB1-16L36C Thumbnail
LARSD2-08T12BP2C
LARSD2-08T12BP2C Thumbnail


To learn more: https://www.automationdirect.com/linear-motion?utm_source=PBO9OjOfeao&utm_medium=VideoTeamDescription

(VID-MC-0020)

In this video we show how to rebuild and refurbish a Value Series Linear Slide/Actuator.

Online Support Page: https://community.automationdirect.com/s/?utm_source=PBO9OjOfeao&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Rebuilding a Value Series Linear Actuator can be a little tricky, so we’re going to quickly walk through the process step by step. All you need is a set of metric and imperial Allen wrenches, possibly a 12mm wrench and the appropriate re-build kit. I’m using this slide, which has a point 5 pitch on the lead screw, so I need this rebuild kit which is for the point 5 pitch value series slides. It has lubricant, new bearings, a new lead screw nut and a new set of liners. There’s another kit for the Value series slides with a point 2 pitch lead screw. These instructions are the same for any length slide; I’m using this short 6 inch slide for the demo because it is easier to fit on the video screen. Here we go. Loosen the shaft coupler on the Linear Slide side – not the motor side – remove the four motor screws and remove the motor, coupler and adapter plate. Loosen the set screw on the lead screws lock nut – don’t take the screw out, just loosen it a little bit. You can usually remove the lock nut by hand, but if it is tight, use a 12 mm wrench to loosen it. If you need to use a wrench, then go ahead and take one of the motor mount legs off to make the nut easier to reach. To get more torque, just move the carriage to the far end plate – that will lock the lead screw in place and make the nut easier to get off. Remove the screws holding the lead screw in, remove the motor end plate, and pull the leadscrew out. Remove the other end plate. Loosen the pre-load screws on the carriage – don’t take them all the way out, we don’t want the carriage to come apart, remove the carriage and replace all four liners. When you put the new ones in, there is a raised ring that sits in a groove on the carriage. Make sure that’s seated. Slide the carriage back onto the rails making sure this tab is on the same side as the proximity sensor mounts and also making sure the new liners are seated. If you have trouble getting it on, loosen these pre-load screws a little bit more. Once the carriage is on, lubricate the rails. There is a spring in the bottle you can use to help mix up the lubricant in case there was any settling. Apply a little lubricant to the rails and slide the carriage back and forth to help evenly spread the lubricant. There should be a thin even layer of lubricant on the rails. If not, add some more and move the slide around to distribute it. Tighten the preload screws until you feel a slight resistance. Adjust the screws until the carriage can be pushed with light effort. It shouldn’t move freely on its own. Replace the motor mount bearings with new ones and replace the bearing on the lead screw. I use the lead screw nut to push that last bearing off the lead screw and remove the lead screw nut at the same time. Replace the lead screw nut and bearing. Make sure the triangle flange faces the motor end of the leadscrew and move the nut up the screw a little ways. Insert the leadscrew into the motor mounting plate. Add the lock nut and tighten using just your fingers. Then tighten the set screw. The lead screw should spin freely. If not, then adjust the lock nut. Attach the end plate using the original screws. Don’t tighten it down yet – we need this loose so we can adjust it in a minute. Pass the lead screw through the carriage and seat the bearing into the end plate. Re-attach the motor end plate, again leaving it loose for the moment so we can adjust things. Fasten the new lead screw nut to the carriage using the original screws. Rotate the lead screw to move the carriage to the motor end plate and tighten the endplate screws to lock its position in place. Now move the carriage to the other end and tighten that end plate. Move the carriage back and forth several times the full length of the rails to make sure there isn’t any binding. If there is some binding then just repeat the previous steps until it moves nice and freely. When you are happy with that, go ahead and do any final tightening, attach the motor and tighten the shaft coupler. Apply a little lubricant to the screw and rails and then have the motor move the carriage up and down the slide a few times to spread the lubricant. Step by step instruction on how to do all of this are on the product page right here. If you have any questions about these linear slides, please contact AutomationDirect’s free award winning tech support during regular business hours. They will be happy to help. And don’t forget the forums. There are lots of folks there that love to share their years of experience. Just don’t post any questions directed at AutomationDirect’s support team, they don’t monitor the forums on a regular basis.



No data returned!
An error has occurred! Please contact support
Videos Home > Linear Slide Value Series Rebuild from AutomationDirect