Productivity Series EtherNet/IP Admontec ADAM-6050EI Remote I/O at AutomationDirect


Related Products

P1-540
P1-540 Thumbnail
P1-START
P1-START Thumbnail
MICSD-16G
MICSD-16G Thumbnail
P1-01AC
P1-01AC Thumbnail
P1-08ND3
P1-08ND3 Thumbnail
P1-08TD1
P1-08TD1 Thumbnail
P1-08TD2
P1-08TD2 Thumbnail
P1-15CDD1
P1-15CDD1 Thumbnail
P1-15CDD2
P1-15CDD2 Thumbnail
P1-16CDR
P1-16CDR Thumbnail
P1-08TRS
P1-08TRS Thumbnail
P1-16TR
P1-16TR Thumbnail
P1-04ADL-1
P1-04ADL-1 Thumbnail
P1-04ADL-2
P1-04ADL-2 Thumbnail
P1-04DAL-1
P1-04DAL-1 Thumbnail
P1-04DAL-2
P1-04DAL-2 Thumbnail
P1-04THM
P1-04THM Thumbnail
P1-04NTC
P1-04NTC Thumbnail
P1-08SIM
P1-08SIM Thumbnail
PS-PGMSW
PS-PGMSW Thumbnail
P2-550
P2-550 Thumbnail
P2-RS
P2-RS Thumbnail
P2-START2
P2-START2 Thumbnail
P2-04B
P2-04B Thumbnail
P2-07B
P2-07B Thumbnail
P2-11B
P2-11B Thumbnail
P2-15B
P2-15B Thumbnail
P2-01AC
P2-01AC Thumbnail
P2-01DCAC
P2-01DCAC Thumbnail
P2-08ND3-1
P2-08ND3-1 Thumbnail
P2-08NE3
P2-08NE3 Thumbnail
P2-16ND3-1
P2-16ND3-1 Thumbnail
P2-16NE3
P2-16NE3 Thumbnail
P2-32ND3-1
P2-32ND3-1 Thumbnail
P2-32NE3
P2-32NE3 Thumbnail
P2-08TD1S
P2-08TD1S Thumbnail
P2-08TD2S
P2-08TD2S Thumbnail
P2-08TD1P
P2-08TD1P Thumbnail
P2-08TD2P
P2-08TD2P Thumbnail
P2-15TD1
P2-15TD1 Thumbnail
P2-15TD2
P2-15TD2 Thumbnail
P2-16TD1P
P2-16TD1P Thumbnail
P2-16TD2P
P2-16TD2P Thumbnail
P2-32TD1P
P2-32TD1P Thumbnail
P2-32TD2P
P2-32TD2P Thumbnail
P2-08NAS
P2-08NAS Thumbnail
P2-16NA
P2-16NA Thumbnail
P2-08TAS
P2-08TAS Thumbnail
P2-16TA
P2-16TA Thumbnail
P2-08TRS
P2-08TRS Thumbnail
P2-16TR
P2-16TR Thumbnail
P2-04AD
P2-04AD Thumbnail
P2-08AD-1
P2-08AD-1 Thumbnail
P2-08AD-2
P2-08AD-2 Thumbnail
P2-08ADL-1
P2-08ADL-1 Thumbnail
P2-08ADL-2
P2-08ADL-2 Thumbnail
P2-16AD-1
P2-16AD-1 Thumbnail
P2-16AD-2
P2-16AD-2 Thumbnail
P2-16ADL-1
P2-16ADL-1 Thumbnail
P2-16ADL-2
P2-16ADL-2 Thumbnail
P2-04DA
P2-04DA Thumbnail
P2-04DAL-1
P2-04DAL-1 Thumbnail
P2-04DAL-2
P2-04DAL-2 Thumbnail
P2-08DA-1
P2-08DA-1 Thumbnail
P2-08DA-2
P2-08DA-2 Thumbnail
P2-16DA-1
P2-16DA-1 Thumbnail
P2-16DA-2
P2-16DA-2 Thumbnail
P2-08DAL-1
P2-08DAL-1 Thumbnail
P2-08DAL-2
P2-08DAL-2 Thumbnail
P2-16DAL-1
P2-16DAL-1 Thumbnail
P2-16DAL-2
P2-16DAL-2 Thumbnail
P2-8AD4DA-1
P2-8AD4DA-1 Thumbnail
P2-8AD4DA-2
P2-8AD4DA-2 Thumbnail
P2-08THM
P2-08THM Thumbnail
P2-06RTD
P2-06RTD Thumbnail
P2-08NTC
P2-08NTC Thumbnail
P2-SCM
P2-SCM Thumbnail
P2-HSI
P2-HSI Thumbnail
P2-HSO
P2-HSO Thumbnail
P2-08SIM
P2-08SIM Thumbnail
P3-550E
P3-550E Thumbnail
P3-550
P3-550 Thumbnail
P3-530
P3-530 Thumbnail
P3-RX
P3-RX Thumbnail
P3-EX
P3-EX Thumbnail
P3-03B
P3-03B Thumbnail
P3-05B
P3-05B Thumbnail
P3-08B
P3-08B Thumbnail
P3-11B
P3-11B Thumbnail
P3-01AC
P3-01AC Thumbnail
P3-01DC
P3-01DC Thumbnail
P3-08ND3S
P3-08ND3S Thumbnail
P3-16ND3
P3-16ND3 Thumbnail
P3-32ND3
P3-32ND3 Thumbnail
P3-64ND3
P3-64ND3 Thumbnail
P3-08TD1S
P3-08TD1S Thumbnail
P3-08TD2S
P3-08TD2S Thumbnail
P3-16TD1
P3-16TD1 Thumbnail
P3-16TD2
P3-16TD2 Thumbnail
P3-32TD1
P3-32TD1 Thumbnail
P3-32TD2
P3-32TD2 Thumbnail
P3-64TD1
P3-64TD1 Thumbnail
P3-64TD2
P3-64TD2 Thumbnail
P3-08NAS
P3-08NAS Thumbnail
P3-16NA
P3-16NA Thumbnail
P3-08TAS
P3-08TAS Thumbnail
P3-16TA
P3-16TA Thumbnail
P3-08TRS
P3-08TRS Thumbnail
P3-08TRS-1
P3-08TRS-1 Thumbnail
P3-16TR
P3-16TR Thumbnail
P3-04ADS
P3-04ADS Thumbnail
P3-08AD
P3-08AD Thumbnail
P3-16AD-1
P3-16AD-1 Thumbnail
P3-16AD-2
P3-16AD-2 Thumbnail
P3-08RTD
P3-08RTD Thumbnail
P3-08THM
P3-08THM Thumbnail
P3-04DA
P3-04DA Thumbnail
P3-08DA-1
P3-08DA-1 Thumbnail
P3-08DA-2
P3-08DA-2 Thumbnail
P3-06DAS-1
P3-06DAS-1 Thumbnail
P3-16DA-1
P3-16DA-1 Thumbnail
P3-16DA-2
P3-16DA-2 Thumbnail
P3-8AD4DA-1
P3-8AD4DA-1 Thumbnail
P3-8AD4DA-2
P3-8AD4DA-2 Thumbnail
P3-SCM
P3-SCM Thumbnail
P3-HSI
P3-HSI Thumbnail
P3-HSO
P3-HSO Thumbnail
P3-16SIM
P3-16SIM Thumbnail


To learn more: https://www.automationdirect.com/productivity?utm_source=P51t0BO8kE4&utm_medium=VideoTeamDescription

(VID-P3-0045)

Watch this demo to see how easy it is to set up implicit (connected) EtherNet/IP messaging between a Productivity series controller and an Advantech ADAM-6150EI Remote I/O module.
**Correction Note: The Correct Advantech part number is: ADAM-6150EI, not ADAM-6050EI.

**Requires Productivity Suite Software 1.10.0.10 or later.

Online Support Page: https://community.automationdirect.com/s/?utm_source=P51t0BO8kE4&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

The Productivity 3000’s Ethernet IP feature makes using the Advantec ADAM Remote IO a snap. We just want the input data collected by the ADAM module to appear in the Productivity 3000, and we want output data written to a TAG in the Productivity 3000, to appear on the outputs of the ADAM Remote IO device. We’ll that’s just the Implicit – or IO – messaging of the Ethernet IP standard, right? So we just setup the Productivity 3000 as a scanner and connect it to the ADAM Remote IO module via Ethernet and we are done. And the Productivity 3000 software makes it so easy – here we go … Ok, I’ve already opened up a new project, ran an auto-detect on the hardware to configure it and am online with the Productivity 3000. To setup a scanner, you just double click on Hardware Configuration, the Ethernet/IP tab. And drag a generic Client over into this area over here. Now we just fill in the blanks. Let’s give it a name – I’ll call this m ADAM 6050. I need to enter the IP address of the Adam module right here. And I’ll go ahead and fill in these tags here so we can monitor the status of the scanner. We already know we want to use the I/O messaging – not the explicit messaging. So we select that one. And now we have some more blanks to fill in. First we need to create a tag we can use to turn the scanner on and off. Then I’ll go ahead and create some tags so we can monitor the status of this connection. And finally fill in the details of the Adam Device. The first tab is the target to originator –that’s the Adam device to us – our input. We want that to be delivered in a unicast so it only comes to us. We’ll have the Adam device send that four times a second. That’s fine. The connection point for the Adam Device Input Channel is 102. And I need to create a tag for that input data to end up in. So I’ll call that my 6050 input. As soon as I click away, the Productivity 3000 reminds me that I haven’t defined that tag yet and gives me a chance to do so. So let’s see, we know the Adam device is sending us a 16 bit unsigned integer. So let’s change it to that. And it’s only sending one, so one column is all I need. Perfect. Now, normally in these arrays you have multiple elements and you can select how many you want ot send. We only have one so of course it’s going to send us that one. Great, so it’s going to send us a unicast message, four times a second, from this connection point, and it’s going to put this result I this array which is only one element large. Let’s do the same thing for the output data. This is the data sent from us – the originator – to the target which is the Adam device. We’ll send that data four times a second. Note that this rate does not have to be the same as the input data array. The connection point for the out put on the Adam is 101. We need to create a data array to put the data into so we can transfer it down to the Adam, and again when we click away the software reminds us that we haven’t actually created that tag yet. That’s another 16 bit unsigned integer and it’s only one element large. And of course, we’re going to send that one element down the pipe. Some devices require a four byte status header to be sent with the output data. The Adam device is one of those so we definitely want to make sure this box is checked. Under configuration data, that connection point is 100. And again, I just got that from the Adam documentation. We need to create a data array for this. And when we click away the software reminds us we haven’t created that yet. So we’ll make that a 16 bit unsigned integer, one element. Now some EtherNet/IP devices, while they require this configuration data, don’t really us to send any data with it. And that is the case with the Adam I/O device. This is zero length data, but we still need to send this field. So great. We gave it a name and defined some status tags. We tell the Productivity 3000 the name of IP address Adam device. And then we setup the I/O messaging for the Input, output, and configuration data. And that’s it. We’re done. Now since I hit OK, the Productivity 3000 is reminding me that I created a bunch of new tags and that I haven’t defined them yet. It’s recommending these types which all look great. The exception is the string. I really like to make this string kind of long so it can handle anything that might come down the pipe. Give me a second while I change these. And great, now all of our tags are defined. Well, that’s it! We setup a scanner the Adam 6050 Remote IO device. I do want to do one more thing though. Let’s go back into the device and click this monitor button. What that does is it takes all of these tags we created and builds a data view for us. I really love that feature so I don’t have to do that manually myself. We’ll call it the ADAM 6050. Great. Close all of this stuff out. We’re already on-line with the Productivity 3000 so al we have to do is transfer this program o the controller. And we’re good to go. Ok, let’s see what’s going on. Bring up that dataview. And here are all the tags we created. In particular, here’s our input array, output array and our configuration data. To turn this scanner on, all we have to do is toggle that enable bit we created. So I’ll toggle that. Write it out. And look – we’re connected to the Adam Device, and we have a successful connection. So now that we are enabled data is begin transferred back and forth between the Adam Device and the Productivity 3000. Well, let’s try it. The inputs on this ADAM device are pulled up, so if I simply ground the D0 pin, the sure enough, the data is transferred fro the Adam device to the Productivity3000 in the background and it just appears in this input array we just created right here at the D0 bit. If I release that one and ground the D1 bit, then sure enough that information is transferred from the Adam Device up to the Productivity 3000 and drops into this input array we created. Note that on the productivity 3000 it’s easy to change the view of this. Right now we’re viewing it in decimal, let’s change that view to hex and see how that looks. And there it is. It’s a little easier to read that way. Ok, let’s do one more. I’m going to ground pin D7 and see what happens. And sure enough that input data is transferred from the Adam remote IO device, up to the Productivity 3000 and dropped into this input array where our ladder logic can use it how ever it wants. Perfect. And again, keep in mind, this is all automatically happening in the background. Our ladder code doesn’t have to do anything to fetch that data. It’s just there ready to use. How about the output data? Well, it’s the exact same thing. We just modify this array and the EtherNet/IP automatically transfers that down to the ADAM device for us. Let’s try it. I have some LEDs connected to the output pins on this Adam device so we can see the results. Note that on this device, it’s the upper 8 bits of the 16 bit word that drives the outputs. So let’s change this output to hex so it’s easier to see. And let’s turn on that 8th bit – which will be output bit 0 on the device. Write that out and sure enough output bit D0 lights up. Let’s try D1. And sure enough that lights up. Let’s go crazy here. Let’s put alternating bits in. And sure enough those light up. Normally your ladder code would set these bits, of course. We’re just using the dataview here because it’s easy and to show you that no ladder code is required to do the actual transfer of the data down to the ADAM device. So bottom line here is all we did is to setup a scanner to talk to the ADAM IO device, we just went to Hardware Configuration, we dropped a generic client in here and filled in the blanks. Once we were done with that, we brought up our dataview, enabled the device, we checked that we were connected and had a successful connection. Then all we had to do was watch the input values as they changed on the device, and write output values to drive the output pins on the device. That’s it. That’s all there is to setup a Productivity 3000 to work with an Advantec Adam remote IO device. Could we add more devices? Sure! Go back to hardware configuration, grab another generic client, fill in the blanks. You can add as many as you want to. It’s easy. Check out the other videos in this series for more tips on using EtherNet/IP with the Productivity 3000. Performance plus value. That’s productivity. From automation direct.



No data returned!
An error has occurred! Please contact support
Videos Home > Productivity Series EtherNet/IP Admontec ADAM-6050EI Remote I/O at AutomationDirect