Visit www.AutomationDirect.com for products and prices. (VID-MC-0045)
Have a look at this nifty stepper drive from Ever Motion Solutions. AutomationDirect sells these “Titanio” series drives in several variations based on motor size and power, as well as position feedback from an encoder. Not gonna lie, the name is pretty cool too… “Titanio!” These are pulse commanded drives, and we offer options for AC and DC power input. We have simple dipswitch configuration for the basic drives, as well as high-end software configuration for the more advanced drives in the series. As an added feature, these drives offer sinusoidal current control which removes some of the jitters and vibrations usual with stepper systems. If you need a stepper drive that’s smooth as butter, offers stall detection and closed loop control, at a ridiculously low price, then take a look at the Titanio series by Ever, from AutomationDirect. You can find them on our webstore…. AutomationDirect.com
Voted #1 mid-sized employer in Atlanta
Check out our
job openings