WEG CFW300 & CFW320 VFD Maintenance Made Easy from AutomationDirect


Related Products

CFW300A01P6S1NB20
CFW300A01P6S1NB20 Thumbnail
CFW300A06P0S1NB20
CFW300A06P0S1NB20 Thumbnail
CFW300A01P6S2NB20
CFW300A01P6S2NB20 Thumbnail
CFW300A02P6S2NB20
CFW300A02P6S2NB20 Thumbnail
CFW300A04P2S2NB20
CFW300A04P2S2NB20 Thumbnail
CFW300A06P0S2NB20
CFW300A06P0S2NB20 Thumbnail
CFW300A07P3S2NB20
CFW300A07P3S2NB20 Thumbnail
CFW300A01P6T2NB20
CFW300A01P6T2NB20 Thumbnail
CFW300A02P6T2NB20
CFW300A02P6T2NB20 Thumbnail
CFW300A04P2T2NB20
CFW300A04P2T2NB20 Thumbnail
CFW300A06P0T2NB20
CFW300A06P0T2NB20 Thumbnail
CFW300A07P3T2NB20
CFW300A07P3T2NB20 Thumbnail
CFW300B10P0B2DB20
CFW300B10P0B2DB20 Thumbnail
CFW300B15P2T2DB20
CFW300B15P2T2DB20 Thumbnail
CFW300-CRS232
CFW300-CRS232 Thumbnail
CFW300-CRS485
CFW300-CRS485 Thumbnail
CFW300-CUSB
CFW300-CUSB Thumbnail
CFW300-KHMIR
CFW300-KHMIR Thumbnail
CFW300-IODR
CFW300-IODR Thumbnail
CFW300-IOAR
CFW300-IOAR Thumbnail
CFW300-IOADR
CFW300-IOADR Thumbnail
CFW300-IOAENC
CFW300-IOAENC Thumbnail
CFW300-KFA-S1-S2
CFW300-KFA-S1-S2 Thumbnail
CFW300-KFB-S2
CFW300-KFB-S2 Thumbnail
CFW-WPS
CFW-WPS Thumbnail
CFW300-FAN-A
CFW300-FAN-A Thumbnail
CFW300-FAN-B
CFW300-FAN-B Thumbnail
CFW320A01P6S1NB20
CFW320A01P6S1NB20 Thumbnail
CFW320A02P6S1NB20
CFW320A02P6S1NB20 Thumbnail
CFW320A04P2S1NB20
CFW320A04P2S1NB20 Thumbnail
CFW320A06P0S1NB20
CFW320A06P0S1NB20 Thumbnail
CFW320A01P6S2NB20
CFW320A01P6S2NB20 Thumbnail
CFW320A02P6S2NB20
CFW320A02P6S2NB20 Thumbnail
CFW320A04P2S2NB20
CFW320A04P2S2NB20 Thumbnail
CFW320A06P0S2NB20
CFW320A06P0S2NB20 Thumbnail
CFW320A07P3S2NB20
CFW320A07P3S2NB20 Thumbnail
CFW320A01P6T2NB20
CFW320A01P6T2NB20 Thumbnail
CFW320A02P6T2NB20
CFW320A02P6T2NB20 Thumbnail
CFW320A04P2T2NB20
CFW320A04P2T2NB20 Thumbnail
CFW320A06P0T2NB20
CFW320A06P0T2NB20 Thumbnail
CFW320A07P3T2NB20
CFW320A07P3T2NB20 Thumbnail
CFW320B10P0B2DB20
CFW320B10P0B2DB20 Thumbnail
CFW320B15P2T2DB20
CFW320B15P2T2DB20 Thumbnail
CFW320A01P1T4NB20
CFW320A01P1T4NB20 Thumbnail
CFW320A02P6T4NB20
CFW320A02P6T4NB20 Thumbnail
CFW320A03P5T4NB20
CFW320A03P5T4NB20 Thumbnail
CFW320A04P8T4NB20
CFW320A04P8T4NB20 Thumbnail
CFW320B07P6T4NB20
CFW320B07P6T4NB20 Thumbnail
CFW320C11P0T4NB20
CFW320C11P0T4NB20 Thumbnail
CFW320C14P0T4NB20
CFW320C14P0T4NB20 Thumbnail
CFW320B01P1T4DB20
CFW320B01P1T4DB20 Thumbnail
CFW320B02P6T4DB20
CFW320B02P6T4DB20 Thumbnail
CFW320B03P5T4DB20
CFW320B03P5T4DB20 Thumbnail
CFW320B04P8T4DB20
CFW320B04P8T4DB20 Thumbnail
CFW320B07P6T4DB20
CFW320B07P6T4DB20 Thumbnail
CFW320C11P0T4DB20
CFW320C11P0T4DB20 Thumbnail
CFW320C14P0T4DB20
CFW320C14P0T4DB20 Thumbnail


To learn more: https://www.AutomationDirect.com/drives?utm_source=MRn78K4i6rQ&utm_medium=VideoTeamDescription

(VID-DR-0072)

Regular maintenance of your WEG VFD motor control can extend the life of the drive and save you money. This video shows you how to swap out old fan modules, reform capacitors, and what kinds of VFD periodic maintenance should be done and how often. The CFW300/320 drive is a low cost VFD with high end features like a built-in PLC, Dynamic Braking, Fire Mode, PID, 65,000A SCCR, Zero Stack foot print, Multi-Speed, etc and is even cULus listed!

Online Support Page: https://community.automationdirect.com/s/?utm_source=MRn78K4i6rQ&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Taking care of your WEG CFW300 Drive is easy. Just replace the fan periodically, reform the capacitors, and do the regular periodic inspections. To replace the fan - Pop the old one out. Drop a new one in. It’s recommended that the fan be replaced every 40,000 hours of run time under normal conditions – your mileage may vary depending on your environment. That’s Fan run time – not drive run time. When the fan run time exceeds 50,000 hrs., the drive will generate a 177-alarm reminding you to replace the fan. You can see the current fan run time in parameter 45. That’s a hex number so it can go to a hexadecimal four f’s - which is a little over 65,000 hrs. Once you have replaced the fan, reset the fan time that’s shown in parameter 45 by going to parameter 204 and entering a thirteen. If we go back to parameter 45 – we see our fan time is now zero. Perfect. One thing to be aware of is the fan time shown in parameter 45 is only updated when the drive is power cycled. That’s because normally you would only want to check it during your regular maintenance schedule. So, don’t expect to see parameter 45 update each hour on the LCD while the drive runs. Parameter 352 allows you to control how the fan operates. You can turn it off, have it always on, or let the drive decide when it needs to be on – which is the default and what you probably want to be using. Maintaining the drives capacitors is crucial to preventing pre-mature failure. And it’s easy. If your drive hasn’t had power applied in over a year, then just apply whatever power your drive would normally expect for at least one hour. Then disconnect the drive from the power source and let it sit for at least 24 hours before using it. Why is this important? A capacitor is basically two metal plates with opposing charge. The charges are kept separate from each other by an insulating layer. The electrolytic capacitors in a drive typically use paper soaked in an electrolytic solution. When the electrolyte is kept charged, it forms an oxide layer on the anode plate and it is that oxide layer that serves as the insulator between the two metal plates. If the electrolyte isn’t kept charged, the oxide layer degrades, which means the two metal plates aren’t very well insulated from each other and you ultimately get something very close to a short circuit. So, now when you apply power to the drive, current passes straight through causing everything to get really hot which boils the electrolyte, burns up the metal plates and causes the electrolytic capacitor to explode. Which not only destroys the capacitor but all the stuff around it too because the gases that are released are caustic. So, if your drive has been sitting for a while – roughly a year or so – PLEASE take the time to reform the capacitors. By the way, it’s called reforming the capacitors because you are literally reforming that oxide layer by applying voltage in a controlled manner. What about that drive you just got form the factory? Does it need to be reformed? It certainly can’t hurt, but the easiest way to tell is to look at the label. This code right here is the week and year the drive was manufactured. So, if it has been a year since the drive was manufactured, then will definitely want to reform the capacitors. And finally, every 6 months, inspect the items listed in table 6.3 of the drive’s user manual. The manual even has step by step procedures for cleaning the ventilation System and Circuit Cards. Well, that’s about it for drive maintenance. Click here to learn more about the WEG CFW300 Variable Frequency Drive. Click here to learn about AutomationDirect’s free award-winning support options and click here to subscribe to our YouTube Channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > WEG CFW300 & CFW320 VFD Maintenance Made Easy from AutomationDirect