AutomationDirect
Login | Register
Accounts & Orders
Cart
12
$2,838.50

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $2,838.50
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
Videos Home > WEG CFW500 VFD PID Pump Genius...

WEG CFW500 VFD PID Pump Genius Simplex Part 2 from AutomationDirect


Related Products

15342909
15342909 Thumbnail
15572819
15572819 Thumbnail
15572908
15572908 Thumbnail
15573714
15573714 Thumbnail
15573819
15573819 Thumbnail
15573823
15573823 Thumbnail
15575568
15575568 Thumbnail
15575577
15575577 Thumbnail
15575665
15575665 Thumbnail
15575699
15575699 Thumbnail
15575707
15575707 Thumbnail
15576919
15576919 Thumbnail
15577021
15577021 Thumbnail
15577211
15577211 Thumbnail
15577452
15577452 Thumbnail
15733937
15733937 Thumbnail
15734064
15734064 Thumbnail
15734119
15734119 Thumbnail
14990863
14990863 Thumbnail
14991103
14991103 Thumbnail
14991753
14991753 Thumbnail
14938005
14938005 Thumbnail
14938047
14938047 Thumbnail
14938113
14938113 Thumbnail
14975838
14975838 Thumbnail
14938655
14938655 Thumbnail
14991953
14991953 Thumbnail
14992148
14992148 Thumbnail
14976517
14976517 Thumbnail
14976809
14976809 Thumbnail
14977065
14977065 Thumbnail
14977266
14977266 Thumbnail
14977397
14977397 Thumbnail
14978365
14978365 Thumbnail
14978573
14978573 Thumbnail
14989840
14989840 Thumbnail
14990985
14990985 Thumbnail
14991517
14991517 Thumbnail
14937890
14937890 Thumbnail
14938041
14938041 Thumbnail
14938111
14938111 Thumbnail
14975783
14975783 Thumbnail
14938547
14938547 Thumbnail
14991899
14991899 Thumbnail
14992113
14992113 Thumbnail
14975888
14975888 Thumbnail
14976683
14976683 Thumbnail
14976814
14976814 Thumbnail
14977261
14977261 Thumbnail
14977391
14977391 Thumbnail
14977629
14977629 Thumbnail
14978548
14978548 Thumbnail
15342760
15342760 Thumbnail
15570800
15570800 Thumbnail
15571879
15571879 Thumbnail
15571881
15571881 Thumbnail
15574655
15574655 Thumbnail
15575067
15575067 Thumbnail
15572625
15572625 Thumbnail
15572689
15572689 Thumbnail
15575202
15575202 Thumbnail
15575701
15575701 Thumbnail
15575716
15575716 Thumbnail
15576540
15576540 Thumbnail
15577077
15577077 Thumbnail
15342437
15342437 Thumbnail


To learn more: https://www.AutomationDirect.com/drives?utm_source=JXV7P81yb_c&utm_medium=VideoTeamDescription

(VID-DR-0337)

The Pump Genius makes configuring Pumping applications a snap. From single pumps to multi-pump systems, the Pump Genius walks you through building an app to suit your specific needs and then it walks you through configuring the parameters. All you have to do is load it into the drive and run it. Follow us in this three part series as we do exactly that:
Part 1: Build a Pump Genius App for our specific application
Part 2: Configure the Parameters
Part 3: Try it!

Online Support Page: https://community.automationdirect.com/s/?utm_source=JXV7P81yb_c&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

In Part 1, we reset the drive to factory default and reset the SoftPLC to factory default. We then set up the motor parameters, built a Pump Genius for our specific drive and downloaded it to the drive. In this video, we’ll configure the parameters for the Pump Genius. The good news is the Pump Genius is very capable. The bad news is that means there are a lot of parameters to configure. The good news is, WLP has a Pump Genius wizard that walks us through it one little step at a time. If you haven’t done so already, double click over here to bring up that wizard. We see this is a simplex version of the Pump Genius – that is, we are only using one motor and pump. Next. First, we set up the local and remote speed reference and control inputs. In the PID Quick Start videos, we used remote only so we’ll do that here too. In remote mode when we are running the Pump Genius, the SoftPLC will control the speed reference, we don’t care about forward and reverse so I’ll set it to not used, and run/stop will be controlled by a digital input. Next dialog. We’ll use the default Digital Input 1 to control run/stop – which is what we did in the PID Quick Start video. We also used Digital Input 2 to control the auto/manual mode of PID. But the Pump Genius doesn’t allow that. You have to use Digital Input 3. We changed that wire on our test set in Part 1. We didn’t use any other inputs and we didn’t use any outputs in the PID Quick Start videos. You would normally set the outputs to drive a process running light, a fault beacon, or one of the fault conditions. We’ll just turn those off for now. Next. Here we set up our ramp times. You want to keep those as short as is reasonable so they don’t interfere with PID's ability to do it’s thing. In the Quick Start videos, we used .2 seconds which was something you would probably never use, but we’ll do that here to keep things as similar as possible to those Quick Start videos. Also as we explained in the PID Quick Start videos, these min and max values are really important. Mostly make sure the min speed is a little above where the pump stops pumping and the max speed is the motor speed that max’s out your sensor. This is what we used in the PID Quick Start videos. You can watch those videos to find out why. Next. The process variable is coming in on Analog Input 1. Next. Tell Analog Input 1 he is the process variable, we’re using a 0-10 volt sensor, our units are psi, and we’ll use 1 decimal point. Don’t forget to make sure the DIP switch on the I/O module is set to volts. This is where you set up the analog input. We don’t need an offset, gain of 1 is good, and I always like to add a little filtering – just keep it small or it will make PID less responsive. These go with the min and max speed we set back here. So, when the motor runs from the min to max speed, our sensor runs from zero to 15 psi. Notice this uses our engineering units. This is what PID uses to calibrate all of its calculations so make sure you get this right. Again, see the PID Quick Start video for more info on that. Next. This is a forward or direct PID loop. That is, the pressure goes up when the motor speed goes up. Reverse would be like a cooling system, where the process variable – the temperature – goes down when the motor speed goes up. Next. Do we want the Pump Genius to always run automatically, control it manually or use a digital input to switch between the two? We used a digital input to switch between automatic and manual modes in the PID Quick Start so that’s what we’re doing here. This just says use the digital input we assigned in Parameter 265 back in the second dialog to control this switch. So Digital Input 3 will decide if we send the PID result or a value that we manually set out to the drive. This is the bumpless mode we talked about in the PID Quick Start. We’ll leave that off again, but in most applications you will usually want to enable it. Check out the bumpless videos to learn more about that. We’ll use the Pump Genius default coefficients which are a little different from what we used in the previous PID Quick Start videos. And we’ll start the manual setpoint at 0 Hertz so we aren’t surprised when we turn this thing on. Next. We want the setpoint to be controlled by the drives keypad – which can also be controlled by a network write. Next. We want to use the same 6 psi setpoint as the quick start. Again, that’s in engineering units. By the way, if you mess up on any of these dialogs, there’s a handy default button down here which will reset that dialog. I’ve used that more than once … and hit Next. We’ll skip sleep mode for this demo. There’s a whole separate video on that if you want to learn more. It’s great for tank filling applications or any time you want PID to sleep until there is demand. Since we aren’t using that we skip the sleep mode configuration dialogs and go from this Dialog 11 all the way to Dialog 14 where can add pipe charging. If enabled, it will turn the motor on like this for this much time to pre-fill the pipes before reverting to PID control. This is common in irrigation systems or if you just need to prime your system. You can also specify a maximum amount of amps allowed during pipe charging so you don’t overload your system during this time. We won’t be doing pipe charging in this demo, so we hit Next. Here we can set up our high and low-level alarms. Normally, you would want to set the high alarm below the pipes burst pressure and the low alarm to whatever your system needs. You’ll get an alarm when either happens and after the time specified you’ll get a fault and the drive will shut down. For this demo, we’ll disable the faults by leaving their times set at zero. And make sure the alarms are beyond our zero to 15 psi range just to keep things simple. Next. You can set up a dry pump alarm. That is if the motor speed revs up or the torque drops because there is no load, issue an alarm and after so many seconds, issue a fault and shut the system down. We’ll disable that by setting these beyond the min and max speeds we set in the third dialog and leaving the fault time at zero seconds. You can also have an external sensor – maybe something that is detecting low suction for example – and if that sensor which is normally closed opens, then you get an alarm and some time later get a fault that shuts the system down. We’ll leave that disabled. You can also do that with an analog input. We’ll skip that too which allows us to skip a few more dialogs. You can derag the pump on startup, a digital input, or if clogging is detected. Deragging automatically reverses the motor to clean off the impeller. That’s primarily for waste-water applications. We’ll leave that off. We want the setpoint on the first line of the display, the process variable on the second line and the current in amps on the last line. And we’re done configuring the Pump Genius parameters! I like to drag to select this parameter summary, copy it and paste it into a document so I have a written record of all the parameter values. You can also print it to all the usual places including PDF. Hit Finish and it asks you if you want to send the values to the drive. Sure. And of course, remember to save the project so you don’t lose everything you’ve done. Ok, in Part 1 we put the Pump Genius app in the drive and in this part we configured the parameters. The drive is ready to go. Join me in Part 3 where we will do a live demo of the Pump Genius in operation. Meanwhile, click here to learn more about the WEG CFW500 drive. Click here to learn about AutomationDirect’s Free award winning support options, and click here to subscribe to our YouTube channel so you’ll be notified when we publish more videos like this one.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info