Trumeter ADM Graphical Panel Meter Configure Alarm Setpoints & Outputs from AutomationDirect


Related Products

ADM100-LP
ADM100-LP Thumbnail
ADM100-LN
ADM100-LN Thumbnail
ADM100-HP
ADM100-HP Thumbnail
ADM100-HN
ADM100-HN Thumbnail


To learn more: https://www.automationdirect.com/graphical-panel-meters?utm_source=JHO2I13ALzs&utm_medium=VideoTeamDescription

(VID-PPO-0003)

This video detail how to setup the Trumeter ADM Graphical panel meter alarm setpoint and configure the outputs.

Online Support Page: https://community.automationdirect.com/s/?utm_source=JHO2I13ALzs&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Trumeter ADM panel meters feature two setpoint alarms that can easily be configured using the ADM Configurator software. See this link above to download the software, now. In the software you have a tab for each alarm. Here you can define the type of physical output for this alarm. These can be used to output to a PLC, an audible alarm, or any other monitoring device. If you set this up for analog output, here is where you would setup the scale for your 4-20 ma signal. Here you define the alarm condition. I am setting my alarm 1 condition to be when the voltage drops below 12 Volts, which is the midpoint of my scale. By checking here, you can assign if SP1 turns on or off based upon this alarm condition. Now, if you don’t want the physical output to turn on or off just uncheck this box, here. This defines how the Backlight changes based upon this alarm. I am selecting it to flash Red when this alarm is active. Here is where you are going to define your alarm text. This text will replace the message shown here while in alarm 1condition. Now, that sets up for Alarm 1. Alarm 2 is independent, but sets up just the same but make sure to note that the Alarm 2 condition has priority over alarm 1. This just means that if Alarm 1 and Alarm 2 are active at the same time, Alarm 2 is the one that will display on the panel. To send this configuration to the panel, select here and then select to write the configuration. Now, when my panel goes into alarm 1 condition it looks like this. To see more setup videos for the ADM panel meters select here. If you have any questions, please feel free to comment below or call into our technical support team. And select here to subscribe to our YouTube channel for upcoming products and solutions.



No data returned!
An error has occurred! Please contact support
Videos Home > Trumeter ADM Graphical Panel Meter Configure Alarm Setpoints & Outputs from AutomationDirect