AutomationDirect
Login | Register
Accounts & Orders
Cart
2
$95.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $95.00
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
Videos Home > DirectLOGIC Motion Control: Po...

DirectLOGIC Motion Control: Position of a Part on a Conveyor (Part 3 of 8) from AutomationDirect


Related Documents


Motion Control - Slides


DirectSOFT5 Project file


CTRIO Workbench Project file


C-more Micro-Graphic Project file



Related Products

STP-DRV-4850
STP-DRV-4850 Thumbnail
STP-DRV-6575
STP-DRV-6575 Thumbnail
STP-DRV-80100
STP-DRV-80100 Thumbnail
STP-MTR-17040
STP-MTR-17040 Thumbnail
STP-MTR-17040D
STP-MTR-17040D Thumbnail
STP-MTR-17048
STP-MTR-17048 Thumbnail
STP-MTR-17048D
STP-MTR-17048D Thumbnail
STP-MTR-17060
STP-MTR-17060 Thumbnail
STP-MTR-17060D
STP-MTR-17060D Thumbnail
STP-MTR-23055
STP-MTR-23055 Thumbnail
STP-MTR-23055D
STP-MTR-23055D Thumbnail
STP-MTR-23079
STP-MTR-23079 Thumbnail
STP-MTR-23079D
STP-MTR-23079D Thumbnail
STP-MTR-34066
STP-MTR-34066 Thumbnail
STP-MTR-34066D
STP-MTR-34066D Thumbnail
STP-MTRH-23079
STP-MTRH-23079 Thumbnail
STP-MTRH-23079D
STP-MTRH-23079D Thumbnail
STP-MTRH-34066
STP-MTRH-34066 Thumbnail
STP-MTRH-34066D
STP-MTRH-34066D Thumbnail
STP-MTRH-34097
STP-MTRH-34097 Thumbnail
STP-MTRH-34097D
STP-MTRH-34097D Thumbnail
STP-MTRH-34127
STP-MTRH-34127 Thumbnail
STP-MTRH-34127D
STP-MTRH-34127D Thumbnail
STP-PWR-3204
STP-PWR-3204 Thumbnail
STP-PWR-4805
STP-PWR-4805 Thumbnail
STP-PWR-4810
STP-PWR-4810 Thumbnail
STP-PWR-7005
STP-PWR-7005 Thumbnail


To learn more: https://www.automationdirect.com/motion-controlutm_source=J8_Kdyq9G0A&utm_medium=VideoTeamDescription

(VID-MC-0007)

Part 3 of 8, In this video I will cover some of the typical Motion Control applications that are used with stepping systems, and then explain the hardware for the linear slide application I am using for the video series demonstration.

**Take-away PDF and three application software projects can be found below.
**Storyboard Handout take-away:
https://www.automationdirect.com/resources/microsites/videos/take_aways/VID_L_PC_DL_STP_001-A.pdf
**DirectSOFT5 Project File take-away:
https://www.automationdirect.com/resources/microsites/videos/take_aways/motion%20control%20demo%20-%20directsoft5%20project.zip
**CTRIO Project file take-away:
https://www.automationdirect.com/resources/microsites/videos/take_aways/motion%20control%20demo%20-%20ctrio%20workbench.zip
**C-more Micro-Graphic Project File take-away:
https://www.automationdirect.com/resources/microsites/videos/take_aways/motion%20control%20demo%20-%20c-more%20micro%20project.zip
**SureStep User Manual: https://bit.ly/r5dgUO
**Starting with Steppers, Part 1: https://bit.ly/J5U0tN
**Starting with Steppers, Part 2: https://bit.ly/IQSjUb

Online Support Page: https://community.automationdirect.com/s/?utm_source=J8_Kdyq9G0A&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

In the following video I will cover some of the typical Motion Control applications that are used with stepping systems, and then explain the hardware for the linear slide application I am using for the video series demonstration. One of the most popular applications using a stepping system for Motion Control involves converting a stepping motor’s rotary motion into linear motion. This is accomplished with the use of a leadscrew. As the leadscrew rotates, a matched threaded nut, that is mechanically adapted to a slide mechanism, moves the slide along guides. The slide usually rides on two rods with rotating ball bearings attached to the slide. This arrangement provides the mechanical translation from rotary to linear motion. The slide is moved from position to position, as needed, to perform the work or sequences the process requires. The number of threads per inch, or pitch, determines the distance the slide mechanism will travel. For example, if we use a lead screw with 10 threads per inch, then one revolution of the attached stepping motor will cause the lead screw to produce 0.100 inches of travel. Let’s call it a tenth of an inch of travel. Using a stepper motor to drive a conveyor belt is another typical application. In this type of application we would be able to precisely control the position of a part on the conveyor, stop the part at various positions, back the belt up if the process required a second look be taken, such as a visual inspection, and then either move the part to an acceptance area, or possibly stop it a short distance from the inspection point, and then eject it into a rejection bin. The part’s position on the conveyor could be altered on the fly to suit changing conditions. Complex movements can also be handled with a stepping motor driving a conveyor. Different speed rates can be programmed, along with various acceleration and deceleration times, synchronizing with other devices in the process. A stepper motor coupled to a rotary table provides a simple method for indexing a table into precise locations. This type of application is ideal for assembly machines that may have multiple locations where various steps or operations are preformed. The use of a stepper motor can provide excellent repeatability between the various stations on an assembly machine. The same locations can be accurately returned to with each move. Another great benefit of using a stepper motor for this type of applications, and others, is the stepper motor cannot be damaged by mechanical overload. I chose a linear leadscrew slide driven with a SureStep stepper motor as my demonstration for this video series. The linear slide has a total travel distance of 300 millimeters, or approximately 11 and 3/4 inches if you prefer. The linear slide includes a mounting adapter that can accept a NEMA 23 frame size. The slide also includes a shaft coupler that matches the lead screw’s shaft diameter to the stepper motor's shaft diameter. The leadscrew on the slide has eight threads per inch. This means the slide will move a total of one inch for eight full revolutions of the leadscrew. In general practice, inch based leadscrews are defined in terms of Threads per Inch, abbreviated as TPI. Metric leadscrew threads are generally defined by ‘Pitch’. Without trying to be too confusing, I could say my slide leadscrew has a ‘Pitch’ of 1/8 inch or 0.125 inches. What does this mean? The slide can move a distance of 0.125 inches for every revolution of the stepping motor. Based on the 2,000 micro stepping steps per revolution I will use from the SureStep drive, my slide will move 0.0000625 inches per step! In Part Four, I will cover the wiring of the Motion Control demonstration, show how to configure the CTRIO module’s jumpers, and then show how to set the STP-DRV-4035 drive’s DIP switch parameters to match my application selections. Motion Control – VID: L-PC-DL-STP-001-3 Part 3 of 8 – Typical Stepping System Applications & Demo Linear Slide Hardware 0 2
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info