https://www.automationdirect.com/do-more?utm_source=HX1th57oYeU&utm_medium=VideoTeamDescription (VID-DD-0001)
- This video gives basic information on Using the DLRX "DirectLogic Network read" instruction in the Do-more designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0
Online Support Page: https://community.automationdirect.com/s/?utm_source=HX1th57oYeU&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
This instruction should only be used, to read from a Directlogic PLC. If you are using an ECOM or Ecom100, as your master device, Slave ID will be the only option available. You will need to use the Netedit tool to set up this ID. When using the internal Ethernet port, all three addressing options are available, but I find it best to use Fixed or variable addressing. This is the most common stumbling block, notice this instruction uses number of bytes and not number of addresses. These are the ways that this instruction can be triggered. I usually set the instruction for the following settings with a constant time of 1 second until I can verify I have good Communications. For more information on this instruction click here
Voted #1 mid-sized employer in Atlanta
Check out our
job openings