AutomationDirect
Login | Register
Accounts & Orders
Cart
0
$0.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $0.00
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
Videos Home > NITRA PAL Integration with Pro...

NITRA PAL Integration with Productivity PLC at AutomationDirect


Related Products

PAL-ACC20
PAL-ACC20 Thumbnail
PAL-ACC21
PAL-ACC21 Thumbnail
PAL-EIP
PAL-EIP Thumbnail
PAL-ACC19
PAL-ACC19 Thumbnail
PAL-SPC
PAL-SPC Thumbnail
PAL-E25
PAL-E25 Thumbnail
PAL-E44
PAL-E44 Thumbnail
PAL-P12
PAL-P12 Thumbnail
PAL-C2
PAL-C2 Thumbnail
PAL-C3
PAL-C3 Thumbnail
PAL-C4
PAL-C4 Thumbnail
PAL-S01
PAL-S01 Thumbnail
PAL-S02
PAL-S02 Thumbnail
PAL-S03
PAL-S03 Thumbnail
PAL-S04
PAL-S04 Thumbnail
PAL-S05
PAL-S05 Thumbnail
PAL-S06
PAL-S06 Thumbnail
PAL-S07
PAL-S07 Thumbnail
PAL-S08
PAL-S08 Thumbnail
PAL-CB4414
PAL-CB4414 Thumbnail
PAL-CB4814
PAL-CB4814 Thumbnail
PAL-B3314
PAL-B3314 Thumbnail
PAL-B3614
PAL-B3614 Thumbnail
PAL-B4414
PAL-B4414 Thumbnail
PAL-B4814
PAL-B4814 Thumbnail
PAL-M12
PAL-M12 Thumbnail
PAL-M12P
PAL-M12P Thumbnail
PAL-V2-32C
PAL-V2-32C Thumbnail
PAL-V2-32A
PAL-V2-32A Thumbnail
PAL-V2-32C32A
PAL-V2-32C32A Thumbnail
PAL-V1-52
PAL-V1-52 Thumbnail
PAL-V2-52
PAL-V2-52 Thumbnail
PAL-V2-53C
PAL-V2-53C Thumbnail
PAL-V1-32C
PAL-V1-32C Thumbnail
PAL-V1-32A
PAL-V1-32A Thumbnail
PAL-V1-SR
PAL-V1-SR Thumbnail
PAL-V0-PLUG
PAL-V0-PLUG Thumbnail
PAL-Y38
PAL-Y38 Thumbnail
PAL-PC12
PAL-PC12 Thumbnail
PAL-PC04M
PAL-PC04M Thumbnail
PAL-PC06M
PAL-PC06M Thumbnail
PAL-PC08M
PAL-PC08M Thumbnail
PAL-PC14
PAL-PC14 Thumbnail
PAL-ACC01
PAL-ACC01 Thumbnail
PAL-ACC02
PAL-ACC02 Thumbnail
PAL-ACC03
PAL-ACC03 Thumbnail
PAL-ACC04
PAL-ACC04 Thumbnail
PAL-ACC05
PAL-ACC05 Thumbnail
PAL-ACC06
PAL-ACC06 Thumbnail
PAL-ACC07
PAL-ACC07 Thumbnail
PAL-ACC08
PAL-ACC08 Thumbnail
PAL-ACC09
PAL-ACC09 Thumbnail
PAL-ACC10
PAL-ACC10 Thumbnail
PAL-ACC11
PAL-ACC11 Thumbnail
PAL-ACC12
PAL-ACC12 Thumbnail
PAL-ACC13
PAL-ACC13 Thumbnail
PAL-ACC14
PAL-ACC14 Thumbnail
PAL-ACC15
PAL-ACC15 Thumbnail
PAL-ACC16
PAL-ACC16 Thumbnail
PAL-ACC17
PAL-ACC17 Thumbnail
PAL-ACC18
PAL-ACC18 Thumbnail
PAL-EAD
PAL-EAD Thumbnail


To learn more: https://www.automationdirect.com/solenoid-valve-io?utm_source=H3E4hcr1ldw&utm_medium=VideoTeamDescription

(VID-PN-0049)

NITRA PAL Pneumatic solenoid and IO distribution system Integrate via Ethernet/IP to Productivity series PLC. In this video we will detail the process of creating an EthernetIP device, in Productivity PLC, inserting tasks to handle the NITRA PAL in Productivity PLC and pass data between the NITRA PAL and Productivity PLC

Online Support Page: https://community.automationdirect.com/s/?utm_source=H3E4hcr1ldw&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

AutomationDirect NITRA PAL or Pneumatic Automation Link is a highly versatile and scalable remote I/O and pneumatic system integrated via Ethernet/IP. AutomationDirect has made it simple to integrate your NITRA PAL with the Productivity series PLCs. There are just 3 steps to accomplish this. First import the EDS and create the Ethernet/IP device. Next, import the tasks and add to your code. And last pass data between the device and the tasks. Please follow this link or scan this QR code to get all the software and documentation for your system. Within these downloads, you’ll find the files referenced in this video and a walkthrough that accompanies this video for further reference. This video assumes the PAL system has already been configured. If you have not already configured it, please see the video in the link above. A brief note on Ethernet/IP. There are several terms that get used interchangeably. The PAL unit is an adapter, this is also called a server or a target. The PLC is a Scanner that may be called a client or an originator. So essentially, this means the PLC always initiates the connection for the exchange of data. On the Ethernet/IP tab of your hardware configuration within Productivity Suite import the EDS file from the link above and give it a name. Drag this new device to the left and add an exclusive owner message. I like using the structure to make tag name creation simple and logical. Then we’ll add an input array - this should be an 8-bit unsigned data type and 146 columns. This target to originator array or input array is the data the PLC receives from the PAL. And in an output array, this should also be an 8-bit unsigned data type, and it requires 102 columns. The originator to target array, also called the output array is the data the PLC sends to the PAL. And for troubleshooting help, let’s add an extended status array. This can tell us a lot about issues if we happen to have any. This completes the Ethernet/IP device creation for a single PAL unit. If you have more than one unit, you’ll repeat this process for each unit. To make things even easier, we’ve created tasks to manage your NITRA PAL data. These tasks are also part of the above download. We’ll just import the tasks into the task library. Now we can see the input and output tasks. Move the input task to run every scan above all other tasks. This ensures the inputs are updated prior to any logic that may use them. Then we’ll place the output task and run every scan. This should be the last task so that outputs changed by other logic will get updated properly. You’ll need to customize these tasks to your system. First, make sure the number of columns in the PAL user-defined structure is equal to the number of PAL systems you are adding. Since we only have one system, the default value of 1 is correct. While we’re in the Tagname database let’s look at what’s been created. The PAL_unit user-defined structure has all the PAL data in a logical fashion. We can see each of our I/O modules and valves with common sense names. You’ll need to pass the data from the Ethernet/IP device to the tasks. At the beginning of the input task, we’ll copy the target to originator (T->O) array we created in the EtherNet IP client into the PAL_unit user- defined structure that the task has created. This provides a more logical breakdown of the data from the PAL. We’ll also copy the number of PAL systems into the MaxNo_PAL_units tag so the logic can scan all units. In our case, this is 1 since we only have one system. At the end of the output task, we add another copy array so the UDS can be copied to the originator to target (O->T) array created in the device. If you have multiple PAL systems and created multiple PAL Ethernet/IP devices, you will need to duplicate these copies for each one and have them pass data to different columns of the PAL_unit user-defined structure. We need to enable the message, so I’ll just add an out coil to the main task. Now, download and make sure the CPU is in run mode. We can see the entire system in the user-defined structure so I’ll toggle a valve and verify it is functioning. Notice the diagnostic data reads 0 indicating there is no error. If an error code were present we could refer to the configuration software help file for a definition. So that’s it. We’re up and running with our PAL connected to our Productivity PLC. AutomationDirect is providing the products and support you need to make us your common-sense way to buy industrial controls. Please see this playlist for more integration videos and other content for the NITRA PAL system. We have a vast library of other videos. Please click here to view all product videos. Click here to subscribe to our YouTube channel for upcoming products and solutions.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info