To learn more: https://www.AutomationDirect.com/mccb?utm_source=H0P8TnWL2Cs&utm_medium=VideoTeamDescription
(VID-PPO-0006)
This video demonstrates installing the Eaton Flex Shaft disconnect handle to an Eaton MCCB. This works for the G-Frame, F-Frame, K-Frame and L-Frame Molded Case Circuit breakers from Eaton.
Online Support Page: https://community.automationdirect.com/s/?utm_source=H0P8TnWL2Cs&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
[Music] hi my name is brent o'reilly and i'm a product marketing engineer for eaton's molded case circuit breaker product line today we're going to demonstrate the installation of eaton's flex shaft handle for molded-case circuit breakers switches and hmcps we'll be using a b-line enclosure for the demonstration as you can see this circuit breaker has already been installed in the b-line enclosure for simplicity the breaker installation process is omitted from this tutorial first we'll attach the outer handle and toggle mechanism to the enclosure start by removing the two screws and lock washers from the outer handle mechanism place the handle with attached gasket over the enclosure cutout as shown insert the top quarter 20 mounting screw and lock washer through the enclosure and thread into the outer handle mac only tighten the screw for a few turns with the outer handle mechanism held loosely in place slide the toggle mechanism assembly over the top of the handle mounting screw insert the bottom mounting screw and lock washer through the toggle mechanism bracket the beeline enclosure and then into the handle adjust both mounting screws to the prescribed tightness next we'll attach the actuator mechanism which connects directly to the breaker handle remove and discard the two primary cover screws as demonstrated verify that the breaker and the outer handle mechanism are both in the on position but not connected to a power source this will make it much easier to mount the actuator place the actuator on the front of the breaker and orient the slider so that the slot captures the breaker handle fasten securely with the two 10 32 three and a half inch screws and two number eight three quarter inch thread cutting screws with the actuator fastened in place we will install the spring connect the long end of the spring through the hole in the handle actuator link as shown hook the shorter end of the spring into the tab on the lower portion of the toggle mechanism rotate the bell crank toward the handle and rotate the outer handle to the on position also make sure that the breaker itself is in the on position align the actuator link and attach it to the bell crank as shown secure it using an e-ring mount the door interlock pin and lock washer to the handle adjust to the prescribed tightness operate the handle mechanism to ensure functionality to operate either close the door or defeat the door interlock lever if minor adjustments are necessary refer to the adjustment checklist in section 3 of the instruction leaflet it is important to note that the fully seated outer handle position is reserved for breaker reset the off position is located just prior to the reset position finally you'll need to install any appropriate door hardware which is supplied in the kit thank you for watching and please refer to the instruction leaflet for any additional questions [Music] you
Voted #1 mid-sized employer in Atlanta
Check out our
job openings