WEG CFW VFD Quick Start 1 WPS Software from AutomationDirect


Related Products

CFW300A01P6S1NB20
CFW300A01P6S1NB20 Thumbnail
CFW300A06P0S1NB20
CFW300A06P0S1NB20 Thumbnail
CFW300A01P6S2NB20
CFW300A01P6S2NB20 Thumbnail
CFW300A02P6S2NB20
CFW300A02P6S2NB20 Thumbnail
CFW300A04P2S2NB20
CFW300A04P2S2NB20 Thumbnail
CFW300A06P0S2NB20
CFW300A06P0S2NB20 Thumbnail
CFW300A07P3S2NB20
CFW300A07P3S2NB20 Thumbnail
CFW300A01P6T2NB20
CFW300A01P6T2NB20 Thumbnail
CFW300A02P6T2NB20
CFW300A02P6T2NB20 Thumbnail
CFW300A04P2T2NB20
CFW300A04P2T2NB20 Thumbnail
CFW300A06P0T2NB20
CFW300A06P0T2NB20 Thumbnail
CFW300A07P3T2NB20
CFW300A07P3T2NB20 Thumbnail
CFW300B10P0B2DB20
CFW300B10P0B2DB20 Thumbnail
CFW300B15P2T2DB20
CFW300B15P2T2DB20 Thumbnail
CFW300-CRS232
CFW300-CRS232 Thumbnail
CFW300-CRS485
CFW300-CRS485 Thumbnail
CFW300-CUSB
CFW300-CUSB Thumbnail
CFW300-KHMIR
CFW300-KHMIR Thumbnail
CFW300-IODR
CFW300-IODR Thumbnail
CFW300-IOAR
CFW300-IOAR Thumbnail
CFW300-IOADR
CFW300-IOADR Thumbnail
CFW300-IOAENC
CFW300-IOAENC Thumbnail
CFW300-KFA-S1-S2
CFW300-KFA-S1-S2 Thumbnail
CFW300-KFB-S2
CFW300-KFB-S2 Thumbnail
CFW-WPS
CFW-WPS Thumbnail
CFW300-FAN-A
CFW300-FAN-A Thumbnail
CFW300-FAN-B
CFW300-FAN-B Thumbnail
CFW100A01P6S120G2
CFW100A01P6S120G2 Thumbnail
CFW100B02P6S120G2
CFW100B02P6S120G2 Thumbnail
CFW100A01P6S220G2
CFW100A01P6S220G2 Thumbnail
CFW100B02P6S220G2
CFW100B02P6S220G2 Thumbnail
CFW100C04P2S220G2
CFW100C04P2S220G2 Thumbnail
CFW100-KHMIR
CFW100-KHMIR Thumbnail
CFW100-IOD
CFW100-IOD Thumbnail
CFW100-IOAR
CFW100-IOAR Thumbnail
CFW100-IOADR
CFW100-IOADR Thumbnail
CFW100-IOA
CFW100-IOA Thumbnail
CFW100-CUSB
CFW100-CUSB Thumbnail
CFW100-CRS485
CFW100-CRS485 Thumbnail
CFW100-IOP
CFW100-IOP Thumbnail
CFW100-KFABC-S2
CFW100-KFABC-S2 Thumbnail
CFW100-KFABC-S1
CFW100-KFABC-S1 Thumbnail
15570800
15570800 Thumbnail
15571879
15571879 Thumbnail
15571881
15571881 Thumbnail
15574655
15574655 Thumbnail
15575067
15575067 Thumbnail
15572625
15572625 Thumbnail
15572689
15572689 Thumbnail
15575202
15575202 Thumbnail
15575701
15575701 Thumbnail
15575716
15575716 Thumbnail
15576540
15576540 Thumbnail
15577077
15577077 Thumbnail
15342437
15342437 Thumbnail
15342760
15342760 Thumbnail
15342909
15342909 Thumbnail
15572819
15572819 Thumbnail
15572908
15572908 Thumbnail
15573714
15573714 Thumbnail
15573819
15573819 Thumbnail
15573823
15573823 Thumbnail
15575568
15575568 Thumbnail
15575577
15575577 Thumbnail
15575665
15575665 Thumbnail
15575699
15575699 Thumbnail
15575707
15575707 Thumbnail
15576919
15576919 Thumbnail
15577021
15577021 Thumbnail
15577211
15577211 Thumbnail
15577452
15577452 Thumbnail
15733937
15733937 Thumbnail
15734064
15734064 Thumbnail
15734119
15734119 Thumbnail
14990863
14990863 Thumbnail
14991103
14991103 Thumbnail
14991753
14991753 Thumbnail
14938005
14938005 Thumbnail
14938047
14938047 Thumbnail
14938113
14938113 Thumbnail
14975838
14975838 Thumbnail
14938655
14938655 Thumbnail
14991953
14991953 Thumbnail
14992148
14992148 Thumbnail
14976517
14976517 Thumbnail
14976809
14976809 Thumbnail
14977065
14977065 Thumbnail
14977266
14977266 Thumbnail
14977397
14977397 Thumbnail
14978365
14978365 Thumbnail
14978573
14978573 Thumbnail
14989840
14989840 Thumbnail
14990985
14990985 Thumbnail
14991517
14991517 Thumbnail
14937890
14937890 Thumbnail
14938041
14938041 Thumbnail
14938111
14938111 Thumbnail
14975783
14975783 Thumbnail
14938547
14938547 Thumbnail
14991899
14991899 Thumbnail
14992113
14992113 Thumbnail
14975888
14975888 Thumbnail
14976683
14976683 Thumbnail
14976814
14976814 Thumbnail
14977261
14977261 Thumbnail
14977391
14977391 Thumbnail
14977629
14977629 Thumbnail
14978548
14978548 Thumbnail
CFW320A01P6S1NB20
CFW320A01P6S1NB20 Thumbnail
CFW320A02P6S1NB20
CFW320A02P6S1NB20 Thumbnail
CFW320A04P2S1NB20
CFW320A04P2S1NB20 Thumbnail
CFW320A06P0S1NB20
CFW320A06P0S1NB20 Thumbnail
CFW320A01P6S2NB20
CFW320A01P6S2NB20 Thumbnail
CFW320A02P6S2NB20
CFW320A02P6S2NB20 Thumbnail
CFW320A04P2S2NB20
CFW320A04P2S2NB20 Thumbnail
CFW320A06P0S2NB20
CFW320A06P0S2NB20 Thumbnail
CFW320A07P3S2NB20
CFW320A07P3S2NB20 Thumbnail
CFW320A01P6T2NB20
CFW320A01P6T2NB20 Thumbnail
CFW320A02P6T2NB20
CFW320A02P6T2NB20 Thumbnail
CFW320A04P2T2NB20
CFW320A04P2T2NB20 Thumbnail
CFW320A06P0T2NB20
CFW320A06P0T2NB20 Thumbnail
CFW320A07P3T2NB20
CFW320A07P3T2NB20 Thumbnail
CFW320B10P0B2DB20
CFW320B10P0B2DB20 Thumbnail
CFW320B15P2T2DB20
CFW320B15P2T2DB20 Thumbnail
CFW320A01P1T4NB20
CFW320A01P1T4NB20 Thumbnail
CFW320A02P6T4NB20
CFW320A02P6T4NB20 Thumbnail
CFW320A03P5T4NB20
CFW320A03P5T4NB20 Thumbnail
CFW320A04P8T4NB20
CFW320A04P8T4NB20 Thumbnail
CFW320B07P6T4NB20
CFW320B07P6T4NB20 Thumbnail
CFW320C11P0T4NB20
CFW320C11P0T4NB20 Thumbnail
CFW320C14P0T4NB20
CFW320C14P0T4NB20 Thumbnail
CFW320B01P1T4DB20
CFW320B01P1T4DB20 Thumbnail
CFW320B02P6T4DB20
CFW320B02P6T4DB20 Thumbnail
CFW320B03P5T4DB20
CFW320B03P5T4DB20 Thumbnail
CFW320B04P8T4DB20
CFW320B04P8T4DB20 Thumbnail
CFW320B07P6T4DB20
CFW320B07P6T4DB20 Thumbnail
CFW320C11P0T4DB20
CFW320C11P0T4DB20 Thumbnail
CFW320C14P0T4DB20
CFW320C14P0T4DB20 Thumbnail
CFW320-CRS232
CFW320-CRS232 Thumbnail
CFW320-CRS485
CFW320-CRS485 Thumbnail
CFW320-CUSB
CFW320-CUSB Thumbnail
CFW320-IODR
CFW320-IODR Thumbnail
CFW320-IOAR
CFW320-IOAR Thumbnail
CFW320-IOAENC
CFW320-IOAENC Thumbnail
MMF-uDrives
MMF-uDrives Thumbnail
CFW320-KHMIR
CFW320-KHMIR Thumbnail
CFW320-KFA-S1-S2
CFW320-KFA-S1-S2 Thumbnail
CFW320-KFB-S2
CFW320-KFB-S2 Thumbnail
CFW320-CETH
CFW320-CETH Thumbnail
CFW320-IOP
CFW320-IOP Thumbnail
CFW320-IODF
CFW320-IODF Thumbnail
CFW320-KFA-T2
CFW320-KFA-T2 Thumbnail
CFW320-KFB-T2
CFW320-KFB-T2 Thumbnail
CFW320-KFA-T4
CFW320-KFA-T4 Thumbnail
CFW320-KFB-T4
CFW320-KFB-T4 Thumbnail
CFW320-KFC-T4
CFW320-KFC-T4 Thumbnail


To learn more: https://www.automationdirect.com/drives?utm_source=E4EqEJ_m99M&utm_medium=VideoTeamDescription

(VID-DR-0071)

A quick introduction to the FREE WEG Programming Software (WPS) and how to use it to quickly view and change parameters in a WEG VFD CFW300. WEG Electric Windows configuration software, USB or free download. For use with all WEG CFW series AC drives and SSW07 and SSW900 series soft starters. Requires PC USB or RJ45 port and corresponding communication module for CFW or SSW series products.

Online Support Page: https://community.automationdirect.com/s/?utm_source=E4EqEJ_m99M&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

The WEG Programming Software makes it super easy to monitor and configure a drive. BUT, before starting though there are a couple important things you need to know. First and MOST important – don’t plug a USB cable into the drive. Yeah, I know, it has a couple ports that look just like mini-USB connectors, but you do NOT want to plug a USB cable into those – bad things can happen to the drive and your PC. The only way to communicate with this drive from your PC is to use one of the three available communications modules. Let’s install the 485 module for this video. Make sure the power to the drive is off – the manufacturer recommends waiting 10 minutes - then remove this cover and plug in the 485 module. I’m using this USB to 485 converter with this flying lead cable and all I have to do is connect the RED wire to plus and the green wire to minus. Apply power to the drive and launch the WEG Programming Software, which I’ll refer to as WPS. If this “show welcome” screen box is checked then you will see this dialog. For this video we are just going to quickly monitor and change some parameters sing this guy. If the box isn’t checked, then just go to On Line >> Quick Parameter Monitoring. I like leaving that box checked so I don’t have to remember which menu this is in. If you ever need to get back to the Welcome screen, it’s up here in the Help Menu. Click on quick parameters monitoring. Even though we are using a USB converter, the PC thinks it is a serial port so we check this one. We need to know which serial port the USB converter is emulating so bring up your PC’s device manager, open ports and we see that this Silicon Labs device is on port 12, so we put that … here. The rest of this is the default for the CFW300 drive so I’ll hit test to make sure we can connect. Yep, the device is on line and we are good to go. If test DOESN’T give you that result, then check that these settings match these serial parameters in the drive. Click OK and you instantly see all the drives parameters, names, factory defaults and units. And since we are connected to the drive, these are the actual parameters in the drive. You can also view by category – if I click on Motor control, then I only see the parameters associated with motor control, and I can even limit those to just the common ones, and the common ones I can view by groups. Let’s narrow that down to just the ramps values. The red numbers highlight differences between the on line and off-line values. That makes it super easy to see what’s different. Again, these on-line values are the real-time values. If I change parameter 100 on the drive … you immediately see that change on the screen. Likewise, if I change the parameter change on the screen, the parameter in the drive changes when I hit return, click away or tab away from the cell. So, changing single parameters is super quick and easy. Suppose you want to change the parameters in bulk. For example, let’s write all of these red ramp parameters to the drive – Well, I just hit the write button - and it sends all the parameters in this list to the drive. That’s important to understand. This write button only writes the parameters in the currently selected list For example, I’ll change these ramp parameters again … then select regulation. I’ll change the regulation and hit the write button. Now if I go back to the ramps parameters – ahh look at that! - they are unchanged. Again, the write button only updates the parameters that in the currently selected list. So, if I want to write all parameters, then I would click here to select all parameters and THEN hit the write button. It’s great that this WPS software gives me complete control over what gets written to the drive. This read button works the same way – it only reads the parameters in the currently selected list. Again, giving you complete control over which parameters you want to mess with. What if you want to write only some of the parameters in a group? Just select the parameters you don’t want to mess with and hit the minus button. It removed them from this window, so now they won’t get written or read for that matter. Want them back? Hit the plus button and select the parameters you want back and hit ok. This is cool – I can filter parameters shown. I currently have all parameters selected, but suppose I only want to see parameters that deal with “current.” Look at that, the software narrows the list as I type. How about fire mode? Or braking? Very cool. That’s a huge time saver when I am trying to find a specific parameter AND it also clues me in to other parameters I may not have been aware of. I love that feature. Parameters 910 and up are user parameters which are primarily used for the built in Soft PLC. Clicking on this button gives you total control over how those parameters are defined. You can change the data type, the min the max, the default value if it is retentive or not, read only, do you want the drive to ask for confirmation before implementing the change, is it password protected and do you want it displayed in hex. If you click on this guy, then you can also specify the units shown on the LCD display and even the number of digits. We’ll get into all of that in the video on the Soft PLC. For now, just beware that you have TOTAL control over those parameters. That’s amazing. In the next video we’ll learn about configurations. Configurations open up a whole bunch of handy features like Monitoring and configuration wizards that show all the common things you want to know about the drive at a glance, Monitoring windows that you can customize however you want, trending, diagnostics, and a whole lot more. In the meantime, click here to learn more about the WEG CFW300 variable frequency drive. Click here to learn about AutomationDirect’s free award winning support options, and click here to subscribe to our YouTube Channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > WEG CFW VFD Quick Start 1 WPS Software from AutomationDirect