To learn more: https://www.AutomationDirect.com/drives?utm_source=DPN7EX_C5Ks&utm_medium=VideoTeamDescription
(VID-DR-0118)
All of the PID videos that use a CFW300 VFD also apply to the CFW100 VFD. In this video we will look at the differences between the two and then do a live demo showing a CFW100 using PID.
Download resources used in these videos here: https://library.automationdirect.com/weg-vfd-pid-resource-page/
Online Support Page: https://community.automationdirect.com/s/?utm_source=DPN7EX_C5Ks&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
While we used a CFW300 drive in all of the videos in this series, everything we did in those videos also applies to the compact CFW100 drive – except for two things. First, while we used a single phase 120 Volt one horsepower CFW300 in all of the videos in this series, the CFW100 only goes to a half horsepower with a single phase 120 volt input. So we have to use single phase 240 volts as the power source to get 1 horsepower in a CFW100 drive. Second, the CFW300 has an analog input for the process variable on the base drive. The CFW100 doesn’t so we have to add an option module with an analog input The CFW100 has three option modules with analog inputs so I just chose the least expensive one. This video does a side by side comparison of all the option modules for the CFW100 and 300 drives. There is a little switch on the bottom that selects voltage or current input. It defaults to voltage, so I didn’t need to change it. I just removed this cover, plugged the module in and wired it like this. And since this appears to the drive as the same analog input 1 that we used on the CFW300 drive, we don’t have to modify any parameters at all. How about that? Everything else is identical so I took all of the parameters we used in the quick start and entered them directly into the CFW100 drive. I have auto mode selected, so I’ll switch to run and sure enough the CFW100 drive automatically adjusts the motor speed to maintain 6 psi. And if I change the load on the system by opening another valve – yep it automatically adjusts the motor speed to maintain 6psi. How about two more valves? Again, PID adjusts the motor speed to maintain 6 psi just like it did with the CFW300 drive. And that’s the point – everything we did in the PID series of videos using the CFW300 drive, applies directly to the CFW100. That’s it. I just used the exact same parameters as we used in the CFW300 drive, added an analog option module, switched to a single phase 240VAC supply and everything just worked. If we compare apples to apples and use 240 volt drives for both, the drives were the same price when I made this video, but I had to add an option module to the CFW100. So, if you are tight on cabinet space then it’s probably worth a couple dollars to have the smaller drive. Otherwise, the larger CFW300 is the way to go if you need to save a few dollars or need to use a single phase 120 volt supply.. Click here to see all of the videos in this series which also apply to the CFW100 drive. Click here to subscribe to our YouTube channel so you will be notified when we publish new videos and Click here to learn about AutomationDirect’s free award winning support options.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings