AutomationDirect
Login | Register
Accounts & Orders
Cart
0
$0.00

Recent Orders

View and Manage | Request Cancellation
Loading Order History
Loading...

Your Account

Account Home

Checkout   $0.00
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
Videos Home > Productivity3000 Send Text to ...

Productivity3000 Send Text to ViewMarq LED via Modbus from AutomationDirect


Related Products

MD4-0112T-1
MD4-0112T-1 Thumbnail
MD4-0124T-1
MD4-0124T-1 Thumbnail
MD4-0212T-1
MD4-0212T-1 Thumbnail
MD4-0224T-1
MD4-0224T-1 Thumbnail
MD4-0412T-1
MD4-0412T-1 Thumbnail
MD4-0424T-1
MD4-0424T-1 Thumbnail
MD-BRK-1
MD-BRK-1 Thumbnail
MD-BRK-2
MD-BRK-2 Thumbnail
MD-COM-COV
MD-COM-COV Thumbnail
MD-PGMSW
MD-PGMSW Thumbnail
MD-PWR-COV
MD-PWR-COV Thumbnail
MD-TERM-SET
MD-TERM-SET Thumbnail
MD-USER-M
MD-USER-M Thumbnail
P3-550
P3-550 Thumbnail
P3-530
P3-530 Thumbnail
P3-550E
P3-550E Thumbnail


To learn more: https://www.automationdirect.com//ViewMarq?utm_source=Bz5EakUfBYg&utm_medium=VideoTeamDescription

(VID-VW-0010)

How to use the Productivity3000 to display simple text messages on the ViewMarq LED Messaging display. REQUIRES Software Version 1.8 or better

Online Support Page: https://community.automationdirect.com/s/?utm_source=Bz5EakUfBYg&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

The procedure for controlling a Viewmarq via Modbus for most PLCs would be to send the message as a Modbus write, then when that is complete use a read instruction to do a bunch of Modbus reads of the command block to see when the Viewmarq is finished and then finally, read the Reply Status Block, to see if the result is "OK". If so then everything is ready to go, if not, then there was an error. The good news is you don't have to do ANY of that with the Productivity 3000. It has a built in Viewmarq instruction that does all of that message transfer and error checking for you! Let's take a look ... Let's start a brand new project and open up the hardware configuration. Make sure the controller is in Stop Mode and then hit this button to auto discover all of your hardware. This dialog is warning me that this PLC doesn't match my project -- we know that so we'll tell it to ignore all of these messages -- and here is our system. If we double click on that we can see that we have a small base, with a processor and an input simulator. Now we just double click on the CPU to configure it. We're going to connect to the Viewmarq via the serial port in this video, but if you were using the Ethernet port you would simply click on that tab. Over here in the serial port tab, we just need to match the settings that are on the ViewMarq. Our ViewMarq is operating at 38 4, it's at address 1, Odd Parity, 8 data bits, and 1 stop bit. Perfect. Over in the ViewMarq software, go ahead and establish communications between the PC and the Viewmarq. Our productivity 3000 project will be using serial Modbus so let's set this to the same thing: Modbus, 38 4, odd, 1 and 8. Once we have configured that connection, we can now go check out the LED display configuration. Since we're connected via Serial, we want to make sure we are talking Modbus, we have the right parameters, and for this demo we'll turn on the diagnostic LED. Perfect. Well, now that the hardware is setup, the software is trivial. We just drop a ViewMarq instruction in place. Let's scroll down until we find it. Right here. Drop it on the rung. And fill in the blanks. We're using the serial port, so we'll select that. The node address of the ViewMarq is 1 -- that's correct. Next we grab our ViewMarq string by pressing "copy" and we paste it in here. And then finally, we need to define a TAG for the Syntax Response. Let's call that the ViewMarq Reply. So we setup our serial port, we pasted our string in, and we setup the one required tag. Hit OK. The software recognizes that we created a new tag, and it asks: do we want to go ahead and create that tag? The answer is yes, but, I'm going to expand the length of this to 128 characters to give the ViewMarq plenty of room to reply. Let's add a contact to enable the message -- we'll use the input simulator so let me go back to the hardware configuration, double click on my input simulator, and let's define this first switch as our message enable. Now that we have done that, we can place a contact over here and we can enable this instruction by flipping that switch on the front of the input simulator. Note this little arrow right here on the ViewMarq instruction. That tells me this is an edge triggered instruction. So the rising edge of this contact will enable this instruction, and then it will run to completion over several scans all by itself. You don't have to worry about it. Let's go ahead and transfer our project over to the Productivity 3000. Now I'm gin got reach down to the input simulator and flip that enable switch we just setup.. And there's our message. Easy. Easy. So all we did was setup the Productivity3000 hardware, setup the Viewmarq hardware, drop a Viewmarq instruction on the screen and fill in the blanks. And that's all there is to it. That ought to be enough to get you going. Let us know if you have any questions. Automation Directs Customer Support is always free and just a phone call or e-mail away. Performance plus Value ... That's productivity. From Automation Direct.
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
Site Map    Send Us your Feedback    Unsubscribe    Email Preferences    Legal & Business Policies    Cookie Preferences    YouTube Terms of Service    AutomationDirect Product API
Clear login credentials
Back to Top


 Updating...
Info